Post Go back to editing

AD9371+ zcu102

Thread Summary

The user is trying to bring up the ADRV9371 on a ZCU102 platform using a bitstream generated with Vivado 2024.2. The final answer suggests building the device tree, kernel, and BOOT.bin manually, as meta-adi does not support PetaLinux 2024.2. The user should verify device initialization and data path functionality. The accompanying answers clarify that using a 2023 PetaLinux image with a 2024.2 bitstream is not recommended and ask for the desired sample rate and JESD mode.
AI Generated Content
Category: Software
Product Number: AD9371

Hi ,

I have a using ADRV9371, i have gebnerated build for zcu102 fpga board from ADI hdl git repo with 2024.2 Vivado version, after generating bit file 

1. What is the next step to get ADC / DAC data and configure sampling rate of Transciever?

2. If we will download Petalinx imagae for IIO etc then how to control / process data further in PL side of FPGA ?

3. My build bit file is generated with repect to 2024.2 Vivado version so can i work with petalinux image that is om 2023 by ADI?

Please assist for the same.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.