Post Go back to editing

Using libiio over PCIe between ZU4EG FPGA (Endpoint) and Jetson Host with AD9361

Thread Summary

The user inquires about streaming AD9361 ADC samples from a Zynq UltraScale+ ZU4EG FPGA to an NVIDIA Jetson platform via PCIe using libiio. The final answer confirms that libiio does not support PCIe transport directly, and data must be routed through the ARM on the Zynq. ADI does not provide PCIe IP or reference implementations for data movement. The fastest supported interfaces by libiio are Ethernet or USB.
AI Generated Content
Category: Software
Product Number: ad9361
Software Version: Petalinux-v2023.2

Hi Team,

We are currently evaluating the possibility of streaming AD9361 ADC samples from an FPGA (Zynq UltraScale+ ZU4EG) to an NVIDIA Jetson platform through PCIe using the libiio framework.

Setup details:

  • Transceiver: AD9361

  • FPGA: ZU4EG (configured as PCIe Endpoint)

  • Host: Jetson (Linux-based, acts as PCIe Root Complex)

  • Goal: Transfer ADC samples acquired through the AD9361 interface in FPGA fabric to Jetson via PCIe and access them using libiio (IIO context).

We want to confirm:

  1. Whether libiio supports PCIe transport between a Xilinx FPGA (Endpoint) and a Jetson host.

  2. If yes, what driver or setup is recommended for the FPGA endpoint side and Jetson host side?

  3. If not supported, what alternative interface ADI recommends for high-speed sample streaming from FPGA to Jetson using IIO.

Thank you very much for your guidance and support.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.