Post Go back to editing

AD9081 bypass with ZCU102

Category: Software

We are trying to use the AD9081 as an 8 channel high speed DAC/ADC system.  I see the hardware works fine with the example BOOT.BIN and dtb files.  (ie. zynqmp-zcu102-rev10-ad9081-204c-txmode0-rxmode1).

I have verified my build environment is fine and was able to re-create the same working setup from the linux and hdl sources.  I am using 2023.R2 for both the Xilinx tools as well as the 2023_R2 tags of the source repositories.

I started with the txmode0_rxmode1 dts as a starting point and modified the 204c and clock settings to what I thought was correct for txmode 35 and rxmode 25.10 with 17.96 GHz as the lane rates for both rx and tx.

The dts is inserted below

#include <dt-bindings/iio/frequency/hmc7044.h>
#include <dt-bindings/iio/adc/adi,ad9081.h>
#include "zynqmp-zcu102-rev10-ad9081-default.dtsi"

&axi_ad9081_rx_jesd {
	clocks = <&zynqmp_clk 71>, <&hmc7044 10>, <&axi_ad9081_adxcvr_rx 1>, <&axi_ad9081_adxcvr_rx 0>;
	clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
};

&axi_ad9081_tx_jesd {
	clocks = <&zynqmp_clk 71>, <&hmc7044 6>, <&axi_ad9081_adxcvr_tx 1>, <&axi_ad9081_adxcvr_tx 0>;
	clock-names = "s_axi_aclk", "device_clk", "link_clk", "lane_clk";
};

&axi_ad9081_adxcvr_rx {
	adi,sys-clk-select = <XCVR_QPLL>;
	adi,out-clk-select = <XCVR_PROGDIV_CLK>;
};

&axi_ad9081_adxcvr_tx {
	adi,out-clk-select = <XCVR_REFCLK>;
	adi,out-clk-select = <XCVR_PROGDIV_CLK>;
};

&spi1 {
	status = "okay";

	hmc7044: hmc7044@0 {
		#address-cells = <1>;
		#size-cells = <0>;
		#clock-cells = <1>;
		compatible = "adi,hmc7044";
		reg = <0>;
		spi-max-frequency = <1000000>;

		jesd204-device;
		#jesd204-cells = <2>;
		jesd204-sysref-provider;

		adi,jesd204-max-sysref-frequency-hz = <2000000>; /* 2 MHz */

		/*
		 * There are different versions of the AD9081-FMCA-EBZ & AD9082-FMCA-EBZ
		 * VCXO = 122.880 MHz, XO = 122.880MHz (AD9081-FMC-EBZ & AD9082-FMC-EBZ)
		 * VCXO = 100.000 MHz, XO = 100.000MHz (AD9081-FMC-EBZ-A2 & AD9082-FMC-EBZ-A2)
		 * To determine which board is which, read the freqency printed on the VCXO
		 * or use the fru-dump utility:
		 * #fru-dump -b /sys/bus/i2c/devices/15-0050/eeprom
		 */

		//adi,pll1-clkin-frequencies = <122880000 30720000 0 0>;
		//adi,vcxo-frequency = <122880000>;

		adi,pll1-clkin-frequencies = <100000000 10000000 0 0>;
		adi,vcxo-frequency = <100000000>;

		adi,pll1-loop-bandwidth-hz = <200>;
		adi,pll1-charge-pump-current-ua = <720>;
		adi,pfd1-maximum-limit-frequency-hz = <1000000>; /* 1 MHz */
		adi,pll1-ref-prio-ctrl = <0xE1>; /* prefer CLKIN1 -> CLKIN0 -> CLKIN2 -> CLKIN3 */
		adi,pll1-ref-autorevert-enable;

		adi,pll2-output-frequency = <2900000000>;

		adi,sysref-timer-divider = <1024>;
		adi,pulse-generator-mode = <0>;

		adi,clkin0-buffer-mode  = <0x07>;
		adi,clkin1-buffer-mode  = <0x07>;
		adi,oscin-buffer-mode = <0x15>;

		adi,gpi-controls = <0x00 0x00 0x00 0x00>;
		adi,gpo-controls = <0x37 0x33 0x00 0x00>;

		clock-output-names =
		"hmc7044_out0", "hmc7044_out1", "hmc7044_out2",
		"hmc7044_out3", "hmc7044_out4", "hmc7044_out5",
		"hmc7044_out6", "hmc7044_out7", "hmc7044_out8",
		"hmc7044_out9", "hmc7044_out10", "hmc7044_out11",
		"hmc7044_out12", "hmc7044_out13";

		hmc7044_c0: channel@0 {
			reg = <0>;
			adi,extended-name = "CORE_CLK_RX";
			adi,divider = <24>;
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
			adi.disable;
		};
		hmc7044_c2: channel@2 {
			reg = <2>;
			adi,extended-name = "DEV_REFCLK";
			adi,divider = <8>;
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
		};

		hmc7044_c3: channel@3 {
			reg = <3>;
			adi,extended-name = "DEV_SYSREF";
			adi,divider = <768>;
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
			adi,jesd204-sysref-chan;
		};

		hmc7044_c6: channel@6 {
			reg = <6>;
			adi,extended-name = "CORE_CLK_TX";
			adi,divider = <24>;
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
		};

		hmc7044_c8: channel@8 {
			reg = <8>;
			adi,extended-name = "FPGA_REFCLK1";
			adi,divider = <16>;
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
			adi.disable;
		};

		hmc7044_c10: channel@10 {
			reg = <10>;
			adi,extended-name = "CORE_CLK_RX_ALT";
			adi,divider = <24>;
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
		};

		hmc7044_c12: channel@12 {
			reg = <12>;
			adi,extended-name = "FPGA_REFCLK2";
			adi,divider = <16>;
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
		};

		hmc7044_c13: channel@13 {
			reg = <13>;
			adi,extended-name = "FPGA_SYSREF";
			adi,divider = <768>;
			adi,driver-mode = <HMC7044_DRIVER_MODE_LVDS>;
			adi,jesd204-sysref-chan;
		};
	};
};

&fmc_spi {

	trx0_ad9081: ad9081@0 {
		#address-cells = <1>;
		#size-cells = <0>;
		compatible = "adi,ad9081";
		reg = <0>;
		spi-max-frequency = <5000000>;

		/* Clocks */
		clocks = <&hmc7044 2>;
		clock-names = "dev_clk";

		clock-output-names = "rx_sampl_clk", "tx_sampl_clk";
		#clock-cells = <1>;

		jesd204-device;
		#jesd204-cells = <2>;
		jesd204-top-device = <0>; /* This is the TOP device */
		jesd204-link-ids = <FRAMER_LINK0_RX DEFRAMER_LINK0_TX>;

		jesd204-inputs =
			<&axi_ad9081_core_rx 0 FRAMER_LINK0_RX>,
			<&axi_ad9081_core_tx 0 DEFRAMER_LINK0_TX>;

		adi,tx-dacs {
			#size-cells = <0>;
			#address-cells = <1>;

			adi,dac-frequency-hz = /bits/ 64 <2900000000>;

			adi,main-data-paths {
				#address-cells = <1>;
				#size-cells = <0>;

				adi,interpolation = <1>;

				ad9081_dac0: dac@0 {
					reg = <0>;
					adi,crossbar-select = <&ad9081_tx_fddc_chan0>;
					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1000 MHz */
				};
				ad9081_dac1: dac@1 {
					reg = <1>;
					adi,crossbar-select = <&ad9081_tx_fddc_chan1>;
					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1000 MHz */
				};
				ad9081_dac2: dac@2 {
					reg = <2>;
					adi,crossbar-select = <&ad9081_tx_fddc_chan2>; /* All 4 channels @ dac2 */
					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1000 MHz */
				};
				ad9081_dac3: dac@3 {
					reg = <3>;
					adi,crossbar-select = <&ad9081_tx_fddc_chan3>; /* All 4 channels @ dac2 */
					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1000 MHz */
				};
			};

			adi,channelizer-paths {
				#address-cells = <1>;
				#size-cells = <0>;
				adi,interpolation = <1>;

				ad9081_tx_fddc_chan0: channel@0 {
					reg = <0>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
				ad9081_tx_fddc_chan1: channel@1 {
					reg = <1>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
				ad9081_tx_fddc_chan2: channel@2 {
					reg = <2>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
				ad9081_tx_fddc_chan3: channel@3 {
					reg = <3>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;

				};
			};

			adi,jesd-links {
				#size-cells = <0>;
				#address-cells = <1>;

				ad9081_tx_jesd_l0: link@0 {
					#address-cells = <1>;
					#size-cells = <0>;
					reg = <0>;

					adi,logical-lane-mapping = /bits/ 8 <0 2 7 7 1 7 7 3>;

					adi,link-mode = <35>;			/* JESD Quick Configuration Mode */
					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
					adi,version = <2>;			/* JESD VERSION 0=204A,1=204B,2=204C */
					adi,dual-link = <0>;			/* JESD Dual Link Mode */

					adi,converters-per-device = <4>;	/* JESD M */
					adi,octets-per-frame = <3>;		/* JESD F */

					adi,frames-per-multiframe = <256>;	/* JESD K */
					adi,converter-resolution = <12>;	/* JESD N */
					adi,bits-per-sample = <12>;		/* JESD NP' */
					adi,control-bits-per-sample = <0>;	/* JESD CS */
					adi,lanes-per-device = <8>;		/* JESD L */
					adi,samples-per-converter-per-frame = <4>; /* JESD S */
					adi,high-density = <1>;			/* JESD HD */

					adi,tpl-phase-adjust = <0x3>;
				};
			};
		};

		adi,rx-adcs {
			#size-cells = <0>;
			#address-cells = <1>;

			adi,adc-frequency-hz = /bits/ 64 <1450000000>;

			adi,main-data-paths {
				#address-cells = <1>;
				#size-cells = <0>;


				ad9081_adc0: adc@0 {
					reg = <0>;
					adi,decimation = <1>;
					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1000 MHz */
					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
					adi,digital-gain-6db-enable;
					//adi,crossbar-select = <&ad9081_rx_fddc_chan0>, <&ad9081_rx_fddc_chan2>; /* Static for now */
				};
				ad9081_adc1: adc@1 {
					reg = <1>;
					adi,decimation = <1>;
					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1000 MHz */
					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
					adi,digital-gain-6db-enable;
					//adi,crossbar-select = <&ad9081_rx_fddc_chan1>, <&ad9081_rx_fddc_chan3>; /* Static for now */
				};
				ad9081_adc2: adc@2 {
					reg = <2>;
					adi,decimation = <1>;
					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1000 MHz */
					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
					adi,digital-gain-6db-enable;
					//adi,crossbar-select = <&ad9081_rx_fddc_chan4>, <&ad9081_rx_fddc_chan6>; /* Static for now */
				};
				ad9081_adc3: adc@3 {
					reg = <3>;
					adi,decimation = <1>;
					adi,nco-frequency-shift-hz = /bits/ 64 <1000000000>; /* 1000 MHz */
					adi,nco-mixer-mode = <AD9081_ADC_NCO_VIF>;
					adi,digital-gain-6db-enable;
					//adi,crossbar-select = <&ad9081_rx_fddc_chan5>, <&ad9081_rx_fddc_chan7>; /* Static for now */
				};
			};

			adi,channelizer-paths {
				#address-cells = <1>;
				#size-cells = <0>;


				ad9081_rx_fddc_chan0: channel@0 {
					reg = <0>;
					adi,decimation = <1>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
					adi,digital-gain-6db-enable;

				};
				ad9081_rx_fddc_chan1: channel@1 {
					reg = <1>;
					adi,decimation = <1>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
					adi,digital-gain-6db-enable;

				};
				ad9081_rx_fddc_chan4: channel@4 {
					reg = <4>;
					adi,decimation = <1>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
					adi,digital-gain-6db-enable;

				};
				ad9081_rx_fddc_chan5: channel@5 {
					reg = <5>;
					adi,decimation = <1>;
					adi,gain = <2048>; /* 2048 * 10^(gain_dB/20) */
					adi,nco-frequency-shift-hz =  /bits/ 64 <0>;
					adi,digital-gain-6db-enable;
				};
			};

			adi,jesd-links {
				#size-cells = <0>;
				#address-cells = <1>;

				ad9081_rx_jesd_l0: link@0 {
					reg = <0>;
					adi,converter-select =
						<&ad9081_rx_fddc_chan0 FDDC_I>, <&ad9081_rx_fddc_chan0 FDDC_Q>,
						<&ad9081_rx_fddc_chan1 FDDC_I>, <&ad9081_rx_fddc_chan1 FDDC_Q>,
						<&ad9081_rx_fddc_chan4 FDDC_I>, <&ad9081_rx_fddc_chan4 FDDC_Q>,
						<&ad9081_rx_fddc_chan5 FDDC_I>, <&ad9081_rx_fddc_chan5 FDDC_Q>;

					adi,logical-lane-mapping = /bits/ 8 <2 0 7 7 7 7 3 1>;

					adi,link-mode = <25>;			/* JESD Quick Configuration Mode */
					adi,subclass = <1>;			/* JESD SUBCLASS 0,1,2 */
					adi,version = <2>;			/* JESD VERSION 0=204A,1=204B,2=204C */
					adi,dual-link = <0>;			/* JESD Dual Link Mode */

					adi,converters-per-device = <4>;	/* JESD M */
					adi,octets-per-frame = <6>;		/* JESD F */

					adi,frames-per-multiframe = <128>;	/* JESD K */
					adi,converter-resolution = <12>;	/* JESD N */
					adi,bits-per-sample = <12>;		/* JESD NP' */
					adi,control-bits-per-sample = <0>;	/* JESD CS */
					adi,lanes-per-device = <4>;		/* JESD L */
					adi,samples-per-converter-per-frame = <4>; /* JESD S */
					adi,high-density = <1>;			/* JESD HD */
				};
			};
		};
	};
};

&axi_ad9081_core_tx {
	single-shot-output-gpios = <&gpio 139 0>;
};

The FPGA system_project.tcl modifed to be:


adi_project ad9081_fmca_ebz_zcu102 0 [list \
  JESD_MODE        [get_env_param JESD_MODE      64B66B ] \
  RX_LANE_RATE     [get_env_param RX_LANE_RATE      17.96] \
  TX_LANE_RATE     [get_env_param TX_LANE_RATE      17.96 ] \
  RX_JESD_M        [get_env_param RX_JESD_M          4 ] \
  RX_JESD_L        [get_env_param RX_JESD_L          4 ] \
  RX_JESD_S        [get_env_param RX_JESD_S          2 ] \
  RX_JESD_NP       [get_env_param RX_JESD_NP        12 ] \
  RX_NUM_LINKS     [get_env_param RX_NUM_LINKS       1 ] \
  RX_TPL_WIDTH     [get_env_param RX_TPL_WIDTH      {} ] \
  TX_JESD_M        [get_env_param TX_JESD_M          4 ] \
  TX_JESD_L        [get_env_param TX_JESD_L          8 ] \
  TX_JESD_S        [get_env_param TX_JESD_S          4 ] \
  TX_JESD_NP       [get_env_param TX_JESD_NP        12 ] \
  TX_NUM_LINKS     [get_env_param TX_NUM_LINKS       1 ] \
  TX_TPL_WIDTH     [get_env_param TX_TPL_WIDTH      {} ] \
  TDD_SUPPORT      [get_env_param TDD_SUPPORT        0 ] \
  SHARED_DEVCLK    [get_env_param SHARED_DEVCLK      0 ] \
  TDD_CHANNEL_CNT  [get_env_param TDD_CHANNEL_CNT    2 ] \
  TDD_SYNC_WIDTH   [get_env_param TDD_SYNC_WIDTH    32 ] \
  TDD_SYNC_INT     [get_env_param TDD_SYNC_INT       1 ] \
  TDD_SYNC_EXT     [get_env_param TDD_SYNC_EXT       0 ] \
  TDD_SYNC_EXT_CDC [get_env_param TDD_SYNC_EXT_CDC   0 ] \
]

The jesd_status -s gives me:


The clk_summary is

                                 enable  prepare  protect                                duty         hardware
   clock                          count    count    count        rate   accuracy phase  cycle  nshot    enable
--------------------------------------------------------------------------------------------------------------
 clkin2_0                             0        0        0           0          0     0  50000        0
         Y
 clkin1_0                             0        0        0           0          0     0  50000        0
         Y
 si570_mgt                            0        0        0   148499999          0     0  50000        0
         Y
 si570_user                           0        0        0   299999998          0     0  50000        0
         Y
 hmc7044_out13                        0        0        0     2832031          0     0  50000        0
         Y
 hmc7044_out12                        2        2        0   181250000          0     0  50000        0
         Y
    tx_gt_clk                         0        0        0     3625000          0     0  50000        0
         ?
       tx_out_clk                     0        0        0    54924242          0     0  50000        0
         Y
    rx_gt_clk                         0        0        0           0          0     0  50000        0
         ?
       rx_out_clk                     0        0        0           0          0     0  50000        0
         Y
 hmc7044_out10                        0        0        0   181250000          0     0  50000        0
         Y
 hmc7044_out8                         0        0        0   181250000          0     0  50000        0
         Y
 hmc7044_out6                         0        0        0   181250000          0     0  50000        0
         Y
 hmc7044_out3                         0        0        0     2832031          0     0  50000        0
         Y
 hmc7044_out2                         2        2        0   362500000          0     0  50000        0
         Y
    spi1.0-tx_sampl_clk               1        1        0  2900000000          0     0  50000        0
         Y
    spi1.0-rx_sampl_clk               0        0        0  1450000000          0     0  50000        0
         Y
 hmc7044_out0                         0        0        0   120833333          0     0  50000        0
         Y
 refhdmi                              1        1        0   114285000          0     0  50000        0
         Y
    xtal_0                            0        0        0   114285000          0     0  50000        0
         Y
       pll_0                          0        0        0 40731174000000          0     0  50000        0
         Y
          clk1_0                      0        0        0    27000000          0     0  50000        0
         Y
          clk0_0                      0        0        0    27000000          0     0  50000        0
         Y
 ref48M                               2        2        0    48000000          0     0  50000        0
         Y
    si5341                            3        3        0    14000000          0     0  50000        0
         Y
       clock-generator.N4             0        0        0           0          0     0  50000        0
         Y
       clock-generator.N3             0        0        0           0          0     0  50000        0
         Y
       clock-generator.N2             1        1        0   104000000          0     0  50000        0
         Y
          clock-generator.2           1        2        0    26000000          0     0  50000        0
         Y
       clock-generator.N1             1        2        0   594000000          0     0  50000        0
         Y
          clock-generator.7           0        1        0    74250000          0     0  50000        0
         Y
          clock-generator.0           1        2        0    27000000          0     0  50000        0
         Y
       clock-generator.N0             1        5        0  1000000000          0     0  50000        0
         Y
          clock-generator.9           0        1        0    33333333          0     0  50000        0
         Y
          clock-generator.8           0        0        0           0          0     0  50000        0
         Y
          clock-generator.6           0        1        0   125000000          0     0  50000        0
         Y
          clock-generator.5           0        1        0   100000000          0     0  50000        0
         Y
          clock-generator.4           0        1        0   100000000          0     0  50000        0
         Y
          clock-generator.3           1        2        0   125000000          0     0  50000        0
         Y
          clock-generator.1           0        0        0           0          0     0  50000        0
         Y
 aux_ref_clk                          0        0        0    27000000          0     0  50000        0
         Y
 gt_crx_ref_clk                       0        0        0   108000000          0     0  50000        0
         Y
 pss_alt_ref_clk                      0        0        0           0          0     0  50000        0
         Y
 video_clk                            0        0        0    27000000          0     0  50000        0
         Y
 pss_ref_clk                          3        3        3    33333333          0     0  50000        0
         Y
    vpll_post_src                     0        0        0    33333333          0     0  50000        0
         Y
    vpll_pre_src                      1        1        1    33333333          0     0  50000        0
         Y
       vpll_int                       1        1        1  1781999697          0     0  50000        0
         Y
          vpll_half                   1        1        1   890999848          0     0  50000        0
         Y
             vpll_int_mux             1        1        1   890999848          0     0  50000        0
         Y
                vpll                  1        1        1   890999848          0     0  50000        0
         Y
                   dp_video_ref_mux       1        1        1   890999848          0     0  50000        0
         Y
                      dp_video_ref_div1       1        1        1   148499975          0     0  50000        0
         Y
                         dp_video_ref_div2       1        1        1   148499975          0     0  50000        0
         Y
                            dp_video_ref       1        1        1   148499975          0     0  50000        0
         Y
                   vpll_to_lpd        0        0        0   296999950          0     0  50000        0
         Y
    dpll_post_src                     0        0        0    33333333          0     0  50000        0
         Y
    dpll_pre_src                      0        0        0    33333333          0     0  50000        0
         Y
       dpll_int                       0        0        0  2099999979          0     0  50000        0
         Y
          dpll_half                   0        0        0  1049999989          0     0  50000        0
         Y
             dpll_int_mux             0        0        0  1049999989          0     0  50000        0
         Y
                dpll                  0        0        0  1049999989          0     0  50000        0
         Y
                   dpll_to_lpd        0        0        0   524999995          0     0  50000        0
         Y
    apll_post_src                     0        0        0    33333333          0     0  50000        0
         Y
    apll_pre_src                      1        1        1    33333333          0     0  50000        0
         Y
       apll_int                       1        1        1  2399999976          0     0  50000        0
         Y
          apll_half                   1        1        1  1199999988          0     0  50000        0
         Y
             apll_int_mux             1        1        1  1199999988          0     0  50000        0
         Y
                apll                  1        1        1  1199999988          0     0  50000        0
         Y
                   dpdma_ref_mux       1        1        1  1199999988          0     0  50000        0
         Y
                      dpdma_ref_div1       1        1        1   599999994          0     0  50000        0
         Y
                         dpdma_ref       1        1        1   599999994          0     0  50000        0
         Y
                   gdma_ref_mux       0        0        0  1199999988          0     0  50000        0
         Y
                      gdma_ref_div1       0        0        0   599999994          0     0  50000        0
         Y
                         gdma_ref       0        0        0   599999994          0     0  50000        0
         N
                   acpu_mux           0        0        0  1199999988          0     0  50000        0
         Y
                      acpu            0        0        0  1199999988          0     0  50000        0
         Y
    rpll_post_src                     0        0        0    33333333          0     0  50000        0
         Y
    rpll_pre_src                      0        0        0    33333333          0     0  50000        0
         Y
       rpll_int                       0        0        0  2399999976          0     0  50000        0
         N
          rpll_half                   0        0        0  1199999988          0     0  50000        0
         Y
             rpll_int_mux             0        0        0  1199999988          0     0  50000        0
         Y
                rpll                  0        0        0  1199999988          0     0  50000        0
         Y
                   spi1_ref_mux       0        0        0  1199999988          0     0  50000        0
         Y
                      spi1_ref_div1       0        0        0    99999999          0     0  50000        0
         Y
                         spi1_ref_div2       0        0        0    99999999          0     0  50000        0
         Y
                            spi1_ref       0        0        0    99999999          0     0  50000        0
         N
                   spi0_ref_mux       0        0        0  1199999988          0     0  50000        0
         Y
                      spi0_ref_div1       0        0        0    99999999          0     0  50000        0
         Y
                         spi0_ref_div2       0        0        0    99999999          0     0  50000        0
         Y
                            spi0_ref       0        0        0    99999999          0     0  50000        0
         N
                   rpll_to_fpd        0        0        0    22641510          0     0  50000        0
         Y
                      dp_stc_ref_mux       0        0        0    22641510          0     0  50000        0
         Y
                         dp_stc_ref_div1       0        0        0     1509434          0     0  50000        0
         Y
                            dp_stc_ref_div2       0        0        0     1509434          0     0  50000        0
         Y
                               dp_stc_ref       0        0        0     1509434          0     0  50000        0
         Y
                      dp_audio_ref_mux       0        0        0    22641510          0     0  50000        0
         Y
                         dp_audio_ref_div1       0        0        0    22641510          0     0  50000        0
         Y
                            dp_audio_ref_div2       0        0        0    22641510          0     0  50000        0
         Y
                               dp_audio_ref       0        0        0    22641510          0     0  50000        0
         N
    iopll_post_src                    0        0        0    33333333          0     0  50000        0
         Y
    iopll_pre_src                     1        1        1    33333333          0     0  50000        0
         Y
       iopll_int                      1        1        1  2999999970          0     0  50000        0
         Y
          iopll_half                  1        1        1  1499999985          0     0  50000        0
         Y
             iopll_int_mux            1        1        1  1499999985          0     0  50000        0
         Y
                iopll                14       17       11  1499999985          0     0  50000        0
         Y
                   gem3_ref_ung_mux       1        1        0  1499999985          0     0  50000        0
         Y
                      gem3_ref_ung_div1       1        1        0  1499999985          0     0  50000        0
         Y
                         gem3_ref_ung       1        1        0   124999999          0     0  50000        0
         Y
                            gem3_ref       2        2        0   124999999          0     0  50000        0
         Y
                               gem3_tx       1        1        0   124999999          0     0  50000        0
         Y
                   gem2_ref_ung_mux       0        0        0  1499999985          0     0  50000        0
         Y
                      gem2_ref_ung_div1       0        0        0    62500000          0     0  50000        0
         Y
                         gem2_ref_ung       0        0        0    62500000          0     0  50000        0
         Y
                            gem2_ref       0        0        0    62500000          0     0  50000        0
         Y
                               gem2_tx       0        0        0    62500000          0     0  50000        0
         Y
                   gem1_ref_ung_mux       0        0        0  1499999985          0     0  50000        0
         Y
                      gem1_ref_ung_div1       0        0        0    62500000          0     0  50000        0
         Y
                         gem1_ref_ung       0        0        0    62500000          0     0  50000        0
         Y
                            gem1_ref       0        0        0    62500000          0     0  50000        0
         Y
                               gem1_tx       0        0        0    62500000          0     0  50000        0
         Y
                   gem0_ref_ung_mux       0        0        0  1499999985          0     0  50000        0
         Y
                      gem0_ref_ung_div1       0        0        0    62500000          0     0  50000        0
         Y
                         gem0_ref_ung       0        0        0    62500000          0     0  50000        0
         Y
                            gem0_ref       0        0        0    62500000          0     0  50000        0
         Y
                               gem0_tx       0        0        0    62500000          0     0  50000        0
         Y
                   pl3_ref_mux        1        1        0  1499999985          0     0  50000        0
         Y
                      pl3_ref_div1       1        1        0    46875000          0     0  50000        0
         Y
                         pl3_ref_div2       1        1        0     9375000          0     0  50000        0
         Y
                            pl3_ref       1        1        0     9375000          0     0  50000        0
         Y
                   pl2_ref_mux        1        1        0  1499999985          0     0  50000        0
         Y
                      pl2_ref_div1       1        1        0   499999995          0     0  50000        0
         Y
                         pl2_ref_div2       1        1        0   499999995          0     0  50000        0
         Y
                            pl2_ref       3        3        0   499999995          0     0  50000        0
         Y
                   pl1_ref_mux        1        1        0  1499999985          0     0  50000        0
         Y
                      pl1_ref_div1       1        1        0   249999998          0     0  50000        0
         Y
                         pl1_ref_div2       1        1        0   249999998          0     0  50000        0
         Y
                            pl1_ref       1        1        0   249999998          0     0  50000        0
         Y
                   pl0_ref_mux        1        1        0  1499999985          0     0  50000        0
         Y
                      pl0_ref_div1       1        1        0    99999999          0     0  50000        0
         Y
                         pl0_ref_div2       1        1        0    99999999          0     0  50000        0
         Y
                            pl0_ref       3        3        0    99999999          0     0  50000        0
         Y
                   ams_ref_mux        1        1        1  1499999985          0     0  50000        0
         Y
                      ams_ref_div1       1        1        1    50000000          0     0  50000        0
         Y
                         ams_ref_div2       1        1        1    50000000          0     0  50000        0
         Y
                            ams_ref       1        1        1    50000000          0     0  50000        0
         Y
                   adma_ref_mux       0        0        0  1499999985          0     0  50000        0
         Y
                      adma_ref_div1       0        0        0   499999995          0     0  50000        0
         Y
                         adma_ref       0        0        0   499999995          0     0  50000        0
         Y
                   can1_ref_mux       0        0        0  1499999985          0     0  50000        0
         Y
                      can1_ref_div1       0        0        0    99999999          0     0  50000        0
         Y
                         can1_ref_div2       0        0        0    99999999          0     0  50000        0
         Y
                            can1_ref       0        0        0    99999999          0     0  50000        0
         N
                               can1       0        0        0    99999999          0     0  50000        0
         Y
                   can0_ref_mux       0        0        0  1499999985          0     0  50000        0
         Y
                      can0_ref_div1       0        0        0    46875000          0     0  50000        0
         Y
                         can0_ref_div2       0        0        0    46875000          0     0  50000        0
         Y
                            can0_ref       0        0        0    46875000          0     0  50000        0
         Y
                               can0       0        0        0    46875000          0     0  50000        0
         Y
                   i2c1_ref_mux       0        1        1  1499999985          0     0  50000        0
         Y
                      i2c1_ref_div1       0        1        1    99999999          0     0  50000        0
         Y
                         i2c1_ref_div2       0        1        1    99999999          0     0  50000        0
         Y
                            i2c1_ref       0        1        1    99999999          0     0  50000        0
         N
                   i2c0_ref_mux       0        1        1  1499999985          0     0  50000        0
         Y
                      i2c0_ref_div1       0        1        1    99999999          0     0  50000        0
         Y
                         i2c0_ref_div2       0        1        1    99999999          0     0  50000        0
         Y
                            i2c0_ref       0        1        1    99999999          0     0  50000        0
         N
                   nand_ref_mux       0        0        0  1499999985          0     0  50000        0
         Y
                      nand_ref_div1       0        0        0    46875000          0     0  50000        0
         Y
                         nand_ref_div2       0        0        0     9375000          0     0  50000        0
         Y
                            nand_ref       0        0        0     9375000          0     0  50000        0
         N
                   uart1_ref_mux       0        1        1  1499999985          0     0  50000        0
         Y
                      uart1_ref_div1       0        1        1    99999999          0     0  50000        0
         Y
                         uart1_ref_div2       0        1        1    99999999          0     0  50000        0
         Y
                            uart1_ref       0        1        1    99999999          0     0  50000        0
         N
                   uart0_ref_mux       1        1        1  1499999985          0     0  50000        0
         Y
                      uart0_ref_div1       1        1        1    99999999          0     0  50000        0
         Y
                         uart0_ref_div2       1        1        1    99999999          0     0  50000        0
         Y
                            uart0_ref       1        1        1    99999999          0     0  50000        0
         Y
                   sdio1_ref_mux       1        1        1  1499999985          0     0  50000        0
         Y
                      sdio1_ref_div1       1        1        1   187499999          0     0  50000        0
         Y
                         sdio1_ref_div2       1        1        1   187499999          0     0  50000        0
         Y
                            sdio1_ref       1        1        1   187499999          0     0  50000        0
         Y
                               clk_in_sd1       0        0        0    50000000          0     0  50000        0
         Y
                               clk_out_sd1       0        0        0    50000000          0     0  50000        0
         Y
                   sdio0_ref_mux       0        0        0  1499999985          0     0  50000        0
         Y
                      sdio0_ref_div1       0        0        0    99999999          0     0  50000        0
         Y
                         sdio0_ref_div2       0        0        0    99999999          0     0  50000        0
         Y
                            sdio0_ref       0        0        0    99999999          0     0  50000        0
         Y
                   qspi_ref_mux       1        1        1  1499999985          0     0  50000        0
         Y
                      qspi_ref_div1       1        1        1   124999999          0     0  50000        0
         Y
                         qspi_ref_div2       1        1        1   124999999          0     0  50000        0
         Y
                            qspi_ref       1        1        1   124999999          0     0  50000        0
         Y
                   gem_tsu_ref_mux       1        1        1  1499999985          0     0  50000        0
         Y
                      gem_tsu_ref_div1       1        1        1   249999998          0     0  50000        0
         Y
                         gem_tsu_ref_div2       1        1        1   249999998          0     0  50000        0
         Y
                            gem_tsu_ref       1        1        1   249999998          0     0  50000        0
         Y
                               gem_tsu       1        1        0   249999998          0     0  50000        0
         Y
                   usb3_dual_ref_mux       1        1        1  1499999985          0     0  50000        0
         Y
                      usb3_dual_ref_div1       1        1        1    60000000          0     0  50000        0
         Y
                         usb3_dual_ref_div2       1        1        1    20000000          0     0  50000        0
         Y
                            usb3_dual_ref       2        2        2    20000000          0     0  50000        0
         Y
                   usb1_bus_ref_mux       0        0        0  1499999985          0     0  50000        0
         Y
                      usb1_bus_ref_div1       0        0        0   124999999          0     0  50000        0
         Y
                         usb1_bus_ref_div2       0        0        0   124999999          0     0  50000        0
         Y
                            usb1_bus_ref       0        0        0   124999999          0     0  50000        0
         N
                   usb0_bus_ref_mux       1        1        1  1499999985          0     0  50000        0
         Y
                      usb0_bus_ref_div1       1        1        1   249999998          0     0  50000        0
         Y
                         usb0_bus_ref_div2       1        1        1   249999998          0     0  50000        0
         Y
                            usb0_bus_ref       1        1        1   249999998          0     0  50000        0
         Y
                   lpd_lsbus_mux       1        1        0  1499999985          0     0  50000        0
         Y
                      lpd_lsbus_div1       1        1        0    99999999          0     0  50000        0
         Y
                         lpd_lsbus       7        8        0    99999999          0     0  50000        0
         Y
                            lpd_wdt       0        0        0    99999999          0     0  50000        0
         Y
                   iopll_to_fpd       3        3        2   499999995          0     0  50000        0
         Y
                      topsw_lsbus_mux       1        1        0   499999995          0     0  50000        0
         Y
                         topsw_lsbus_div1       1        1        0    99999999          0     0  50000        0
         Y
                            topsw_lsbus       4        4        0    99999999          0     0  50000        0
         Y
                               fpd_wdt       1        1        0    99999999          0     0  50000        0
         Y
                      gpu_ref_mux       0        0        0   499999995          0     0  50000        0
         Y
                         gpu_ref_div1       0        0        0   499999995          0     0  50000        0
         Y
                            gpu_ref       0        0        0   499999995          0     0  50000        0
         Y
                               gpu_pp1_ref       0        0        0   499999995          0     0  50000        0
         N
                               gpu_pp0_ref       0        0        0   499999995          0     0  50000        0
         N
                      pcie_ref_mux       1        1        1   499999995          0     0  50000        0
         Y
                         pcie_ref_div1       1        1        1   249999998          0     0  50000        0
         Y
                            pcie_ref       1        1        1   249999998          0     0  50000        0
         Y
                      sata_ref_mux       1        1        1   499999995          0     0  50000        0
         Y
                         sata_ref_div1       1        1        1   249999998          0     0  50000        0
         Y
                            sata_ref       1        1        1   249999998          0     0  50000        0
         Y
 can1_mio                             0        0        0           0          0     0  50000        0
         Y
 can0_mio                             0        0        0           0          0     0  50000        0
         Y
 gem3_rx                              1        1        0           0          0     0  50000        0
         Y
 gem2_rx                              0        0        0           0          0     0  50000        0
         N
 gem1_rx                              0        0        0           0          0     0  50000        0
         N
 gem0_rx                              0        0        0           0          0     0  50000        0
         N

Any help would be greatly appreciated.

  • Hi,

    I may be wrong but I believe the maximum lane rate supported with ZCU102 platform is 16Gbps. If then, could you check the kernel message and see whether there is any related error?

    -YH

  • Yes, you are right:

    Mar 12 19:53:35 analog kernel: [    7.432817] axi-jesd204-tx 84b90000.axi-jesd204-tx: axi_jesd204_tx_jesd204_link_pre_setup: Link0 set lane rate 17943750 kHz failed (-22)
    Mar 12 19:53:35 analog kernel: [    7.445080] jesd204: /fpga-axi@0/axi-jesd204-tx@84b90000,jesd204:5,parent=84b90000.axi-jesd204-tx: JESD204[0:0] In link_pre_setup got error from cb: -22
    Mar 12 19:53:35 analog kernel: [    7.458730] jesd204: /axi/spi@ff040000/ad9081@0,jesd204:0,parent=spi1.0: Rolling back from 'link_supported', got error -22

    I will try to find config under 16Gbps and report back.  Thank you!

  • I tried just lowering the lane rate down to 11.96 but this does not work either as it seems I have exceeded the minimum DAC and ADC frequencies.  I am using this as a simple DAC and ADC.  Is there any way to bypass this lower frequency bound?

    Mar 13 09:25:22 analog kernel: [    5.200415] ad9081 spi1.0: Invalid param passed., "adc_clk_hz < 1450000000ULL" in adi_ad9081_device_clk_config_set(...), line596 in drivers/iio/adc/ad9081/adi_ad9081_device.c
    Mar 13 09:25:22 analog kernel: [    5.215981] ad9081 spi1.0: Invalid param passed., "dac_clk_hz < 2900000000ULL" in adi_ad9081_device_clk_config_set(...), line598 in drivers/iio/adc/ad9081/adi_ad9081_device.c
    Mar 13 09:25:22 analog kernel: [    5.232127] ad9081 spi1.0: Cannot find any settings to lock device PLL.
    Mar 13 09:25:22 analog kernel: [    5.238740] ad9081 spi1.0: Failed to initialize: -14
    Mar 13 09:25:22 analog kernel: [    5.243707] ad9081: probe of spi1.0 failed with error -14

  • Hi,

    It looks like you are trying to implement FBW mode for both TX and RX without any interpolation and decimation, then I see some issues in your device tree (and possibly HDL as well).

    For example, if you use JESD mode 25 for ADC path, then you have only the following options as specified in the user guide.

    Only the first line in the table is FBW mode, and in this case the lane rate cannot be lower than 16 Gbps. In order to keep it below, you need to have a different mode with either higher L or lower M. For example, you may be able to implement mode 28 with L=8 and M=4. 

    Please note that all CDDC and FDDC are bypassed in FBW with decimation ratio of 1x1 and it doesn't make sense to have M bigger than 4. Same rules apply to TX path as well.

    Please review the mode tables in the user guide. We should be able help you once you determine your target configuration consistent with the table.

    -YH

  • Thank you for the detailed response.  I think in order to meet both the lane rate maximum and the dac rate minimum, I have to settle for 2 DAC channels.  I have changed to TX mode 18 and TX mode 19.  Lane rate is 11.9625, DAC and ADC rates are both 2.9.  This build does appear to be working as the jesd_status looks clean and I don't see any errors in the kernel log



    I am using the pyadi-iio library but it's giving me some errors on initialization.  I will open a ticket on the Software Interface Tools board.

    Traceback (most recent call last):
      File "/home/analog/randomized_switching_generator_JA203.py", line 335, in <module>
        sdr = adi.ad9081()
      File "/usr/local/lib/python3.9/dist-packages/adi/ad9081.py", line 145, in __init__
        self._rx_coarse_ddc_channel_names.append(channels[0])
    IndexError: list index out of range

  • Thanks for the help!  I managed to modify the kernel driver as suggested as mentioned here https://ez.analog.com/linux-software-drivers/f/q-a/583588/ad9081-adc-output-glitches/538759.  I seem to be able send out data but I get nothing out of the DAC.  I tried using the oscilloscope/debug tool to drive out a sinewave but it comes out all corrupted.

    Is there anything else I should be looking into?

  • If I use the DAC buffer output with the sinewave matlab file, it seems there is a 300nS gap between bursts.

    I am able to use the tone generator in the oscilloscope program and it generates a continuous waveform properly.

    When I use the pyadi tx function with a single cycle generated sine wave pattern in tx cyclic buffer mode, I also see the same 300ns gap but only between each cycle.  Is this just a latency issue between the computer and the IC?

  • Thank you for the update and good to hear of your progress! I'll try to reproduce what you see and get back to you.

    Do you see this errorneous behaviour only with your modified profile, or is it same with the default profile?

  • I have only seen this since this bypass setup.  I have also narrowed it down a bit more in that it seems that the maximum buffer of samples I can send to the tx function is only 1030.  If I send more than that, I get no output.

    Before, with the normal profile (non-bypass), I could send any number of samples and I would always get an output.  It seems like some sort of buffer limit when in bypass?

  • I created a new profile, should be equivalent to yours, Tx mode 18 and Rx mode 19 (JESD_MODE=64B66B  RX_LANE_RATE=11.9625 TX_LANE_RATE=11.9625 RX_JESD_L=8 RX_JESD_M=2 RX_JESD_S=2 RX_JESD_NP=16 TX_JESD_L=8 TX_JESD_M=2 TX_JESD_S=2 TX_JESD_NP=16), and I confirmed your observation. With IIO OSC, the signal out of DAC is continuous if CW tone is generated with DDS and I see discountinuity in output when DAC Buffer Output is used. Will take a look and get back to you.

    Have a good weekend.