Post Go back to editing

ADIS16489 with Raspberry Pi 4

Category: Software
Product Number: ADIS16489
Software Version: Libiio version: 0.26

Hello,

what is the correct way to connect the ADIS16489 to the Raspberry Pi 4 using the EVAL-ADISIMU1-RPIZ board to read data from the ADIS16489?
This is what I tried:

 I loaded the ADI Kuiper Linux image on a microSD card (2023_r2 Image, wiki.analog.com/.../release_notes). Next, I tried to configure the Raspberry Pi with the required overlay by adding the following line in the /boot/config.txt file:
dtoverlay=adis16489
Then, I rebooted the Rasperry Pi and tried with iio_info and the ADI IIO Oscilloscope to connect to the sensor which did not work. I guess that the overlay configuration is wrong but I do not know what to change. 

This is the output of iio_info:

analog@analog:~ $ iio_info
iio_info version: 0.26 (git tag:bdd5c000)
Libiio version: 0.26 (git tag: bdd5c00) backends: local xml ip usb serial
IIO context created with local backend.
Backend version: 0.26 (git tag: bdd5c00)
Backend description string: Linux analog 6.1.54-v7l+ #1 SMP Tue Nov  5 15:29:09 UTC 2024 armv7l
IIO context has 4 attributes:
    hw_carrier: Raspberry Pi 4 Model B Rev 1.5
    dtoverlay: vc4-kms-v3d,adis16489
    local,kernel: 6.1.54-v7l+
    uri: local:
IIO context has 2 devices:
    hwmon0: cpu_thermal
        1 channels found:
            temp1:  (input)
            2 channel-specific attributes found:
                attr  0: crit value: 110000
                attr  1: input value: 35537
        No trigger on this device
    hwmon1: rpi_volt
        1 channels found:
            in0:  (input)
            1 channel-specific attributes found:
                attr  0: lcrit_alarm value: 0
        No trigger on this device

Thank you for your help!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.