ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
Question:
I am currently working with the ADRV9002 transceiver and have encountered a specific issue related to the LO frequency configuration when generating profiles.
Could you clarify the following:
buha - Moved from Microcontroller no-OS Drivers to Design Support ADRV9001 – ADRV9007. Post date updated from Tuesday, December 3, 2024 8:43 AM UTC to Thursday, December 5, 2024 8:38 AM UTC to reflect the move.
RahulMushini - Moved from Design Support ADRV9001 – ADRV9007 to Linux Software Drivers. Post date updated from Thursday, December 5, 2024 8:38 AM UTC to Monday, December 9, 2024 9:40 AM UTC to reflect the move.
Hi,
We will get back to you.
Regards
Rahul
Hi RahulMushini
waiting for the solution.
Hi,
In order to check the issue, I have used a LTE/Custom profile with TDD/FDD mode. I am able to change the LO frequencies when MCS is enabled and when MCS is disabled



and I am able to successfully program the chip.
The main idea behind having MCS enable is to have a deterministic latency between the channels, this should not restrict you from changing the LO frequencies. For more details please check the Multichip Synchronization chapter in our user guide.
Are you using TES GUI for generating the profile? are you using the custom board or EVB provided by ADI? Can you try again with the LTE profile with and without the MCS enable?
Regards
Rahul
Hi RahulMushini
Thank you for the guide.
This is the required settings
For the FDD mode it do not recommend to keep same LO for Tx and Rx. So I keep it default settings. 
I want to enable the MCS MODE: Enabled with RF PLL Phase 

When I generate profile with this configuration it do not allow to change the LO frequency from IIO
Hi,
After seeing the screen grab provided by you, I can see that the you are not facing issue with the TES, the problem is related to the IIO platform. I will move this question to the relevant IIO platform.
In future, in order get quick solution for the issue please follow the hardware and software selection guide which allow the user to chose the correct forum. link: https://www.analog.com/media/en/evaluation-boards-kits/evaluation-software/adrv9001_software_and_hardware_selection_guide.pdf?isDownload=true
This forum support issues related to product line sdk package.
Regards
Rahul