Hello,
Description:
I have a question corresponding to two products (as in subject) serializer MAX9295 which I want to run it with deserializer MAX96792A (GMSL3 ready). I want to run this setup with one single chanel/link in most easiest way.
So I decided (please correct me if I'm wrong) that the easiest setup it will be pixel mode (MAX9295 did not support tunneling) because it is easiest to run with enabled auto link config.
The I2C communication is working properly so I thought that there will be no problem to see data, but I'm receiving CIS CRC errors on VC0 - VC3. I'm wondering on which part of the configuration I should focused, to solve these problem?
Problems/Questions:
0) I cannot see the data, I'm receiving CIS CRC errors on VC0 - VC3 - on which part of settings I shoul pay atention?
1) What about I should remember writing configuration for this setup?
2) Does the LOCK should be 0V all the time?
3) FS and FE seems to be transferred well but
Br's,
Fr@nk