Is there a part / vendor for the camera used in this demonstration?
MAX96724
Recommended for New Designs
The MAX96724/F/R deserializer converts four GMSLâ„¢2/1 inputs to 1, 2, or 4 MIPI D-PHY or C-PHY outputs. The device allows simultaneous transmit bidirectional...
Datasheet
MAX96724 on Analog.com
MAX96717
Production
The MAX96717 GMSL™ serializer receives video on an MIPI CSI-2 interface and outputs it on a GMSL2 serial link transceiver. Simultaneously, it sends and...
Datasheet
MAX96717 on Analog.com
Is there a part / vendor for the camera used in this demonstration?
Hi clutch12 ,
Unfortunately that camera module is not available to the broad market but the GMSL drivers are generic and can be used with any sensor that Nvidia offers support for.
Can you please tell us the sensor you are targeting? Maybe you already saw but we have examples for the IMX219 (RPI CAM V2) too.
- Bogdan
Can you recommend a camera that you've tried that you think works that can be purchased?
I can get the IMX219 to work in two lane mode on the CAM0 interface. But, when I try to replicate that on my own custom board I can't get it to work. The lane mapping is a bit strange on CAM0 on the Orin dev board.
What I'd like to do is get the IMX219 to work on CAM1 that has more normal lane mapping but I can't get that to work. I've posted about that issue here:
Jetson Orin Nano MAX96724 / MAX96717 gmsl driver doesn't work