MAX96724
Recommended for New Designs
The MAX96724/F/R deserializer converts four GMSL2/1 inputs to 1, 2, or 4 MIPI D-PHY or C-PHY outputs. The device allows simultaneous transmit bidirectional...
Datasheet
MAX96724 on Analog.com
MAX96717
Recommended for New Designs
The MAX96717 GMSLâ„¢ serializer receives video on an MIPI CSI-2 interface and outputs it on a GMSL2 serial link transceiver. Simultaneously, it sends and...
Datasheet
MAX96717 on Analog.com
I'm able to get this to work
https://wiki.analog.com/resources/eval/user-guides/ad-gmslcamrpi-adp/ug_nvidia_jetson_orin_nano
But, I can't get the CAM1 to work with this dtb tegra234-p3767-0003-p3768-0000-a0-gmsl-7.dtb
Besides moving the cable from CAM0 to CAM1 on the Orin nano board are there any other changes?
Hi.
What do you mean by "I can't get the CAM1 to work with this dtb"?
Do the drivers not probe?
What's the output of running the command `media-ctl -p`?
Could you also give us the output of `dmesg`?
Thanks.