Hi,
I have question about possibility of not using FSYNC signal.
HW setup:
My HW connections looks like below:
CAM_SENS-------SER[MAX9292]---<GMSL2>---DES[MAX96724]-------SoC
Question:
For tests I want to run image streaming from single camera connected via MAX9292<>MAX96724 to the SoC. I'm wondering if it is possible to disable FSYNC on deserializer and recive a image from sensor to minimize the configuration?
Br's,
Frank.