Post Go back to editing

AD7124-8 Driver Issue: Input/Output Error When Reading Raw Data

Category: Software
Product Number: AD7124-8
Software Version: Kernel 5.15

Hello AD Community,

I'm currently working with the AD7124-8 ADC on a custom board and encountering an issue. The driver loads successfully and the device tree configuration seems to be correct. However, when I attempt to read from the raw data files (e.g., /sys/bus/iio/devices/iio:device0/in_voltage11-voltage0_raw), I consistently receive an Input/output error.

Device Tree for reference:

ad7124_mclk: oscillator {
compatible = "fixed-clock";
#clock-cells = <0>;
clock-frequency = <614400>;
//clock-frequency = <8192000>;
};

adc@0 {
compatible = "adi,ad7124-8";
reg = <0>;
spi-max-frequency = <5000000>;
interrupts = <25 2>;
interrupt-parent = <&gpio5>;
clocks = <&ad7124_mclk>;
clock-names = "mclk";
syncreset-gpios = <&pca9539 15 GPIO_ACTIVE_HIGH>;

spi-cpol;
spi-cpha;

#address-cells = <1>;
#size-cells = <0>;

channel@0 {
reg = <0>;
diff-channels = <0 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@1 {
reg = <1>;
diff-channels = <1 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@2 {
reg = <2>;
diff-channels = <2 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@3 {
reg = <3>;
diff-channels = <3 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@4 {
reg = <4>;
diff-channels = <4 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@5 {
reg = <5>;
diff-channels = <5 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@6 {
reg = <6>;
diff-channels = <6 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@7 {
reg = <7>;
diff-channels = <7 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@8 {
reg = <8>;
diff-channels = <8 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@9 {
reg = <9>;
diff-channels = <9 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@10 {
reg = <10>;
diff-channels = <10 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@11 {
reg = <11>;
diff-channels = <11 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@12 {
reg = <12>;
diff-channels = <12 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@13 {
reg = <13>;
diff-channels = <13 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@14 {
reg = <14>;
diff-channels = <14 0>;
bipolar = <0>;
adi,buffered-positive;
};

channel@15 {
reg = <15>;
diff-channels = <15 0>;
bipolar = <0>;
adi,buffered-positive;
};
};
};

Observations:

The driver initializes successfully

Despite successful initialization, attempting to read the raw data from the ADC input channels results in an Input/output error.

root@target:/sys/bus/iio/devices/iio:device0# cat in_voltage11-voltage0_raw
cat: in_voltage11-voltage0_raw: Input/output error

Request:

I’m seeking advice on what could be causing this issue. Is there something specific in the configuration or hardware setup that I might be missing? Any guidance or suggestions for additional debugging steps would be greatly appreciated.

Thank you in advance for your support.

Parents
  • Hi  ,

    You can check this example ad7124-4 device tree where the channels used are single-ended: https://github.com/analogdevicesinc/linux/blob/rpi-5.4.y/arch/arm/boot/dts/overlays/rpi-ad7124-overlay.dts

    /dts-v1/;
    /plugin/;
    
    / {
    	compatible = "brcm,bcm2835", "brcm,bcm2708", "brcm,bcm2709";
    
    	fragment@0 {
    		target-path = "/";
    		__overlay__ {
    			vref: fixedregulator@0 {
    				compatible = "regulator-fixed";
    				regulator-name = "fixed-supply";
    				regulator-min-microvolt = <2500000>;
    				regulator-max-microvolt = <2500000>;
    				regulator-boot-on;
    			};
    		};
    	};
    
    	fragment@1 {
    		target-path = "/";
    		__overlay__ {
    			clocks {
    				ad7124_mclk: clock@0 {
    					#clock-cells = <0>;
    					compatible = "fixed-clock";
    					clock-frequency = <614400>;
    				};
    			};
    		};
    	};
    
    	fragment@2 {
    		target = <&spi0>;
    		__overlay__ {
    			#address-cells = <1>;
    			#size-cells = <0>;
    			status = "okay";
    
    			ad7124@0 {
    				compatible = "adi,ad7124-4";
    				reg = <0>;
    				spi-max-frequency = <5000000>;
    				interrupts = <25 2>;
    				interrupt-parent = <&gpio>;
    				refin1-supply = <&vref>;
    				clocks = <&ad7124_mclk>;
    				clock-names = "mclk";
    
    				#address-cells = <1>;
    				#size-cells = <0>;
    
    				channel@0 {
    					reg = <0>;
    					diff-channels = <0 19>;
    					adi,reference-select = <0>;
    				};
    
    				channel@1 {
    					reg = <1>;
    					diff-channels = <1 19>;
    					adi,reference-select = <0>;
    				};
    
    				channel@2 {
    					reg = <2>;
    					diff-channels = <2 19>;
    					adi,reference-select = <0>;
    				};
    
    				channel@3 {
    					reg = <3>;
    					diff-channels = <3 19>;
    					adi,reference-select = <0>;
    				};
    
    				channel@4 {
    					reg = <4>;
    					diff-channels = <4 19>;
    					adi,reference-select = <0>;
    				};
    
    				channel@5 {
    					reg = <5>;
    					diff-channels = <5 19>;
    					adi,reference-select = <0>;
    				};
    
    				channel@6 {
    					reg = <6>;
    					diff-channels = <6 19>;
    					adi,reference-select = <0>;
    				};
    
    				channel@7 {
    					reg = <7>;
    					diff-channels = <7 19>;
    					adi,reference-select = <0>;
    				};
    			};
    		};
    	};
    
    	fragment@3 {
    		target = <&spidev0>;
    		__overlay__ {
    			status = "disabled";
    		};
    	};
    
    	fragment@4 {
    		target = <&spidev1>;
    		__overlay__ {
    			status = "disabled";
    		};
    	};
    };

    Note that to be able to create the single-ended channels, each ADC channel was paired with channel 19, which is a ground. And also note that this device tree example is compatible with the AD7124-4 which only has 4 channels. You can just adjust the number of channels for your AD7124-8.

    You can try to edit your existing device tree and let us know if this works for you.

    Regards,
    Andy

  • Thanks Andieo,

    This is reference I have taken and at first set 19 then set 0 as my AIN0 is grounded. The device tree I shared in this thread is the with this file reference only.

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.