Hi,
We have a two setups where we're using the MAX11617 device with libiio. With the first setup, we have an 8 channel device and we're able to buffer and read all 8 channels correctly. When we switch to the 12 channel device, using the exact same code, we are unable to read the same 8 channels correctly. What comes back appears to be just garbage. If I only enable one channel, the values in the buffer look to be correct. If I disable the buffer and read each channel, the values look correct in that case as well.
The strange thing is, the only thing that has changed is the device package. In both cases it's the MAX11617, it's just that in the second case there's 12 channels available rather than just 8.
Thanks,
Rory