Post Go back to editing

Libiio buffered measurements are not working with the Max11617 when the device has 12 channels.

Thread Summary

The user is experiencing issues reading 8 channels on a 12-channel MAX11617 ADC using libiio, with the buffer returning garbage values. The problem is likely due to the ADC's inability to perform clock stretching through an isolator with a monodirectional clock. The solution involves configuring the device to use an external clock or manually slowing down the I2C bus to prevent clock stretching. The MAX1363 driver may need to be modified to support external clock configuration.
AI Generated Content
Category: Software
Product Number: L
Software Version: 0.21

Hi,

We have a two setups where we're using the MAX11617 device with libiio. With the first setup, we have an 8 channel device and we're able to buffer and read all 8 channels correctly. When we switch to the 12 channel device, using the exact same code, we are unable to read the same 8 channels correctly. What comes back appears to be just garbage. If I only enable one channel, the values in the buffer look to be correct. If I disable the buffer and read each channel, the values look correct in that case as well. 

The strange thing is, the only thing that has changed is the device package. In both cases it's the MAX11617, it's just that in the second case there's 12 channels available rather than just 8.

Thanks,

Rory

Parents
  • Hi  ,

    Sorry about the late reply. When you said the only thing changed is the device package, it means you switched from an 8 channel MAX11617 to a 12 channel MAX11617? I am not aware of an 8 channel MAX11617. 8 channel devices in the family are MAX11614/MAX11615. Could you double check if that is the case?

    Thanks,

    Kevin

  • No worries,

    Now that you've mentioned it, I took another look at the data sheet and realized I was confused. The (N.C) markings on the QSOP package through me off. I thought the QSOP package we had on our test bench (first setup) had a reduced number of channels and our HW team had placed a different package with all channels connected on our board (second setup). Now I realize we have the QSOP on both setups and this has all 12 channels. So then the only difference between the two is that channels 8, 9 and 10 are connected to an analog stage.

  • Hi,

    When you said the only difference between the two setups now is that the problematic one has channel 8, 9, 10 connected to an analog stage. Are you trying to read from these three channels then?

    Previously you mentioned you are not able to read from the same 8 channels with the same code. Does that mean your problematic setup is still reading from the same 8 channels as your working setup but with channel 8~10 connected?

Reply
  • Hi,

    When you said the only difference between the two setups now is that the problematic one has channel 8, 9, 10 connected to an analog stage. Are you trying to read from these three channels then?

    Previously you mentioned you are not able to read from the same 8 channels with the same code. Does that mean your problematic setup is still reading from the same 8 channels as your working setup but with channel 8~10 connected?

Children