I would like to read data from the hardware and then perform some processing on it.
Here is my C code:
// SPDX-License-Identifier: GPL-2.0-or-later /* * libiio - AD9361 IIO streaming example * * Copyright (C) 2014 IABG mbH * Author: Michael Feilen <feilen_at_iabg.de> **/ #include <stdbool.h> #include <stdint.h> #include <string.h> #include <signal.h> #include <stdio.h> #include <iio.h> #include <math.h> /* helper macros */ #define MHZ(x) ((long long)(x*1000000.0 + .5)) #define GHZ(x) ((long long)(x*1000000000.0 + .5)) #define IIO_ENSURE(expr) { \ if (!(expr)) { \ (void) fprintf(stderr, "assertion failed (%s:%d)\n", __FILE__, __LINE__); \ (void) abort(); \ } \ } /* RX is input, TX is output */ enum iodev { RX, TX }; /* common RX and TX streaming params */ struct stream_cfg { long long bw_hz; // Analog banwidth in Hz long long fs_hz; // Baseband sample rate in Hz long long lo_hz; // Local oscillator frequency in Hz const char* rfport; // Port name }; /* static scratch mem for strings */ static char tmpstr[64]; /* IIO structs required for streaming */ static struct iio_context *ctx = NULL; static struct iio_channel *rx0_i = NULL; static struct iio_channel *rx0_q = NULL; static struct iio_channel *tx0_i = NULL; static struct iio_channel *tx0_q = NULL; static struct iio_buffer *rxbuf = NULL; static struct iio_buffer *txbuf = NULL; static bool stop; /* cleanup and exit */ static void shutdown(void) { printf("* Destroying buffers\n"); if (rxbuf) { iio_buffer_destroy(rxbuf); } if (txbuf) { iio_buffer_destroy(txbuf); } printf("* Disabling streaming channels\n"); if (rx0_i) { iio_channel_disable(rx0_i); } if (rx0_q) { iio_channel_disable(rx0_q); } if (tx0_i) { iio_channel_disable(tx0_i); } if (tx0_q) { iio_channel_disable(tx0_q); } printf("* Destroying context\n"); if (ctx) { iio_context_destroy(ctx); } exit(0); } static void handle_sig(int sig) { printf("Waiting for process to finish... Got signal %d\n", sig); stop = true; } /* check return value of attr_write function */ static void errchk(int v, const char* what) { if (v < 0) { fprintf(stderr, "Error %d writing to channel \"%s\"\nvalue may not be supported.\n", v, what); shutdown(); } } /* write attribute: long long int */ static void wr_ch_lli(struct iio_channel *chn, const char* what, long long val) { errchk(iio_channel_attr_write_longlong(chn, what, val), what); } /* write attribute: string */ static void wr_ch_str(struct iio_channel *chn, const char* what, const char* str) { errchk(iio_channel_attr_write(chn, what, str), what); } /* helper function generating channel names */ static char* get_ch_name(const char* type, int id) { snprintf(tmpstr, sizeof(tmpstr), "%s%d", type, id); return tmpstr; } /* returns ad9361 phy device */ static struct iio_device* get_ad9361_phy(void) { struct iio_device *dev = iio_context_find_device(ctx, "ad9361-phy"); IIO_ENSURE(dev && "No ad9361-phy found"); return dev; } /* finds AD9361 streaming IIO devices */ static bool get_ad9361_stream_dev(enum iodev d, struct iio_device **dev) { switch (d) { case TX: *dev = iio_context_find_device(ctx, "cf-ad9361-dds-core-lpc"); return *dev != NULL; case RX: *dev = iio_context_find_device(ctx, "cf-ad9361-lpc"); return *dev != NULL; default: IIO_ENSURE(0); return false; } } /* finds AD9361 streaming IIO channels */ static bool get_ad9361_stream_ch(enum iodev d, struct iio_device *dev, int chid, struct iio_channel **chn) { *chn = iio_device_find_channel(dev, get_ch_name("voltage", chid), d == TX); if (!*chn) *chn = iio_device_find_channel(dev, get_ch_name("altvoltage", chid), d == TX); return *chn != NULL; } /* finds AD9361 phy IIO configuration channel with id chid */ static bool get_phy_chan(enum iodev d, int chid, struct iio_channel **chn) { switch (d) { case RX: *chn = iio_device_find_channel(get_ad9361_phy(), get_ch_name("voltage", chid), false); return *chn != NULL; case TX: *chn = iio_device_find_channel(get_ad9361_phy(), get_ch_name("voltage", chid), true); return *chn != NULL; default: IIO_ENSURE(0); return false; } } /* finds AD9361 local oscillator IIO configuration channels */ static bool get_lo_chan(enum iodev d, struct iio_channel **chn) { switch (d) { // LO chan is always output, i.e. true case RX: *chn = iio_device_find_channel(get_ad9361_phy(), get_ch_name("altvoltage", 0), true); return *chn != NULL; case TX: *chn = iio_device_find_channel(get_ad9361_phy(), get_ch_name("altvoltage", 1), true); return *chn != NULL; default: IIO_ENSURE(0); return false; } } /* applies streaming configuration through IIO */ bool cfg_ad9361_streaming_ch(struct stream_cfg *cfg, enum iodev type, int chid) { struct iio_channel *chn = NULL; // Configure phy and lo channels printf("* Acquiring AD9361 phy channel %d\n", chid); if (!get_phy_chan(type, chid, &chn)) { return false; } wr_ch_str(chn, "rf_port_select", cfg->rfport); wr_ch_lli(chn, "rf_bandwidth", cfg->bw_hz); wr_ch_lli(chn, "sampling_frequency", cfg->fs_hz); // Configure LO channel printf("* Acquiring AD9361 %s lo channel\n", type == TX ? "TX" : "RX"); if (!get_lo_chan(type, &chn)) { return false; } wr_ch_lli(chn, "frequency", cfg->lo_hz); return true; } /* simple configuration and streaming */ /* usage: * Default context, assuming local IIO devices, i.e., this script is run on ADALM-Pluto for example $./a.out * URI context, find out the uri by typing `iio_info -s` at the command line of the host PC $./a.out usb:x.x.x */ int main (int argc, char **argv) { // Streaming devices struct iio_device *tx; struct iio_device *rx; // RX and TX sample counters size_t nrx = 0; size_t ntx = 0; // user variables int a = 0; int b = 0; // Stream configurations struct stream_cfg rxcfg; struct stream_cfg txcfg; // Listen to ctrl+c and IIO_ENSURE signal(SIGINT, handle_sig); // RX stream config rxcfg.bw_hz = MHZ(40); // 2 MHz rf bandwidth rxcfg.fs_hz = MHZ(60); // 2.5 MS/s rx sample rate rxcfg.lo_hz = GHZ(0.35); // 2.5 GHz rf frequency rxcfg.rfport = "A_BALANCED"; // port A (select for rf freq.) // TX stream config txcfg.bw_hz = MHZ(40); // 1.5 MHz rf bandwidth txcfg.fs_hz = MHZ(60); // 2.5 MS/s tx sample rate txcfg.lo_hz = GHZ(0.35); // 2.5 GHz rf frequency txcfg.rfport = "A"; // port A (select for rf freq.) printf("* Acquiring IIO context\n"); if (argc == 1) { IIO_ENSURE((ctx = iio_create_default_context()) && "No context"); } else if (argc == 2) { IIO_ENSURE((ctx = iio_create_context_from_uri(argv[1])) && "No context"); } IIO_ENSURE(iio_context_get_devices_count(ctx) > 0 && "No devices"); printf("* Acquiring AD9361 streaming devices\n"); IIO_ENSURE(get_ad9361_stream_dev(TX, &tx) && "No tx dev found"); IIO_ENSURE(get_ad9361_stream_dev(RX, &rx) && "No rx dev found"); printf("* Configuring AD9361 for streaming\n"); IIO_ENSURE(cfg_ad9361_streaming_ch(&rxcfg, RX, 0) && "RX port 0 not found"); IIO_ENSURE(cfg_ad9361_streaming_ch(&txcfg, TX, 0) && "TX port 0 not found"); printf("* Initializing AD9361 IIO streaming channels\n"); IIO_ENSURE(get_ad9361_stream_ch(RX, rx, 0, &rx0_i) && "RX chan i not found"); IIO_ENSURE(get_ad9361_stream_ch(RX, rx, 1, &rx0_q) && "RX chan q not found"); IIO_ENSURE(get_ad9361_stream_ch(TX, tx, 0, &tx0_i) && "TX chan i not found"); IIO_ENSURE(get_ad9361_stream_ch(TX, tx, 1, &tx0_q) && "TX chan q not found"); printf("* Enabling IIO streaming channels\n"); iio_channel_enable(rx0_i); iio_channel_enable(rx0_q); iio_channel_enable(tx0_i); iio_channel_enable(tx0_q); printf("* Creating non-cyclic IIO buffers with 1 MiS\n"); rxbuf = iio_device_create_buffer(rx, 2048, false); if (!rxbuf) { perror("Could not create RX buffer"); shutdown(); } /*txbuf = iio_device_create_buffer(tx, 1024*1024, false); if (!txbuf) { perror("Could not create TX buffer"); shutdown(); }*/ printf("* Starting IO streaming (press CTRL+C to cancel)\n"); while (!stop) { ssize_t nbytes_rx, nbytes_tx; char *p_dat, *p_end; ptrdiff_t p_inc; // Refill RX buffer nbytes_rx = iio_buffer_refill(rxbuf); if (nbytes_rx < 0) { printf("Error refilling buf %d\n",(int) nbytes_rx); shutdown(); } // READ: Get pointers to RX buf and read IQ from RX buf port 0 p_inc = iio_buffer_step(rxbuf); p_end = iio_buffer_end(rxbuf); a = 0; for (p_dat = (char *)iio_buffer_first(rxbuf, rx0_i); p_dat < p_end; p_dat += p_inc) { // Example: swap I and Q const int16_t i = ((int16_t*)p_dat)[0]; // Real (I) const int16_t q = ((int16_t*)p_dat)[1]; // Imag (Q) a++; int abs = sqrt( (i*i) + (q*q) ); if( abs > 20) printf("\tabs:%d,\t a0:%d,\t a1:%d,\t b:%d\n", abs, a, a, b); if( b == 100) shutdown(); } //shutdown(); b++; } shutdown(); return 0; }
When I try to print the data on screen the iio_buffer_refill loses data in the process. My DMA size : 128 MB; CMA 256 MB. can it be done???