Post Go back to editing

Qusestion about MAX96724(MAX9296A) Driver

Thread Summary

The user inquires about using a custom image sensor with a MAX9295 serializer and MAX9296A deserializer on a Raspberry Pi 5, with the MIPI ADAPTER AD-GMSLCAMRPI-ADP. The final answer confirms that a V4L2 sensor driver is required for the custom sensor, and suggests contacting the sensor vendor for a compatible driver or implementing a basic V4L2 driver. The MAX9296A driver for Raspberry Pi is available, but the sensor driver must be platform-agnostic to work.
AI Generated Content
Category: Software
Product Number: MAX96724R

I wanna ask about driver structure for max9296A/MAX96724 Deserializer board

My setup

Analog Device have an example about MAX96724+IMX219+Raspberry4.

Unfortunately, my sensor has no driver for raspberry PI.

"Do I need to develop sensor driver? or i could get image by 9296A and deserializer driver?"

P.S.

  1. MAX9296A Driver for raspberry
  2. Jetson+9296 Guide

Thread Notes