Hello,
Not sure if this is the best place to post, but I will give it a try. I am trying to get FMCOMMS5 working using external oscillator from ADF5355. I have compiled both Kuiper Linux and Petalinux with the device tree called "zynqmp-zcu102-rev10-ad9361-fmcomms5-ext-lo-adf5355". I am using IIO scope to set parameters. It looks like ADF5355 gets written, but I am not seeing any output from LO. I checked voltages on the board, and they all look good. I am also not seeing anything at the connector either. I am using REV C FMCOMMS5, and visually it looks like it is soldered to use ADF5355 as the external LO. What kind of registers, messages or test points I can look into to find if the ADF5355 is working correctly? Did anyone else have this issue with the external oscillator before?
Thank you in advance,
Vladimir