Post Go back to editing

FMCOMMS5 + ZC702, Linux Drivers, IIO-OSC Calibration crashes

Category: Software
Software Version: Win 10

Hi,

I am using FMCOMMS5 + ZC702 with Linux Drivers and I am streaming data via Ethernet to IIO-OSC and Matlab on a Windows 10 PC. I am using the newest version of IIO-Osc and Linux on the ZC702, also all tools and everything was updated just a few days ago. I have these problems/questions:

1.) I do exactly as you describe it here: https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms5-ebz/phase-sync , with SMA connectors between each TX and RX-port (I also tried it with a 4 port splitter and a Pluto-SDR and with an antenna array too) but still in 80% of the case IIO-OSC simply crashes during the calibration. Is there a remedy for this?

2.) I would like to do the calibration and MCS in Matlab using the Transceiver-Toolbox, what are the IIO-commands I need to accomplish this? In IIO-Osc it is possible to set the phase shift for each RX-Channel (I guess the phase shift is then done on the board itself?), I also need the command for this please.

3.) Sometimes the received samples in IIO-Osc of a few channels are simply some random constant value, see here:

But I never have this problem with Matlab.

   

Thank you very much!

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.