Post Go back to editing

Raspbian Bookworm to Kuiper (-like) Linux OS

Thread Summary

The user is building a prototype using an AD7124 or AD4130 RTD measuring board and wants to use vanilla Raspbian with the necessary additions to interface with the ADC. The final answer provides links to Kuiper Linux resources and a GitHub repository for building the kernel, as well as a downloadable image. The user expressed a preference for keeping vanilla Raspbian and adding only the required modules.
AI Generated Content
Category: Software
Product Number: AD7124-4
Software Version: None

Hello,

Kuiper Linux is used to evaluate ADI devices using a Raspberry Pi.

I am building a prototype that will include an AD7124 or AD4130 RTD measuring board and also some other devices.

I would like to use the vanilla Raspbian as an starting point and add whatever is needed to interface with the ADC.

Is there a page listing what is needed to run some of the evaluation tools on a fresh Raspbian OS?

Enable IIO in kernel, etc ?

Modules to load?

ADI drivers?

Libraries needed?

Repos?

Pyadi-IIO, etc?

Thank you for your help.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.