Post Go back to editing

AD9364 does not transmit any signal

Category: Hardware
Product Number: ADRV9364

Hi,

I am using the ADRV9364-Z7020 board with the transceiver configured in CMOS mode, single data rate, dual port, half duplex. In TDD mode, I see that the AD9364 correctly moves into TX state, but no signal is produced from the RF ports, although data ports and TX_FRAME are driven by the Zynq.

What have I missed?

Thank you in advance for your support.

Thread Notes

Parents
  • Can you check using internal BIST that whether you are able to transmit the data in TX state? Refer to the below link for BIST config:

     AD936x Built in Self Test (BIST)  

  • Thank you for your prompt response. I have tried using the BIST but unfortunately I cannot get any signal from the AD9364. The configuration parameters are pretty much the same as the no-OS reference design. Any other suggestion?

    AD9361_InitParam default_init_param = {
      /* Device selection */
      ID_AD9364,  // dev_sel
      /* Reference Clock */
      40000000UL, //reference_clk_rate
      /* Base Configuration */
      0,    //two_rx_two_tx_mode_enable *** adi,2rx-2tx-mode-enable
      1,    //one_rx_one_tx_mode_use_rx_num *** adi,1rx-1tx-mode-use-rx-num
      1,    //one_rx_one_tx_mode_use_tx_num *** adi,1rx-1tx-mode-use-tx-num
      0,    //frequency_division_duplex_mode_enable *** adi,frequency-division-duplex-mode-enable
      0,    //frequency_division_duplex_independent_mode_enable *** adi,frequency-division-duplex-independent-mode-enable
      0,    //tdd_use_dual_synth_mode_enable *** adi,tdd-use-dual-synth-mode-enable
      0,    //tdd_skip_vco_cal_enable *** adi,tdd-skip-vco-cal-enable
      0,    //tx_fastlock_delay_ns *** adi,tx-fastlock-delay-ns
      0,    //rx_fastlock_delay_ns *** adi,rx-fastlock-delay-ns
      0,    //rx_fastlock_pincontrol_enable *** adi,rx-fastlock-pincontrol-enable
      0,    //tx_fastlock_pincontrol_enable *** adi,tx-fastlock-pincontrol-enable
      0,    //external_rx_lo_enable *** adi,external-rx-lo-enable
      0,    //external_tx_lo_enable *** adi,external-tx-lo-enable
      5,    //dc_offset_tracking_update_event_mask *** adi,dc-offset-tracking-update-event-mask
      6,    //dc_offset_attenuation_high_range *** adi,dc-offset-attenuation-high-range
      5,    //dc_offset_attenuation_low_range *** adi,dc-offset-attenuation-low-range
      0x28, //dc_offset_count_high_range *** adi,dc-offset-count-high-range
      0x32, //dc_offset_count_low_range *** adi,dc-offset-count-low-range
      0,    //split_gain_table_mode_enable *** adi,split-gain-table-mode-enable
      MAX_SYNTH_FREF, //trx_synthesizer_target_fref_overwrite_hz *** adi,trx-synthesizer-target-fref-overwrite-hz
      0,    // qec_tracking_slow_mode_enable *** adi,qec-tracking-slow-mode-enable
      /* ENSM Control */
      0,    //ensm_enable_pin_pulse_mode_enable *** adi,ensm-enable-pin-pulse-mode-enable
      1,    //ensm_enable_txnrx_control_enable *** adi,ensm-enable-txnrx-control-enable
      /* LO Control */
      2400000000UL, //rx_synthesizer_frequency_hz *** adi,rx-synthesizer-frequency-hz
      2400000000UL, //tx_synthesizer_frequency_hz *** adi,tx-synthesizer-frequency-hz
      1,        //tx_lo_powerdown_managed_enable *** adi,tx-lo-powerdown-managed-enable
      /* Rate & BW Control */
      {983040000, 245760000, 122880000, 61440000, 30720000, 30720000},// rx_path_clock_frequencies[6] *** adi,rx-path-clock-frequencies
      {983040000, 122880000, 122880000, 61440000, 30720000, 30720000},// tx_path_clock_frequencies[6] *** adi,tx-path-clock-frequencies
      18000000,//rf_rx_bandwidth_hz *** adi,rf-rx-bandwidth-hz
      18000000,//rf_tx_bandwidth_hz *** adi,rf-tx-bandwidth-hz
      /* RF Port Control */
      0,    //rx_rf_port_input_select *** adi,rx-rf-port-input-select
      0,    //tx_rf_port_input_select *** adi,tx-rf-port-input-select
      /* TX Attenuation Control */
      10000,  //tx_attenuation_mdB *** adi,tx-attenuation-mdB
      0,    //update_tx_gain_in_alert_enable *** adi,update-tx-gain-in-alert-enable
      /* Reference Clock Control */
      0,    //xo_disable_use_ext_refclk_enable *** adi,xo-disable-use-ext-refclk-enable
      {8, 5920},  //dcxo_coarse_and_fine_tune[2] *** adi,dcxo-coarse-and-fine-tune
      CLKOUT_DISABLE, //clk_output_mode_select *** adi,clk-output-mode-select
      /* Gain Control */
      2,    //gc_rx1_mode *** adi,gc-rx1-mode
      2,    //gc_rx2_mode *** adi,gc-rx2-mode
      58,   //gc_adc_large_overload_thresh *** adi,gc-adc-large-overload-thresh
      4,    //gc_adc_ovr_sample_size *** adi,gc-adc-ovr-sample-size
      47,   //gc_adc_small_overload_thresh *** adi,gc-adc-small-overload-thresh
      8192, //gc_dec_pow_measurement_duration *** adi,gc-dec-pow-measurement-duration
      0,    //gc_dig_gain_enable *** adi,gc-dig-gain-enable
      800,  //gc_lmt_overload_high_thresh *** adi,gc-lmt-overload-high-thresh
      704,  //gc_lmt_overload_low_thresh *** adi,gc-lmt-overload-low-thresh
      24,   //gc_low_power_thresh *** adi,gc-low-power-thresh
      15,   //gc_max_dig_gain *** adi,gc-max-dig-gain
      0,    //gc_use_rx_fir_out_for_dec_pwr_meas_enable *** adi,gc-use-rx-fir-out-for-dec-pwr-meas-enable
      /* Gain MGC Control */
      2,    //mgc_dec_gain_step *** adi,mgc-dec-gain-step
      2,    //mgc_inc_gain_step *** adi,mgc-inc-gain-step
      0,    //mgc_rx1_ctrl_inp_enable *** adi,mgc-rx1-ctrl-inp-enable
      0,    //mgc_rx2_ctrl_inp_enable *** adi,mgc-rx2-ctrl-inp-enable
      0,    //mgc_split_table_ctrl_inp_gain_mode *** adi,mgc-split-table-ctrl-inp-gain-mode
      /* Gain AGC Control */
      10,   //agc_adc_large_overload_exceed_counter *** adi,agc-adc-large-overload-exceed-counter
      2,    //agc_adc_large_overload_inc_steps *** adi,agc-adc-large-overload-inc-steps
      0,    //agc_adc_lmt_small_overload_prevent_gain_inc_enable *** adi,agc-adc-lmt-small-overload-prevent-gain-inc-enable
      10,   //agc_adc_small_overload_exceed_counter *** adi,agc-adc-small-overload-exceed-counter
      4,    //agc_dig_gain_step_size *** adi,agc-dig-gain-step-size
      3,    //agc_dig_saturation_exceed_counter *** adi,agc-dig-saturation-exceed-counter
      1000, // agc_gain_update_interval_us *** adi,agc-gain-update-interval-us
      0,    //agc_immed_gain_change_if_large_adc_overload_enable *** adi,agc-immed-gain-change-if-large-adc-overload-enable
      0,    //agc_immed_gain_change_if_large_lmt_overload_enable *** adi,agc-immed-gain-change-if-large-lmt-overload-enable
      10,   //agc_inner_thresh_high *** adi,agc-inner-thresh-high
      1,    //agc_inner_thresh_high_dec_steps *** adi,agc-inner-thresh-high-dec-steps
      12,   //agc_inner_thresh_low *** adi,agc-inner-thresh-low
      1,    //agc_inner_thresh_low_inc_steps *** adi,agc-inner-thresh-low-inc-steps
      10,   //agc_lmt_overload_large_exceed_counter *** adi,agc-lmt-overload-large-exceed-counter
      2,    //agc_lmt_overload_large_inc_steps *** adi,agc-lmt-overload-large-inc-steps
      10,   //agc_lmt_overload_small_exceed_counter *** adi,agc-lmt-overload-small-exceed-counter
      5,    //agc_outer_thresh_high *** adi,agc-outer-thresh-high
      2,    //agc_outer_thresh_high_dec_steps *** adi,agc-outer-thresh-high-dec-steps
      18,   //agc_outer_thresh_low *** adi,agc-outer-thresh-low
      2,    //agc_outer_thresh_low_inc_steps *** adi,agc-outer-thresh-low-inc-steps
      1,    //agc_attack_delay_extra_margin_us; *** adi,agc-attack-delay-extra-margin-us
      0,    //agc_sync_for_gain_counter_enable *** adi,agc-sync-for-gain-counter-enable
      /* Fast AGC */
      64,   //fagc_dec_pow_measuremnt_duration ***  adi,fagc-dec-pow-measurement-duration
      260,  //fagc_state_wait_time_ns ***  adi,fagc-state-wait-time-ns
      /* Fast AGC - Low Power */
      0,    //fagc_allow_agc_gain_increase ***  adi,fagc-allow-agc-gain-increase-enable
      5,    //fagc_lp_thresh_increment_time ***  adi,fagc-lp-thresh-increment-time
      1,    //fagc_lp_thresh_increment_steps ***  adi,fagc-lp-thresh-increment-steps
      /* Fast AGC - Lock Level (Lock Level is set via slow AGC inner high threshold) */
      1,    //fagc_lock_level_lmt_gain_increase_en ***  adi,fagc-lock-level-lmt-gain-increase-enable
      5,    //fagc_lock_level_gain_increase_upper_limit ***  adi,fagc-lock-level-gain-increase-upper-limit
      /* Fast AGC - Peak Detectors and Final Settling */
      1,    //fagc_lpf_final_settling_steps ***  adi,fagc-lpf-final-settling-steps
      1,    //fagc_lmt_final_settling_steps ***  adi,fagc-lmt-final-settling-steps
      3,    //fagc_final_overrange_count ***  adi,fagc-final-overrange-count
      /* Fast AGC - Final Power Test */
      0,    //fagc_gain_increase_after_gain_lock_en ***  adi,fagc-gain-increase-after-gain-lock-enable
      /* Fast AGC - Unlocking the Gain */
      0,    //fagc_gain_index_type_after_exit_rx_mode ***  adi,fagc-gain-index-type-after-exit-rx-mode
      1,    //fagc_use_last_lock_level_for_set_gain_en ***  adi,fagc-use-last-lock-level-for-set-gain-enable
      1,    //fagc_rst_gla_stronger_sig_thresh_exceeded_en ***  adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable
      5,    //fagc_optimized_gain_offset ***  adi,fagc-optimized-gain-offset
      10,   //fagc_rst_gla_stronger_sig_thresh_above_ll ***  adi,fagc-rst-gla-stronger-sig-thresh-above-ll
      1,    //fagc_rst_gla_engergy_lost_sig_thresh_exceeded_en ***  adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable
      1,    //fagc_rst_gla_engergy_lost_goto_optim_gain_en ***  adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable
      10,   //fagc_rst_gla_engergy_lost_sig_thresh_below_ll ***  adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll
      8,    //fagc_energy_lost_stronger_sig_gain_lock_exit_cnt ***  adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt
      1,    //fagc_rst_gla_large_adc_overload_en ***  adi,fagc-rst-gla-large-adc-overload-enable
      1,    //fagc_rst_gla_large_lmt_overload_en ***  adi,fagc-rst-gla-large-lmt-overload-enable
      0,    //fagc_rst_gla_en_agc_pulled_high_en ***  adi,fagc-rst-gla-en-agc-pulled-high-enable
      0,    //fagc_rst_gla_if_en_agc_pulled_high_mode ***  adi,fagc-rst-gla-if-en-agc-pulled-high-mode
      64,   //fagc_power_measurement_duration_in_state5 ***  adi,fagc-power-measurement-duration-in-state5
      2,    //fagc_large_overload_inc_steps *** adi,fagc-adc-large-overload-inc-steps
      /* RSSI Control */
      1,    //rssi_delay *** adi,rssi-delay
      1000, //rssi_duration *** adi,rssi-duration
      3,    //rssi_restart_mode *** adi,rssi-restart-mode
      0,    //rssi_unit_is_rx_samples_enable *** adi,rssi-unit-is-rx-samples-enable
      1,    //rssi_wait *** adi,rssi-wait
      /* Aux ADC Control */
      256,  //aux_adc_decimation *** adi,aux-adc-decimation
      40000000UL, //aux_adc_rate *** adi,aux-adc-rate
      /* AuxDAC Control */
      1,    //aux_dac_manual_mode_enable ***  adi,aux-dac-manual-mode-enable
      0,    //aux_dac1_default_value_mV ***  adi,aux-dac1-default-value-mV
      0,    //aux_dac1_active_in_rx_enable ***  adi,aux-dac1-active-in-rx-enable
      0,    //aux_dac1_active_in_tx_enable ***  adi,aux-dac1-active-in-tx-enable
      0,    //aux_dac1_active_in_alert_enable ***  adi,aux-dac1-active-in-alert-enable
      0,    //aux_dac1_rx_delay_us ***  adi,aux-dac1-rx-delay-us
      0,    //aux_dac1_tx_delay_us ***  adi,aux-dac1-tx-delay-us
      0,    //aux_dac2_default_value_mV ***  adi,aux-dac2-default-value-mV
      0,    //aux_dac2_active_in_rx_enable ***  adi,aux-dac2-active-in-rx-enable
      0,    //aux_dac2_active_in_tx_enable ***  adi,aux-dac2-active-in-tx-enable
      0,    //aux_dac2_active_in_alert_enable ***  adi,aux-dac2-active-in-alert-enable
      0,    //aux_dac2_rx_delay_us ***  adi,aux-dac2-rx-delay-us
      0,    //aux_dac2_tx_delay_us ***  adi,aux-dac2-tx-delay-us
      /* Temperature Sensor Control */
      256,  //temp_sense_decimation *** adi,temp-sense-decimation
      1000, //temp_sense_measurement_interval_ms *** adi,temp-sense-measurement-interval-ms
      0xCE, //temp_sense_offset_signed *** adi,temp-sense-offset-signed
      1,    //temp_sense_periodic_measurement_enable *** adi,temp-sense-periodic-measurement-enable
      /* Control Out Setup */
      0xFF, //ctrl_outs_enable_mask *** adi,ctrl-outs-enable-mask
      0,    //ctrl_outs_index *** adi,ctrl-outs-index
      /* External LNA Control */
      0,    //elna_settling_delay_ns *** adi,elna-settling-delay-ns
      0,    //elna_gain_mdB *** adi,elna-gain-mdB
      0,    //elna_bypass_loss_mdB *** adi,elna-bypass-loss-mdB
      0,    //elna_rx1_gpo0_control_enable *** adi,elna-rx1-gpo0-control-enable
      0,    //elna_rx2_gpo1_control_enable *** adi,elna-rx2-gpo1-control-enable
      0,    //elna_gaintable_all_index_enable *** adi,elna-gaintable-all-index-enable
      /* Digital Interface Control */
      0,    //digital_interface_tune_skip_mode *** adi,digital-interface-tune-skip-mode
      0,    //digital_interface_tune_fir_disable *** adi,digital-interface-tune-fir-disable
      1,    //pp_tx_swap_enable *** adi,pp-tx-swap-enable
      1,    //pp_rx_swap_enable *** adi,pp-rx-swap-enable
      0,    //tx_channel_swap_enable *** adi,tx-channel-swap-enable
      0,    //rx_channel_swap_enable *** adi,rx-channel-swap-enable
      1,    //rx_frame_pulse_mode_enable *** adi,rx-frame-pulse-mode-enable
      0,    //two_t_two_r_timing_enable *** adi,2t2r-timing-enable
      0,    //invert_data_bus_enable *** adi,invert-data-bus-enable
      0,    //invert_data_clk_enable *** adi,invert-data-clk-enable
      0,    //fdd_alt_word_order_enable *** adi,fdd-alt-word-order-enable
      0,    //invert_rx_frame_enable *** adi,invert-rx-frame-enable
      0,    //fdd_rx_rate_2tx_enable *** adi,fdd-rx-rate-2tx-enable
      0,    //swap_ports_enable *** adi,swap-ports-enable
      1,    //single_data_rate_enable *** adi,single-data-rate-enable
      0,    //lvds_mode_enable *** adi,lvds-mode-enable
      1,    //half_duplex_mode_enable *** adi,half-duplex-mode-enable
      0,    //single_port_mode_enable *** adi,single-port-mode-enable
      0,    //full_port_enable *** adi,full-port-enable
      0,    //full_duplex_swap_bits_enable *** adi,full-duplex-swap-bits-enable
      0,    //delay_rx_data *** adi,delay-rx-data
      0,    //rx_data_clock_delay *** adi,rx-data-clock-delay
      4,    //rx_data_delay *** adi,rx-data-delay
      7,    //tx_fb_clock_delay *** adi,tx-fb-clock-delay
      0,    //tx_data_delay *** adi,tx-data-delay
    #ifdef ALTERA_PLATFORM
      300,  //lvds_bias_mV *** adi,lvds-bias-mV
    #else
      150,  //lvds_bias_mV *** adi,lvds-bias-mV
    #endif
      1,    //lvds_rx_onchip_termination_enable *** adi,lvds-rx-onchip-termination-enable
      0,    //rx1rx2_phase_inversion_en *** adi,rx1-rx2-phase-inversion-enable
      0xFF, //lvds_invert1_control *** adi,lvds-invert1-control
      0x0F, //lvds_invert2_control *** adi,lvds-invert2-control
      /* GPO Control */
      0,    //gpo_manual_mode_enable *** adi,gpo-manual-mode-enable
      0,    //gpo_manual_mode_enable_mask *** adi,gpo-manual-mode-enable-mask
      0,    //gpo0_inactive_state_high_enable *** adi,gpo0-inactive-state-high-enable
      0,    //gpo1_inactive_state_high_enable *** adi,gpo1-inactive-state-high-enable
      0,    //gpo2_inactive_state_high_enable *** adi,gpo2-inactive-state-high-enable
      0,    //gpo3_inactive_state_high_enable *** adi,gpo3-inactive-state-high-enable
      0,    //gpo0_slave_rx_enable *** adi,gpo0-slave-rx-enable
      0,    //gpo0_slave_tx_enable *** adi,gpo0-slave-tx-enable
      0,    //gpo1_slave_rx_enable *** adi,gpo1-slave-rx-enable
      0,    //gpo1_slave_tx_enable *** adi,gpo1-slave-tx-enable
      0,    //gpo2_slave_rx_enable *** adi,gpo2-slave-rx-enable
      0,    //gpo2_slave_tx_enable *** adi,gpo2-slave-tx-enable
      0,    //gpo3_slave_rx_enable *** adi,gpo3-slave-rx-enable
      0,    //gpo3_slave_tx_enable *** adi,gpo3-slave-tx-enable
      0,    //gpo0_rx_delay_us *** adi,gpo0-rx-delay-us
      0,    //gpo0_tx_delay_us *** adi,gpo0-tx-delay-us
      0,    //gpo1_rx_delay_us *** adi,gpo1-rx-delay-us
      0,    //gpo1_tx_delay_us *** adi,gpo1-tx-delay-us
      0,    //gpo2_rx_delay_us *** adi,gpo2-rx-delay-us
      0,    //gpo2_tx_delay_us *** adi,gpo2-tx-delay-us
      0,    //gpo3_rx_delay_us *** adi,gpo3-rx-delay-us
      0,    //gpo3_tx_delay_us *** adi,gpo3-tx-delay-us
      /* Tx Monitor Control */
      37000,  //low_high_gain_threshold_mdB *** adi,txmon-low-high-thresh
      0,    //low_gain_dB *** adi,txmon-low-gain
      24,   //high_gain_dB *** adi,txmon-high-gain
      0,    //tx_mon_track_en *** adi,txmon-dc-tracking-enable
      0,    //one_shot_mode_en *** adi,txmon-one-shot-mode-enable
      511,  //tx_mon_delay *** adi,txmon-delay
      8192, //tx_mon_duration *** adi,txmon-duration
      2,    //tx1_mon_front_end_gain *** adi,txmon-1-front-end-gain
      2,    //tx2_mon_front_end_gain *** adi,txmon-2-front-end-gain
      48,   //tx1_mon_lo_cm *** adi,txmon-1-lo-cm
      48,   //tx2_mon_lo_cm *** adi,txmon-2-lo-cm
      /* GPIO definitions */
      {
        .number = -1,
        .platform_ops = GPIO_OPS,
        .extra = GPIO_PARAM
      },    //gpio_resetb *** reset-gpios
      /* MCS Sync */
      {
        .number = -1,
        .platform_ops = GPIO_OPS,
        .extra = GPIO_PARAM
      },    //gpio_sync *** sync-gpios
    
      {
        .number = -1,
        .platform_ops = GPIO_OPS,
        .extra = GPIO_PARAM
      },    //gpio_cal_sw1 *** cal-sw1-gpios
    
      {
        .number = -1,
        .platform_ops = GPIO_OPS,
        .extra = GPIO_PARAM
      },    //gpio_cal_sw2 *** cal-sw2-gpios
    
      {
        .device_id = SPI_DEVICE_ID,
        .mode = NO_OS_SPI_MODE_1,
        .chip_select = SPI_CS,
        .platform_ops = SPI_OPS,
        .extra = SPI_PARAM
      },
    
      /* External LO clocks */
      NULL, //(*ad9361_rfpll_ext_recalc_rate)()
      NULL, //(*ad9361_rfpll_ext_round_rate)()
      NULL, //(*ad9361_rfpll_ext_set_rate)()
    #ifndef AXI_ADC_NOT_PRESENT
      &rx_adc_init, // *rx_adc_init
      &tx_dac_init,   // *tx_dac_init
    #endif
    };
  • Are you able to initialize the chip successfully in CMOS mode? If you change to LVDS mode, is it working?

    swap_ports_enable should be 0 (default value) in case of ad9364 device.

    Refer to the below links:

    https://github.com/analogdevicesinc/no-OS/pull/1591/commits/183356f9a985b2d6020c6911ac7c3b6067236c5e 

  • I set swap_ports_enable to 0, as in the code snippet I shared in the previous message. Then I tried both CMOS and LVDS mode, but using the BIST I still cannot get any signal. I believe there is no issue in the initialization since the ad9361_init() function returns successfully and the ENSM moves in TX state. It seems like something is powered down... any other suggestion?
    Thank you for your support.

  • Can you try initializing in FDD mode and then check with internal BIST, if you are able to see the data at the TX output?

    Also, readback the TX channel enable using the below register:

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.