Post Go back to editing

Cross compiling libiio from linux to windows

Category: Software
Product Number: libiio

Hello, 

I have a project with a cmakelist.txt that I cross compile to windows from ubuntu. This project depends on libiio and I know libiio is build also with cmake to allow cross compile. 

When I build it using x86_64-w64-mingw32 i get the message from cmake:

[build] CMake Error at extern/libiio/CMakeLists.txt:295 (message):
[build] Libusb >= 1.0.10 is required.
 
Which is understandable. I only have the libusb on my ubuntu, not for windows. But i found no documentation for this on the wiki, so here is the question:
how in my cmakelist.txt do I add the libusb windows dlls so cmake can see it and use it to build libiio?
Also i might just be missing the point and dont need them, if so can someone point me in the right direction?
Parents
  • Hello  , 


    Is there a particular reason for which you chose to cross-compile libiio?

    Instead, you can download the libiio Windows MinGW DLLs from here: github.com/.../libiio-0.25-gb6028fd-windows.zip

    Extract the archive and copy the Windows-MinGW-W64 and include folders to your project's SYSROOT location.

    Then,from your project's CMakeLists.txt , you can link your program to the libiio DLLs, by adding the following lines : 

    find_library(LIBIIO_LIBRARIES iio)
    find_path(LIBIIO_INCLUDE_DIRS iio.h)

    target_include_directories(your_target PUBLIC ${LIBIIO_INCLUDE_DIRS})
    target_link_libraries(your_target PUBLIC ${LIBIIO_LIBRARIES})

    Your add_executable call should be after the calls for find_library and find path and before the calls for target_include_directories and target_link_libraries

    Alternatively, you can leave the downloaded files where they are and tell cmake where to look for them : 

    find_library(LIBIIO_LIBRARIES iio HINTS "/path/to/Windows-MinGW-W64")
    find_path(LIBIIO_INCLUDE_DIRS iio.h HINTS "/path/to/include")

    If you choose this approach, you will also have to edit the ToolChain file used for compiling and set the following : 

    set(CMAKE_FIND_ROOT_PATH_MODE_LIBRARY BOTH)
    set(CMAKE_FIND_ROOT_PATH_MODE_INCLUDE BOTH)

    Let us know if this fixes your issue. 

    -- Cristina

Reply
  • Hello  , 


    Is there a particular reason for which you chose to cross-compile libiio?

    Instead, you can download the libiio Windows MinGW DLLs from here: github.com/.../libiio-0.25-gb6028fd-windows.zip

    Extract the archive and copy the Windows-MinGW-W64 and include folders to your project's SYSROOT location.

    Then,from your project's CMakeLists.txt , you can link your program to the libiio DLLs, by adding the following lines : 

    find_library(LIBIIO_LIBRARIES iio)
    find_path(LIBIIO_INCLUDE_DIRS iio.h)

    target_include_directories(your_target PUBLIC ${LIBIIO_INCLUDE_DIRS})
    target_link_libraries(your_target PUBLIC ${LIBIIO_LIBRARIES})

    Your add_executable call should be after the calls for find_library and find path and before the calls for target_include_directories and target_link_libraries

    Alternatively, you can leave the downloaded files where they are and tell cmake where to look for them : 

    find_library(LIBIIO_LIBRARIES iio HINTS "/path/to/Windows-MinGW-W64")
    find_path(LIBIIO_INCLUDE_DIRS iio.h HINTS "/path/to/include")

    If you choose this approach, you will also have to edit the ToolChain file used for compiling and set the following : 

    set(CMAKE_FIND_ROOT_PATH_MODE_LIBRARY BOTH)
    set(CMAKE_FIND_ROOT_PATH_MODE_INCLUDE BOTH)

    Let us know if this fixes your issue. 

    -- Cristina

Children