ADRV9002
Recommended for New Designs
The ADRV9002 is a highly integrated RF transceiver that has dual-channel transmitters, dual-channel receivers, integrated synthesizers, and digital signal...
Datasheet
ADRV9002 on Analog.com
I am testing MCS with EVAL-ADRV9002 and ZCU102.
UG-1828 has the following description and I figured that even with one ADRV9002 I would need to use MCS to phase match RX1 and RX2.
"MCS is needed when an application requires deterministic latency among datapaths within one ADRV9001 device or multiple ADRV9001 devices."
I have created a json file with MCS enabled.

I loaded the json file on IIO oscilloscope, MCS is now enabled, but the local oscillator of RX cannot be changed from 2400MHz.
(Local frequency could be changed when MCS is disabled.)

I am trying to run MCS using the following procedure, is there a mistake in the procedure?
1. load Json file with MCS enabled in IIO Oscilloscope.
2. Change the local frequency in IIO Oscilloscope.
3. control the MCS pin.
Best regards
hsato
M_Bugajski - Moved from Design Support ADRV9001 – ADRV9007 to Linux Software Drivers. Post date updated from Tuesday, February 27, 2024 12:07 AM UTC to Tuesday, February 27, 2024 4:02 PM UTC to reflect the move.
M_Bugajski - Moved from Design Support ADRV9001 – ADRV9007 to Linux Software Drivers. Post date updated from Tuesday, February 27, 2024 4:02 PM UTC to Tuesday, February 27, 2024 4:02 PM UTC to reflect the move.