Post Go back to editing

libiio Trigger-less mode

Category: Software
Product Number: libiio
Software Version: 0.23

Hello,
I am trying to use the libiio library to read data from an IMU (I am not experienced with the libiio library). I specifically want to read the buffer of the accelerometer of the IMU. However, the accelerometer does not offer any setting options for a trigger (no trigger available and no trigger file in the accelerometer directory). If I use the program iio_generic_buffer, the readout only works with the trigger-less-mode, i.e. options -A -g -c -1 . If I now use the program iio_readdev with the following options, iio_readdev -s 30 -b 256 iio::device1 I run into an error. Error:

WARNING: High-speed mode not enabled
ERROR: Error during buffer disable: Invalid argument

  • How can I avoid this error and what do I have to consider to fix this?
  • Is it even possible to read the buffer with libiio without a trigger?
  • And is it possible to read the device with the libiio library at all? If yes, could you show me an example.
  • And what does trigger less mode mean, I cannot find anything about this topic

Thanks you in advance!

Top Replies

  • Hi  ,

    May I ask what MUI you are currently using?

    As for the questions you've asked:

    1. The warning stems from the accelerometer lacking a trigger, hindering high-speed reading. The iio_readdev error…