Hello,
Greeting!
I am trying to configure AD9081+ZCU102 on the GNU Radio. My environment is: Virtual Machine of Ubuntu 20.04 on Windows, GNU Radio 3.8. But an error occurs, see below:
I have checked other similar question in the forum. The answer is usually the IP error. But I am sure the ip address on my ZCU102 is 169.254.183.161, because I can connect to it using this address on Matlab.
This is the result of "iio_info -s":
root@analog:~# iio_info -s Library version: 0.24 (git tag: accb7b5) Compiled with backends: local xml ip usb serial Available contexts: 0: 169.254.183.161 (AD-FMCOMMS2-EBZ on Stingray ZynqMP ZCU102 Rev1.0), serial=00045 [ip:analog.local] 1: (adar1000_csb_2_2, xud_control, adar1000_csb_1_4, axi-core-tdd, adar1000_csb_1_2, hmc7044, ams, axi-ad9081-tx-hpc, adar1000_c on Stingray ZynqMP ZCU102 Rev1.0) [local:]
Do you have any idea about my question? I would really appreciate it!
Best,
Dongyu