Hello.
I am testing with ADRV9002 and ZedBoard with transmit and receive looped back.
I tested with transmit local frequency as 1500.5 MHz and receive local frequency as 500 MHz.
I could see the aliasing of harmonics on the IIO oscilloscope.
Next, I changed the analog low-pass filter setting in TES from first order to second order, but there was no difference in the waveform.
I expected characteristics similar to Figures 138 and 139 in the ug-1828.
First Order with 27dB attenuation at 10^9Hz, and Second order with 60dB attenuation at 10^9Hz.
Do I need to make any other changes to the JSON file to enable the analog low pass filter?