Post Go back to editing

AD9986 + ZCU102 Abnomal Work

Thread Summary

The user encountered issues with the AD9986 not being recognized on a ZCU102 board using an SD card with AD9081 boot files. The solution involved re-downloading the latest ADI Kuiper image and ensuring the correct device tree and boot files were used, which resolved the unrecognized chip ID issue. The user also sought advice on configuring the AD9986 for a 6 GHz ADC sample rate and 2.4 GHz bandwidth, which required modifying the device tree to set the ADC frequency, decimation, and JESD mode.
AI Generated Content
Product Number: AD9986
Software Version: IIO-Oscilloscope - v0.16

Hi

   I have a one AD9986 EVAL Board and one ZCU102 Board. Refer to description of this website-https://wiki.analog.com/resources/eval/user-guides/ad9081_fmca_ebz/quickstart/zynqmp. I used the SD Card you provided to make ZCU102 boot. Boot mode choose from SD Card. When ZCU102 was fully started, I used the serial command to find the device, but I didn't find the device AD9986.  When I use IIO software, the list of devices is only HMC7044 and there is no AD9986. There is a print log.3288.ZCU102_print log.log

Thread Notes

Parents Reply
  • I want to increase the sampling frequency to make bandwidth reach 2GHz. I should use iio software to change sampling frequency by spi command or re-download the appropriate device tree and boot files.

    For these parts you can't change the sampling frequency from IIO. It's all done in the devicetree.

    The HMC7044 clocks are related, but your bandwidth depends on DAC rates, ADC rates and their interpolation/decimation factors.  

    -Michael

Children
  • Hi

    My project is collecting boardband digital sianal processing.Our intermediate frequency is 1.5Ghz and the bandwidth is 2G.

    Is there a device tree that can support ADC to sample 6G, decimate it into 2 complex outputs, and the bandwidth can reach 2.4GHz?

    If so, where i can download it?

    Thanks.

  • Sorry

    My project is collecting boardband digital sianal processing.Our intermediate frequency is 1.5Ghz and the bandwidth is 2G.

    Is there a device tree that can support ADC to sample 6G, decimate it into 2 complex outputs, and the bandwidth can reach 2.4GHz?

    Is there such a model for us to choose?

    Thanks.

  • I don't think we have such a use case drafted with a devicetree example.

    For AD9082 I'm pretty sure you could run ADC at 6G and then use decimate by 2 in the coarse DDC.

    That would give you 3G rate which should have 2.4G channel BW.

    And you can tune the main NCO to 1.5G.

    -Michael 

  • Can i get the mode that i want by modifying the device tree and boot file?

    If so, what should i do? 

  • You first need the user guide UG-1578.

    And select the JESD modes - you said you want to have 2 complex channels.

    So M=4, now you need to select a mode either from 204B or 204C and you also need to know how much lanes (L) you have/require. Number of bits (NP), etc.

    Also check that the required interpolation/decimation mode is available for a given mode.

    If you know all this, you can edit the devicetree.

    Set ADC/DAC frequency, enter the decimation/interpolation values and set the JESD mode.

    Please see here:

    https://wiki.analog.com/resources/tools-software/linux-drivers/iio-mxfe/ad9081#device_tree_customization

    -Michael

  • Hmm - with M=4 I think you need all 8 lanes and 204C encoding. Then your lane rate will be 24.750 Gbps.

  • Thanks, i will try it according to your method.If have any question, i will ask you again.

  • Hi

    I try to modify the system.dtb. Then open the software and find that it has no waveform. The Operation mode of the AD9986 what i need. As follow:

    ADC sample frequency is 6GHz.

    just one input channnel (channel ADC0).

    only enable CDDC1 and decimation=2, complex output, bypass FDDC, output data rate =3GSPS (I/Q).

    So it can achieve 2.44GHz Bandwidth analysis. 

    I just modeify the ADC part, and DAC part do not modify. Should I also modify DAC part?

    Part of the device tree information I modify is as below.  Thanks

                    adi,rx-adcs {
    					#size-cells = <0x00>;
    					#address-cells = <0x01>;
    					adi,adc-frequency-hz = <0x01 0x65a0bc00>;     
    
    					adi,main-data-paths {
    						#address-cells = <0x01>;
    						#size-cells = <0x00>;
    
    						adc@0 {
    							reg = <0x00>;
    							adi,decimation = <0x02>; (Modify Mark)
    							adi,nco-frequency-shift-hz = <0x00 0x3b9aca00>;
    							adi,nco-mode = <0x00>;
    						};
    
    						adc@1 {
    							reg = <0x01>;
    							adi,decimation = <0x02>;(Modify Mark)
    							adi,nco-frequency-shift-hz = <0x00 0x3b9aca00>;
    							adi,nco-mode = <0x00>;
    						};
    					};
    
    					adi,channelizer-paths {
    						#address-cells = <0x01>;
    						#size-cells = <0x00>;
    
    						channel@0 {
    							reg = <0x00>;
    							adi,decimation = <0x01>;
    							adi,gain = <0x800>;
    							adi,nco-frequency-shift-hz = <0x00 0x00>;
    							phandle = <0x22>;
    						};
    
    						channel@1 {
    							reg = <0x01>;
    							adi,decimation = <0x01>;
    							adi,gain = <0x800>;
    							adi,nco-frequency-shift-hz = <0x00 0x00>;
    							phandle = <0x23>;
    						};
    					};
    
    					adi,jesd-links {
    						#size-cells = <0x00>;
    						#address-cells = <0x01>;
    
    						link@0 {
    							reg = <0x00>;
    							adi,converter-select = <0x22 0x00 0x22 0x01 0x23 0x00 0x23 0x01>;
    							adi,logical-lane-mapping = <0x2000706 0x5040301>;
    							adi,link-mode = <0x12>;
    							adi,subclass = <0x01>;
    							adi,version = <0x01>;
    							adi,dual-link = <0x00>;
    							adi,converters-per-device = <0x02>;(Modify Mark)
    							adi,octets-per-frame = <0x01>;
    							adi,frames-per-multiframe = <0x20>;
    							adi,converter-resolution = <0x10>;
    							adi,bits-per-sample = <0x10>;
    							adi,control-bits-per-sample = <0x00>;
    							adi,lanes-per-device = <0x08>;
    							adi,samples-per-converter-per-frame = <0x02>;(Modify Mark)
    							adi,high-density = <0x01>;
    						};
    					};
    				};
    
    
            spi@ff050000 {
    			compatible = "cdns,spi-r1p6";
    			status = "okay";
    			interrupt-parent = <0x04>;
    			interrupts = <0x00 0x14 0x04>;
    			reg = <0x00 0xff050000 0x00 0x1000>;
    			clock-names = "ref_clk\0pclk";
    			#address-cells = <0x01>;
    			#size-cells = <0x00>;
    			power-domains = <0x0c 0x24>;
    			clocks = <0x03 0x3b 0x03 0x1f>;
    
    			hmc7044@0 {
    				#address-cells = <0x01>;
    				#size-cells = <0x00>;
    				#clock-cells = <0x01>;
    				compatible = "adi,hmc7044";
    				reg = <0x00>;
    				spi-max-frequency = <0xf4240>;
    				jesd204-device;
    				#jesd204-cells = <0x02>;
    				jesd204-sysref-provider;
    				adi,jesd204-max-sysref-frequency-hz = <0x1e8480>;
    				adi,pll1-clkin-frequencies = <0x7530000 0x1d4c000 0x00 0x00>;
    				adi,vcxo-frequency = <0x7530000>;
    				adi,pll1-loop-bandwidth-hz = <0xc8>;
    				adi,pll2-output-frequency = <0xb2d05e00>;
    				adi,sysref-timer-divider = <0x400>;
    				adi,pulse-generator-mode = <0x00>;
    				adi,clkin0-buffer-mode = <0x07>;
    				adi,clkin1-buffer-mode = <0x07>;
    				adi,oscin-buffer-mode = <0x15>;
    				adi,gpi-controls = <0x00 0x00 0x00 0x00>;
    				adi,gpo-controls = <0x37 0x33 0x00 0x00>;
    				clock-output-names = "hmc7044_out0\0hmc7044_out1\0hmc7044_out2\0hmc7044_out3\0hmc7044_out4\0hmc7044_out5\0hmc7044_out6\0hmc7044_out7\0hmc7044_out8\0hmc7044_out9\0hmc7044_out10\0hmc7044_out11\0hmc7044_out12\0hmc7044_out13";
    				phandle = <0x1d>;
    
    				channel@0 {
    					reg = <0x00>;
    					adi,extended-name = "CORE_CLK_RX";
    					adi,divider = <0x0c>;
    					adi,driver-mode = <0x02>;
    				};
    
    				channel@2 {
    					reg = <0x02>;
    					adi,extended-name = "DEV_REFCLK";
    					adi,divider = <0x0c>;
    					adi,driver-mode = <0x02>;
    				};
    
    				channel@3 {
    					reg = <0x03>;
    					adi,extended-name = "DEV_SYSREF";
    					adi,divider = <0x600>;
    					adi,driver-mode = <0x02>;
    					adi,jesd204-sysref-chan;
    				};
    
    				channel@6 {
    					reg = <0x06>;
    					adi,extended-name = "CORE_CLK_TX";
    					adi,divider = <0x0c>;
    					adi,driver-mode = <0x02>;
    				};
    
    				channel@8 {
    					reg = <0x08>;
    					adi,extended-name = "FPGA_REFCLK1";
    					adi,divider = <0x06>;
    					adi,driver-mode = <0x02>;
    				};
    
    				channel@10 {
    					reg = <0x0a>;
    					adi,extended-name = "CORE_CLK_RX_ALT";
    					adi,divider = <0x0c>;
    					adi,driver-mode = <0x02>;
    				};
    
    				channel@12 {
    					reg = <0x0c>;
    					adi,extended-name = "FPGA_REFCLK2";
    					adi,divider = <0x06>;
    					adi,driver-mode = <0x02>;
    				};
    
    				channel@13 {
    					reg = <0x0d>;
    					adi,extended-name = "FPGA_SYSREF";
    					adi,divider = <0x600>;
    					adi,driver-mode = <0x02>;
    					adi,jesd204-sysref-chan;
    				};
    			};
    		};

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.