Post Go back to editing

AD9986 + ZCU102 Abnomal Work

Thread Summary

The user encountered issues with the AD9986 not being recognized on a ZCU102 board using an SD card with AD9081 boot files. The solution involved re-downloading the latest ADI Kuiper image and ensuring the correct device tree and boot files were used, which resolved the unrecognized chip ID issue. The user also sought advice on configuring the AD9986 for a 6 GHz ADC sample rate and 2.4 GHz bandwidth, which required modifying the device tree to set the ADC frequency, decimation, and JESD mode.
AI Generated Content
Product Number: AD9986
Software Version: IIO-Oscilloscope - v0.16

Hi

   I have a one AD9986 EVAL Board and one ZCU102 Board. Refer to description of this website-https://wiki.analog.com/resources/eval/user-guides/ad9081_fmca_ebz/quickstart/zynqmp. I used the SD Card you provided to make ZCU102 boot. Boot mode choose from SD Card. When ZCU102 was fully started, I used the serial command to find the device, but I didn't find the device AD9986.  When I use IIO software, the list of devices is only HMC7044 and there is no AD9986. There is a print log.3288.ZCU102_print log.log

Thread Notes

Parents
  • Hi,

    Sorry, I got confused with this project, it appeared similar to another one and I thought we have this one in our repository, but we don't.

    The problem comes from the unrecognized chip ID which says there is no 9986, because you used the AD9081-FMCA-EBZ boot files, and the device tree for this is not expecting an AD9986 evaluation board. This is my assumption, but I am not sure regarding the software side.

    I will move this thread to the Linux Software Drivers forum for any thoughts from my colleagues, if these are compatible or not, while I check about the HDL.

    Best regards,
    Iulia

  • You using a very old image:

    Linux version 4.19.0-g17f4223

    Please reimage your card with the latest image from here:

    https://wiki.analog.com/resources/tools-software/linux-software/kuiper-linux

    [    6.516639] ad9081 spi1.0: Unrecognized CHIP_ID 0x9986

    The driver back then wouldn't support AD9986 ...

    -Michael

  • Hi

    In my serial print log, there had two ZCU102 boot processes from two different SD cards. 

    First time, the kernal version is the latest.The version 5.4.0-00602-g88b7d86ff997.

    Second time, the kernal version is old, 4.19.0-g17f4223. And the card was sent along with your ad9986 evaluation board.

    But the two kernals did not recognized CHIP_ID 0x9986.

    [    6.501991] ad9081 spi1.0: Unrecognized CHIP_ID 0x9986

    [    6.516639] ad9081 spi1.0: Unrecognized CHIP_ID 0x9986

    I suspect that the device tree and boot file are wrong. In the SD card of the new kernel, the device tree and boot file are selected as zynqmp-zcu102-rev10-ad9082-m4-l8-vcxo122.88.zip.The file from the website of AD9081/AD9082 Zynq UltraScale+ MPSoC ZCU102 Quick Start Guide [Analog Devices Wiki].

    I am comfused about the difference between the ad9082 and ad9986.When i want to find the file of ad9986, i just find the ad9081 or ad9082.

    Thanks for the answer.

Reply
  • Hi

    In my serial print log, there had two ZCU102 boot processes from two different SD cards. 

    First time, the kernal version is the latest.The version 5.4.0-00602-g88b7d86ff997.

    Second time, the kernal version is old, 4.19.0-g17f4223. And the card was sent along with your ad9986 evaluation board.

    But the two kernals did not recognized CHIP_ID 0x9986.

    [    6.501991] ad9081 spi1.0: Unrecognized CHIP_ID 0x9986

    [    6.516639] ad9081 spi1.0: Unrecognized CHIP_ID 0x9986

    I suspect that the device tree and boot file are wrong. In the SD card of the new kernel, the device tree and boot file are selected as zynqmp-zcu102-rev10-ad9082-m4-l8-vcxo122.88.zip.The file from the website of AD9081/AD9082 Zynq UltraScale+ MPSoC ZCU102 Quick Start Guide [Analog Devices Wiki].

    I am comfused about the difference between the ad9082 and ad9986.When i want to find the file of ad9986, i just find the ad9081 or ad9082.

    Thanks for the answer.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.