Post Go back to editing

ad9528 probe not bringing up vcc-supply on boot

Category: Software
Product Number: AD9528
Software Version: 2021_R1

Hello,

I have a ad9528 that is powered by a GPIO switched, fixed regulator.  The dts binding is shown below (note that regulator-boot-on and regulator-always-on were debugging attempts):

    vdda_3v3_2: vdda-3v3-2 {
        compatible = "regulator-fixed";
        regulator-name = "vdda_3v3_2";
        regulator-min-microvolt = <3300000>;
        regulator-max-microvolt = <3300000>;
        startup-delay-us = <150000>;
        gpio = <&gpio0 98 0>;
        enable-active-high;
        regulator-boot-on;
        regulator-always-on;
    };


The ad9528 has the following line in it:

    vcc-supply = <&vdda_3v3_2>;

When I boot the ad9528 tried to probe the device before the regulator comes online - this is, of course, problematic because the probe fails.  I have verified everything else in the devicetree is correct by manually enabling the GPIO in U-Boot, supplying power to the device before starting Linux.  When I do this the device probes successfully.

Is there something I am missing?  I looked at the driver code and it looks like it should be enabling the regulator before accessing the device.

Parents
  • This fixed it - Should I submit a patch?  This seems like a bug.

    diff --git a/drivers/iio/frequency/ad9528.c b/drivers/iio/frequency/ad9528.c
    index 5696cf191e35..e973f0f17452 100644
    --- a/drivers/iio/frequency/ad9528.c
    +++ b/drivers/iio/frequency/ad9528.c
    @@ -1642,12 +1642,18 @@ static int ad9528_probe(struct spi_device *spi)
            struct gpio_desc *status0_gpio;
            struct gpio_desc *status1_gpio;
            struct clk *clk;
    +       struct regulator *reg;
            int ret;
    
    +       reg = devm_regulator_get(&spi->dev, "vcc");
    +       if (PTR_ERR(reg) == -EPROBE_DEFER)
    +               return -EPROBE_DEFER;
    +
            clk = devm_clk_get(&spi->dev, NULL);
            if (PTR_ERR(clk) == -EPROBE_DEFER)
                    return -EPROBE_DEFER;
    
    +
            if (spi->dev.of_node)
                    pdata = ad9528_parse_dt(&spi->dev);
            else
    @@ -1670,7 +1676,7 @@ static int ad9528_probe(struct spi_device *spi)
    
            mutex_init(&st->lock);
    
    -       st->reg = devm_regulator_get(&spi->dev, "vcc");
    +       st->reg = reg;
            if (!IS_ERR(st->reg)) {
                    ret = regulator_enable(st->reg);
                    if (ret)
    

Reply
  • This fixed it - Should I submit a patch?  This seems like a bug.

    diff --git a/drivers/iio/frequency/ad9528.c b/drivers/iio/frequency/ad9528.c
    index 5696cf191e35..e973f0f17452 100644
    --- a/drivers/iio/frequency/ad9528.c
    +++ b/drivers/iio/frequency/ad9528.c
    @@ -1642,12 +1642,18 @@ static int ad9528_probe(struct spi_device *spi)
            struct gpio_desc *status0_gpio;
            struct gpio_desc *status1_gpio;
            struct clk *clk;
    +       struct regulator *reg;
            int ret;
    
    +       reg = devm_regulator_get(&spi->dev, "vcc");
    +       if (PTR_ERR(reg) == -EPROBE_DEFER)
    +               return -EPROBE_DEFER;
    +
            clk = devm_clk_get(&spi->dev, NULL);
            if (PTR_ERR(clk) == -EPROBE_DEFER)
                    return -EPROBE_DEFER;
    
    +
            if (spi->dev.of_node)
                    pdata = ad9528_parse_dt(&spi->dev);
            else
    @@ -1670,7 +1676,7 @@ static int ad9528_probe(struct spi_device *spi)
    
            mutex_init(&st->lock);
    
    -       st->reg = devm_regulator_get(&spi->dev, "vcc");
    +       st->reg = reg;
            if (!IS_ERR(st->reg)) {
                    ret = regulator_enable(st->reg);
                    if (ret)
    

Children