Hello, I'm building petalinux 2021.1 for standard ADRV9009-ZU11EG target using meta-adi-core and meta-adi-xilinx as they are provided by ADI.
I'm able to boot and setup concretely my ADRV9009-ZU11EG target using my custom PL design ...
I'm now trying to configure and control the ADRV9009 device (which is correctly exposed a IIO device on the virtual file system ) using libiio and the examples provided with it.
Unfortunately, probably due to somethings I'm doing wrongly, gcc do not recognizes libiio as a library (-llibiio) when I compile the ADRV9009 example of libiio 0.24. /usr/lib/libiio.so.0.24 exists and I see the iiod daemon running...
Is libiio build by default when i select the minimal image of petalinux using the ADI layer ?
Is there anything I need to do to succeed with "/libiio/examples# gcc -o test adrv9009-iiostream.c -I ../ -llibiio" ?
Thanks in advance
Joel