MAX31865
Production
The MAX31865 is an easy-to-use resistance-to-digital converter optimized for platinum resistance temperature detectors (RTDs). An external resistor sets...
Datasheet
MAX31865 on Analog.com
AD5593R
Production
The AD5593R has eight input/output (I/O) pins, which can be
independently configured as digital-to-analog converter (DAC)
outputs, analog-to-digital converter...
Datasheet
AD5593R on Analog.com
hello.
I have already modified the rpi-ad5593r-overlay.dts file on the CM4 Board to suit my environment.
And I'm using the pyadi-io Module to use AD5593R.
MAX31865 (not MAX31856) also had a pyadi-iio example.
https://github.com/analogdevicesinc/pyadi-iio/blob/master/examples/max31865.py
However, there was no dts file involved. Is there a way to use MAX31865 through linux iio driver?
Not sure I understand - there is a mainline IIO driver for MAX31865 here:
https://elixir.bootlin.com/linux/latest/source/drivers/iio/temperature/max31865.c
-Michael
Do you know where the max31865 device tree is?
You can find an example here:
examples: - | spi { #address-cells = <1>; #size-cells = <0>; temperature-sensor@0 { compatible = "maxim,max31865"; reg = <0>; spi-max-frequency = <400000>; spi-cpha; maxim,3-wire; }; };
You can find an example here:
examples: - | spi { #address-cells = <1>; #size-cells = <0>; temperature-sensor@0 { compatible = "maxim,max31865"; reg = <0>; spi-max-frequency = <400000>; spi-cpha; maxim,3-wire; }; };