Post Go back to editing

Is there a way to use max31865 through linux iio driver?

Category: Hardware
Product Number: max31865

hello.

I have already modified the rpi-ad5593r-overlay.dts file on the CM4 Board to suit my environment.

And I'm using the pyadi-io Module to use AD5593R.

MAX31865 (not MAX31856) also had a pyadi-iio example.

https://github.com/analogdevicesinc/pyadi-iio/blob/master/examples/max31865.py

However, there was no dts file involved. Is there a way to use MAX31865 through linux iio driver?