Hi,
I am using the hopping mode of LO MUX preprocess on the system with OS.
I want to control RX gain in run-time manually.
I has referred to the following discussion:
ADRV9002 Rx Gain Control in FH Mode
It seems that the DGPIO is the only way for run-time gain control with LO MUX hopping. Is that correct?
If it is true, I want to inquire about how to configure the gain control mode of "3 pins=8 possible gain value" on the OS system.
The configuration may contain the 8-level gain table and the DGPIO pin assignment.
Thanks.
Edit Notes
add tags[edited by: JimmyChen at 7:47 AM (GMT -4) on 30 Aug 2023]