Post Go back to editing

adi iio oscilloscope

Category: Software
Product Number: ADIS16465-1BMLZ
Software Version: libiio version : 0.24-accb7b5

"I want to connect the ADIS16465-1BMLZ module to the Raspberry Pi 4 using the EVAL-ADISIMU1-RPIZ board. To do this, I installed the Kuiper Linux operating system on the Raspberry Pi and ran the ADI IIO Oscilloscope software. Initially, nothing is displayed. By adding the following lines to the config.txt file as shown below, the data is displayed on  DMM:

dtoverlay=adis16475

atparam=drdy_gpio25

However, nothing is displayed in the plot section. What should I do?"

Parents Reply Children