Post Go back to editing

AD7768-1 buffer not functioning on custom Yocto image. DE10-Nano/CN0540

Category: Software
Product Number: ad7768-1

I have created a custom Yocto image for use with the DE10-Nano and CN0540. The AD7768-1's buffer does not work, however the rest of its functions seem to work correctly. I have confirmed it's not a hardware issue by using the Kuiper image provided.

If I try to use the buffer by doing:

> echo 1 > scan_elements/in_voltage0_en
> echo 1 > buffer/enable
> cat /dev/iio:device0 | hexdump

the device will crash and reboot, unless I set the length of the buffer to one with:

> echo 1 > buffer/length

then the device will still crash, but instead of rebooting it repeatedly outputs:

[  441.310599] rcu: INFO: rcu_sched self-detected stall on CPU
[  441.316258] rcu:     0-....: (2099 ticks this GP) idle=10f/1/0x40000002 softirq=2509/2509 fqs=1033
[  441.325163]  (t=2100 jiffies g=497 q=7)
[  441.329057] NMI backtrace for cpu 0
[  441.332592] CPU: 0 PID: 163 Comm: cat Not tainted 5.15.0-yocto-standard-adi #1
[  441.339927] Hardware name: Altera SOCFPGA
[  441.343988] Backtrace:
[  441.346453] [<c0d914b0>] (dump_backtrace) from [<c0d916fc>] (show_stack+0x20/0x24)
[  441.354073]  r7:c010edfc r6:00000000 r5:60070193 r4:c143b218
[  441.359801] [<c0d916dc>] (show_stack) from [<c0d94ecc>] (dump_stack_lvl+0x48/0x54)
[  441.367360] [<c0d94e84>] (dump_stack_lvl) from [<c0d94ef0>] (dump_stack+0x18/0x1c)
[  441.374907]  r5:00000000 r4:20070193
[  441.378525] [<c0d94ed8>] (dump_stack) from [<c05850fc>] (nmi_cpu_backtrace+0xe0/0x114)
[  441.386424] [<c058501c>] (nmi_cpu_backtrace) from [<c0585218>] (nmi_trigger_cpumask_backtrace+0xe8/0x134)
[  441.395965]  r7:c010edfc r6:c0e01ee4 r5:c170469c r4:00000000
[  441.401597] [<c0585130>] (nmi_trigger_cpumask_backtrace) from [<c010fd68>] (arch_trigger_cpumask_backtrace+0x20/0x24)
[  441.412180]  r9:c1703f10 r8:c0e01ee0 r7:c1835438 r6:00000000 r5:c1703fa4 r4:c171e840
[  441.419886] [<c010fd48>] (arch_trigger_cpumask_backtrace) from [<c0d9340c>] (rcu_dump_cpu_stacks+0x144/0x174)
[  441.429922] [<c0d932c8>] (rcu_dump_cpu_stacks) from [<c0198490>] (rcu_sched_clock_irq+0x6a8/0xa58)
[  441.438860]  r10:2e138000 r9:c1702d00 r8:c1693f40 r7:c18361a0 r6:00000000 r5:ef7cbf40
[  441.446784]  r4:c171e840
[  441.449304] [<c0197de8>] (rcu_sched_clock_irq) from [<c01a354c>] (update_process_times+0x98/0xc4)
[  441.458174]  r10:c1702d80 r9:c1702d40 r8:c184fd40 r7:2e138000 r6:c1702d00 r5:00000000
[  441.465969]  r4:ef7c5540
[  441.468524] [<c01a34b4>] (update_process_times) from [<c01b74e0>] (tick_sched_timer+0x88/0x2d8)
[  441.477198]  r7:c1ea9dc0 r6:00000066 r5:bf87a4da r4:ef7c6128
[  441.482830] [<c01b7458>] (tick_sched_timer) from [<c01a4260>] (__hrtimer_run_queues+0x1fc/0x36c)
[  441.491730]  r10:ef7c5e14 r9:ef7c6128 r8:20070193 r7:00000000 r6:c01b7458 r5:ef7c5dc0
[  441.499645]  r4:ef7c5e00
[  441.502183] [<c01a4064>] (__hrtimer_run_queues) from [<c01a5158>] (hrtimer_interrupt+0x13c/0x2c8)
[  441.511041]  r10:ef7c5e98 r9:ef7c5e70 r8:ef7c5e48 r7:ef7c5dcc r6:00000003 r5:20070193
[  441.518836]  r4:ef7c5dc0
[  441.521357] [<c01a501c>] (hrtimer_interrupt) from [<c0110744>] (twd_handler+0x44/0x4c)
[  441.529394]  r10:c1ea8000 r9:c1ea9dc0 r8:f080210c r7:c1d08240 r6:00000018 r5:c17046b4
[  441.537301]  r4:00000001
[  441.539821] [<c0110700>] (twd_handler) from [<c01838c8>] (handle_percpu_devid_irq+0x9c/0x200)
[  441.548321]  r5:c17046b4 r4:c1d09000
[  441.551888] [<c018382c>] (handle_percpu_devid_irq) from [<c017ced4>] (handle_domain_irq+0x6c/0x88)
[  441.560961]  r7:0000001d r6:00000000 r5:00000000 r4:c1692a14
[  441.566593] [<c017ce68>] (handle_domain_irq) from [<c0101300>] (gic_handle_irq+0x88/0x9c)
[  441.574767]  r7:c1692a20 r6:f0802100 r5:c177a344 r4:c17046b4
[  441.580494] [<c0101278>] (gic_handle_irq) from [<c0100afc>] (__irq_svc+0x5c/0x78)
[  441.587952] Exception stack(0xc1ea9dc0 to 0xc1ea9e08)
[  441.593047] 9dc0: c28b3700 00000000 00000000 00000003 00001000 c28b3700 c2b47f40 befe9c04
[  441.601193] 9de0: c28b3774 befe9c04 c1ea8000 c1ea9e24 c1ea9e28 c1ea9e10 c0a95530 c0a949ac
[  441.609342] 9e00: 20070013 ffffffff
[  441.612863]  r9:c1ea8000 r8:c28b3774 r7:c1ea9df4 r6:ffffffff r5:20070013 r4:c0a949ac
[  441.620699] [<c0a949a0>] (iio_dma_buffer_dequeue) from [<c0a95530>] (iio_dma_buffer_read+0x148/0x19c)
[  441.629894]  r5:c28b3700 r4:00001000
[  441.633452] [<c0a953e8>] (iio_dma_buffer_read) from [<c0952618>] (iio_buffer_read+0x178/0x228)
[  441.642168]  r10:c1ea8000 r9:befe9c04 r8:00001000 r7:00000400 r6:00000002 r5:c1e43000
[  441.649962]  r4:c28b3700
[  441.652483] [<c09524a0>] (iio_buffer_read) from [<c0954b24>] (iio_buffer_read_wrapper+0x2c/0x38)
[  441.661248]  r10:00000003 r9:c0954af8 r8:00001000 r7:00000001 r6:c1ea8000 r5:c1ea9f60
[  441.669050]  r4:c2b28540
[  441.671571] [<c0954af8>] (iio_buffer_read_wrapper) from [<c02b2da8>] (vfs_read+0xc4/0x320)
[  441.679817] [<c02b2ce4>] (vfs_read) from [<c02b348c>] (ksys_read+0x74/0xec)
[  441.686766]  r10:00000003 r9:00000000 r8:00000000 r7:befe9c04 r6:c1ea8000 r5:c2b28540
[  441.694560]  r4:c2b28540
[  441.697081] [<c02b3418>] (ksys_read) from [<c02b351c>] (sys_read+0x18/0x1c)
[  441.704027]  r9:c1ea8000 r8:c0100244 r7:00000003 r6:b6f681a0 r5:befe9c04 r4:00001000
[  441.711733] [<c02b3504>] (sys_read) from [<c0100060>] (ret_fast_syscall+0x0/0x48)
[  441.719310] Exception stack(0xc1ea9fa8 to 0xc1ea9ff0)
[  441.724344] 9fa0:                   00001000 befe9c04 00000003 befe9c04 00001000 00000000
[  441.732488] 9fc0: 00001000 befe9c04 b6f681a0 00000003 00000000 01000000 00000003 befe9c04
[  441.740769] 9fe0: 00000003 befe9bb8 b6e6070f b6de1ae6

every ~20 seconds.

If I try to use:

> iio_readdev ad7768-1

I get the error:

> Unable to refill buffer: Connection timed out (110)

The output of

> iio_info

is:

Library version: 0.23 (git tag: 92d6a35)
Compiled with backends: local xml ip usb serial
IIO context created with local backend.
Backend version: 0.23 (git tag: 92d6a35)
Backend description string: Linux VibMonProto 5.15.0-yocto-standard-adi #1 SMP Thu Apr 27 16:34:06 UTC 2023 armv7l
IIO context has 2 attributes:
        local,kernel: 5.15.0-yocto-standard-adi
        uri: local:
IIO context has 5 devices:
        iio:device0: ad7768-1 (buffer capable)
                1 channels found:
                        voltage0:  (input, index: 0, format: le:s24/32>>8)
                        3 channel-specific attributes found:
                                attr  0: label value: (null)
                                attr  1: raw value: -2246463
                                attr  2: scale value: 0.000488281
                4 device-specific attributes found:
                                attr  0: common_mode_voltage value: (AVDD1-AVSS)/2
                                attr  1: common_mode_voltage_available value: (AVDD1-AVSS)/2 2V5 2V05 1V9 1V65 1V1 0V9 OFF
                                attr  2: sampling_frequency value: 256000
                                attr  3: sampling_frequency_available value: 256000 128000 64000 32000 16000 8000 4000 2000 1000
                3 buffer-specific attributes found:
                                attr  0: data_available value: 0
                                attr  1: length_align_bytes value: 16
                                attr  2: watermark value: 2048
                1 debug attributes found:
                                debug attr  0: direct_reg_access value: 0x0
                No trigger on this device
        iio:device1: ltc2308
                8 channels found:
                        voltage6:  (input)
                        2 channel-specific attributes found:
                                attr  0: raw value: 175
                                attr  1: scale value: 1.000000000
                        voltage3:  (input)
                        2 channel-specific attributes found:
                                attr  0: raw value: 163
                                attr  1: scale value: 1.000000000
                        voltage7:  (input)
                        2 channel-specific attributes found:
                                attr  0: raw value: 166
                                attr  1: scale value: 1.000000000
                        voltage0:  (input)
                        2 channel-specific attributes found:
                                attr  0: raw value: 162
                                attr  1: scale value: 1.000000000
                        voltage4:  (input)
                        2 channel-specific attributes found:
                                attr  0: raw value: 169
                                attr  1: scale value: 1.000000000
                        voltage1:  (input)
                        2 channel-specific attributes found:
                                attr  0: raw value: 165
                                attr  1: scale value: 1.000000000
                        voltage5:  (input)
                        2 channel-specific attributes found:
                                attr  0: raw value: 168
                                attr  1: scale value: 1.000000000
                        voltage2:  (input)
                        2 channel-specific attributes found:
                                attr  0: raw value: 161
                                attr  1: scale value: 1.000000000
                2 device-specific attributes found:
                                attr  0: sleep_mode value: DISABLED
                                attr  1: sleep_mode_available value: DISABLED ENABLED
                No trigger on this device
        iio:device2: one-bit-adc-dac
                8 channels found:
                        voltage0:  (input)
                        2 channel-specific attributes found:
                                attr  0: label value: cn0540_sw_ff_gpio
                                attr  1: raw value: 0
                        voltage1:  (output)
                        2 channel-specific attributes found:
                                attr  0: label value: cn0540_red_led
                                attr  1: raw value: 0
                        voltage5:  (output)
                        2 channel-specific attributes found:
                                attr  0: label value: cn0540_FDA_DIS
                                attr  1: raw value: 0
                        voltage0:  (output)
                        2 channel-specific attributes found:
                                attr  0: label value: cn0540_blue_led
                                attr  1: raw value: 0
                        voltage3:  (output)
                        2 channel-specific attributes found:
                                attr  0: label value: cn0540_ad7768-1-gpio0
                                attr  1: raw value: 0
                        voltage6:  (output)
                        2 channel-specific attributes found:
                                attr  0: label value: cn0540_FDA_MODE
                                attr  1: raw value: 0
                        voltage2:  (output)
                        2 channel-specific attributes found:
                                attr  0: label value: cn0540_shutdown_gpio
                                attr  1: raw value: 0
                        voltage4:  (output)
                        2 channel-specific attributes found:
                                attr  0: label value: cn0540_ad7768-1-gpio1
                                attr  1: raw value: 0
                No trigger on this device
        iio:device3: ltc2606
                1 channels found:
                        voltage0:  (output)
                        5 channel-specific attributes found:
                                attr  0: powerdown value: 0
                                attr  1: powerdown_mode value: 90kohm_to_gnd
                                attr  2: powerdown_mode_available value: 90kohm_to_gnd
                                attr  3: raw value: 32768
                                attr  4: scale value: 0.062500000
                No trigger on this device
        iio_sysfs_trigger:
                0 channels found:
                2 device-specific attributes found:
                                attr  0: add_trigger ERROR: Permission denied (13)
                                attr  1: remove_trigger ERROR: Permission denied (13)
                No trigger on this device

The custom image uses the adi kernel fork for its kernel, u-boot-socfpga for its u-boot by utilizing meta-altera, and CN0540 HDL to program the FPGA.

The HDL is compiled and converted to rbf FPPx16, then loaded onto the FPGA by modifying the U-boot bootcmd to include:

fatload mmc 0:1 0x2000000 fpga_design.rbf;
fpga load 0 0x2000000 0x700000;
bridge enable;

The socfpga_cyclone5_de10_nano_cn0540.dts device tree, and socfpga_adi_defconfig are used to configure the kernel.

sysvinit is changed to systemd as well.

Is there a step I'm missing to use this device with a custom image?