Post Go back to editing

ad9361, digital tuning error on linux

Thread Summary

The user encountered digital tuning failures with the AD9361 transceiver on a Zynq-7000 SOM board when using Linux, despite working correctly with NO-OS. The issue was resolved by using a different FSBL, suggesting the problem was related to the FSBL configuration.
AI Generated Content
Category: Hardware
Product Number: ad9361

A riddle from Jacques Fresco.
This error occurs. When I use NO-OS, there is no such error.
ad9361_spi_writem: reg 0x74 val 0x1
ad9361_spi_writem: reg 0x73 val 0x67
ad9361_spi_writem: reg 0x76 val 0x1
ad9361_spi_writem: reg 0x75 val 0x67
ad9361_spi_writem: reg 0x4A val 0x35
ad9361_spi_writem: reg 0x49 val 0x5B
ad9361_spi_writem: reg 0x48 val 0xE8
SAMPL CLK: 25000000 tuning: RX
0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
0:# # # # # # # # # # # # # # # #
1:# # # # # # # # # # # # # # # #
ad9361_spi_writem: reg 0x4A val 0x35
ad9361_spi_writem: reg 0x49 val 0x5B
ad9361_spi_writem: reg 0x48 val 0xE8
SAMPL CLK: 40000000 tuning: RX
0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
0:# # # # # # # # # # # # # # # #
1:# # # # # # # # # # # # # # # #
ad9361_spi_writem: reg 0x4A val 0x35
ad9361_spi_writem: reg 0x49 val 0x5B
ad9361_spi_writem: reg 0x48 val 0xE8
SAMPL CLK: 61440000 tuning: RX
0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
0:# # # # # # # # # # # # # # # #
1:# # # # # # # # # # # # # # # #
SAMPL CLK: 61440000 tuning: RX
0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
0:# # # # # # # # # # # # # # # #
1:# # # # # # # # # # # # # # # #
ad9361 spi2.0: ad9361_dig_tune_delay: Tuning RX FAILED!
ad9361_spi_writem: reg 0x74 val 0x0
ad9361_spi_writem: reg 0x73 val 0x28
ad9361_spi_writem: reg 0x76 val 0x0
ad9361_spi_writem: reg 0x75 val 0x28
cf_axi_adc: probe of 79020000.cf-ad9361-lpc failed with error -5

Here's a tree:

ptm@f889c000 {
compatible = "arm,coresight-etm3x", "arm,primecell";
reg = <0xf889c000 0x1000>;
clocks = <&clkc 27>, <&clkc 46>, <&clkc 47>;
clock-names = "apb_pclk", "dbg_trc", "dbg_apb";
cpu = <&cpu0>;
out-ports {
port {
ptm0_out_port: endpoint {
remote-endpoint = <&funnel0_in_port0>;
};
};
};
};

ptm@f889d000 {
compatible = "arm,coresight-etm3x", "arm,primecell";
reg = <0xf889d000 0x1000>;
clocks = <&clkc 27>, <&clkc 46>, <&clkc 47>;
clock-names = "apb_pclk", "dbg_trc", "dbg_apb";
cpu = <&cpu1>;
out-ports {
port {
ptm1_out_port: endpoint {
remote-endpoint = <&funnel0_in_port1>;
};
};
};
};
};
};
# 3 "zynq.dtsi" 2
/ {
chosen {
bootargs = "earlycon";
stdout-path = "serial0:115200n8";
};
aliases {
serial0 = &uart0;
spi0 = &qspi;
// spi1 = &axi_spi;
spi2 = &spi0;
};
memory {
device_type = "memory";
reg = <0x0 0x20000000>;
};
};

/ {
cpus {
cpu@0 {
operating-points = <800000 1000000 400000 1000000 200000 1000000>;
};
};
};
&gpio0 {
emio-gpio-width = <25>;
gpio-mask-high = <0x0>;
gpio-mask-low = <0x5600>;
};
&intc {
num_cpus = <2>;
num_interrupts = <96>;
};
&qspi {
is-dual = <0>;
num-cs = <0x1>;
spi-rx-bus-width = <4>;
spi-tx-bus-width = <4>;
status = "okay";
};
&sdhci0 {
status = "okay";
xlnx,has-cd = <0x1>;
xlnx,has-power = <0x0>;
xlnx,has-wp = <0x0>;
};
&spi0 {
is-decoded-cs = <0>;
num-cs = <0x3>;
status = "okay";
};
&uart0 {
cts-override ;
device_type = "serial";
port-number = <0>;
status = "okay";
};
&clkc {
fclk-enable = <0x3>;
ps-clk-frequency = <33333333>;
};
# 9 "zynq-antsdre200.dtsi" 2
# 1 "/home/vasiliy/scat_lib/zynq_timestamping/ant_device_tree/generate/include/dt-bindings/input/input.h" 1
# 13 "/home/vasiliy/scat_lib/zynq_timestamping/ant_device_tree/generate/include/dt-bindings/input/input.h"
# 1 "/home/vasiliy/scat_lib/zynq_timestamping/ant_device_tree/generate/include/dt-bindings/input/linux-event-codes.h" 1
# 14 "/home/vasiliy/scat_lib/zynq_timestamping/ant_device_tree/generate/include/dt-bindings/input/input.h" 2
# 10 "zynq-antsdre200.dtsi" 2
# 1 "/home/vasiliy/scat_lib/zynq_timestamping/ant_device_tree/generate/include/dt-bindings/gpio/gpio.h" 1
# 11 "zynq-antsdre200.dtsi" 2
# 1 "/home/vasiliy/scat_lib/zynq_timestamping/ant_device_tree/generate/include/dt-bindings/interrupt-controller/irq.h" 1
# 12 "zynq-antsdre200.dtsi" 2


# 1 "/home/vasiliy/scat_lib/zynq_timestamping/ant_device_tree/generate/include/dt-bindings/iio/adc/adi,ad9361.h" 1
# 15 "zynq-antsdre200.dtsi" 2

/ {
// model = "MicroPhase ANTSDR E200";
// memory {
// device_type = "memory";
// reg = <0x00000000 0x20000000>;
// };

// aliases {
// ethernet0 = &gem0;
// serial0 = &uart0;
// spi0 = &qspi;
// mmc0 = &sdhci0;
// };

// chosen {

// stdout-path = "/amba@0/uart@E0000000";
// };


clocks {
ad9361_clkin: clock@0 {
compatible = "fixed-clock";

clock-frequency = <40000000>;
clock-output-names = "ad9361_ext_refclk";
#clock-cells = <0>;
};
};

// ltc2630 {
// compatible = "microphase,ltc2630";
// status = "okay";
// ext_ref_locked = <&gpio0 68 1>;
// ext_ref_ispps = <&gpio0 69 0>;
// ref_sel = <&gpio0 70 0>;
// };


};


&sdhci0 {
status = "okay";
xlnx,has-cd = <0x0>;
xlnx,has-power = <0x0>;
xlnx,has-wp = <0x0>;
};

&watchdog0 {
status = "okay";
reset-on-timeout;
};

&uart0 {
status = "okay";
};
# 110 "zynq-antsdre200.dtsi"
&gem0 {
status = "okay";

phy-handle = <&phy0>;
phy-mode = "rgmii-rxid";
xlnx,has-mdio = <0x1>;
gmii2rgmii-phy-handle = <&gmii_to_rgmii_0>;

phy0: phy@1 {
compatible = "ethernet-phy-id011c.c916";
device_type = "ethernet-phy";
reg = <0x1>;

};

gmii_to_rgmii_0: gmiitorgmii@8 {
compatible = "xlnx,gmii-to-rgmii-1.0";
reg = <0x8>;
phy-handle = <&phy0>;
};

};

&qspi {
status = "okay";
is-dual = <0>;
num-cs = <1>;
primary_flash: ps7-qspi@0 {
#address-cells = <1>;
#size-cells = <1>;
spi-tx-bus-width = <1>;
spi-rx-bus-width = <4>;
compatible = "n25q256a", "n25q512a", "jedec,spi-nor";
reg = <0x0>;
spi-max-frequency = <50000000>;
partition@qspi-fsbl-uboot {
label = "qspi-fsbl-uboot";
reg = <0x0 0x100000>;
};
partition@qspi-uboot-env {
label = "qspi-uboot-env";
reg = <0x100000 0x20000>;
};
partition@qspi-nvmfs {
label = "qspi-nvmfs";
reg = <0x120000 0xE0000>;
};
partition@qspi-linux {
label = "qspi-linux";
reg = <0x200000 0x1E00000>;
};
};
};

&adc {
xlnx,channels {
#address-cells = <1>;
#size-cells = <0>;
channel@0 {
reg = <0>;
};
};
};

/ {
fpga_axi: fpga-axi@0 {
compatible = "simple-bus";
#address-cells = <0x1>;
#size-cells = <0x1>;
ranges;

rx_dma: dma@7c400000 {
compatible = "adi,axi-dmac-1.00.a";
reg = <0x7c400000 0x1000>;
#dma-cells = <1>;
interrupt-parent = <&intc>;
interrupts = <0 57 4>;
clocks = <&clkc 16>;

adi,channels {
#size-cells = <0>;
#address-cells = <1>;

dma-channel@0 {
reg = <0>;
adi,source-bus-width = <32>;
adi,source-bus-type = <2>;
adi,destination-bus-width = <64>;
adi,destination-bus-type = <0>;
};
};
};

tx_dma: dma@7c420000 {
compatible = "adi,axi-dmac-1.00.a";
reg = <0x7c420000 0x1000>;
#dma-cells = <1>;
interrupt-parent = <&intc>;
interrupts = <0 56 4>;
clocks = <&clkc 16>;

adi,channels {
#size-cells = <0>;
#address-cells = <1>;

dma-channel@0 {
reg = <0>;
adi,source-bus-width = <64>;
adi,source-bus-type = <0>;
adi,destination-bus-width = <32>;
adi,destination-bus-type = <2>;
};
};
};

cf_ad9364_adc_core_0: cf-ad9361-lpc@79020000 {
compatible = "adi,axi-ad9361-6.00.a";
reg = <0x79020000 0x6000>;
dmas = <&rx_dma 0>;
dma-names = "rx";
spibus-connected = <&adc0_ad9361>;
adi,axi-decimation-core-available;
};

cf_ad9364_dac_core_0: cf-ad9361-dds-core-lpc@79024000 {
compatible = "adi,axi-ad9361-dds-6.00.a";
reg = <0x79024000 0x1000>;
clocks = <&adc0_ad9361 13>;
clock-names = "sampl_clk";
dmas = <&tx_dma 0>;
dma-names = "tx";
adi,axi-interpolation-core-available;
adi,axi-dds-default-scale = <0>;
};

mwipcore@43c00000 {
compatible = "mathworks,mwipcore-axi4lite-v1.00";
reg = <0x43c00000 0xffff>;
};
};
};

&spi0 {
status = "okay";

adc0_ad9361: ad9361-phy@0 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "adi,ad9361";

reg = <0>;

/* SPI Setup */
spi-cpha;
spi-max-frequency = <10000000>;

/* Clocks */
clocks = <&ad9361_clkin 0>;
clock-names = "ad9361_ext_refclk";
clock-output-names = "rx_sampl_clk", "tx_sampl_clk";
#clock-cells = <1>;

// adi,debug-mode-enable;
/* Digital Interface Control */

/* adi,digital-interface-tune-skip-mode:
* 0 = TUNE RX&TX
* 1 = SKIP TX
* 2 = SKIP ALL
*/
adi,digital-interface-tune-skip-mode = <0>;

adi,pp-tx-swap-enable;
adi,pp-rx-swap-enable;
adi,rx-frame-pulse-mode-enable;
adi,lvds-mode-enable;
adi,lvds-bias-mV = <150>;
adi,lvds-rx-onchip-termination-enable;
adi,rx-data-delay = <4>;
adi,tx-fb-clock-delay = <7>;

//adi,fdd-rx-rate-2tx-enable;

adi,dcxo-coarse-and-fine-tune = <8 5920>;
//adi,xo-disable-use-ext-refclk-enable;

/* Mode Setup */

adi,2rx-2tx-mode-enable;
//adi,split-gain-table-mode-enable;

/* ENSM Mode */
adi,frequency-division-duplex-mode-enable;
//adi,ensm-enable-pin-pulse-mode-enable;
//adi,ensm-enable-txnrx-control-enable;


/* adi,rx-rf-port-input-select:
* 0 = (RX1A_N & RX1A_P) and (RX2A_N & RX2A_P) enabled; balanced
* 1 = (RX1B_N & RX1B_P) and (RX2B_N & RX2B_P) enabled; balanced
* 2 = (RX1C_N & RX1C_P) and (RX2C_N & RX2C_P) enabled; balanced
*
* 3 = RX1A_N and RX2A_N enabled; unbalanced
* 4 = RX1A_P and RX2A_P enabled; unbalanced
* 5 = RX1B_N and RX2B_N enabled; unbalanced
* 6 = RX1B_P and RX2B_P enabled; unbalanced
* 7 = RX1C_N and RX2C_N enabled; unbalanced
* 8 = RX1C_P and RX2C_P enabled; unbalanced
*/

adi,rx-rf-port-input-select = <0>; /* (RX1A_N & RX1A_P) and (RX2A_N & RX2A_P) enabled; balanced */

/* adi,tx-rf-port-input-select:
* 0 TX1A, TX2A
* 1 TX1B, TX2B
*/

adi,tx-rf-port-input-select = <0>; /* TX1A, TX2A */
//adi,update-tx-gain-in-alert-enable;
adi,tx-attenuation-mdB = <10000>;
adi,tx-lo-powerdown-managed-enable;

adi,rf-rx-bandwidth-hz = <18000000>;
adi,rf-tx-bandwidth-hz = <18000000>;
adi,rx-synthesizer-frequency-hz = /bits/ 64 <2400000000>;
adi,tx-synthesizer-frequency-hz = /bits/ 64 <2400000000>;

/* BBPLL ADC R2CLK R1CLK CLKRF RSAMPL */
adi,rx-path-clock-frequencies = <983040000 245760000 122880000 61440000 30720000 30720000>;
/* BBPLL DAC T2CLK T1CLK CLKTF TSAMPL */
adi,tx-path-clock-frequencies = <983040000 122880000 122880000 61440000 30720000 30720000>;

/* Gain Control */

//adi,gaintable-name = "ad9361_std_gaintable";

/* adi,gc-rx[1|2]-mode:
* 0 = RF_GAIN_MGC
* 1 = RF_GAIN_FASTATTACK_AGC
* 2 = RF_GAIN_SLOWATTACK_AGC
* 3 = RF_GAIN_HYBRID_AGC
*/

adi,gc-rx1-mode = <2>;
adi,gc-rx2-mode = <2>;
adi,gc-adc-ovr-sample-size = <4>; /* sum 4 samples */
adi,gc-adc-small-overload-thresh = <47>; /* sum of squares */
adi,gc-adc-large-overload-thresh = <58>; /* sum of squares */
adi,gc-lmt-overload-high-thresh = <800>; /* mV */
adi,gc-lmt-overload-low-thresh = <704>; /* mV */
adi,gc-dec-pow-measurement-duration = <8192>; /* 0..524288 Samples */
adi,gc-low-power-thresh = <24>; /* 0..-64 dBFS vals are set pos */
//adi,gc-dig-gain-enable;
//adi,gc-max-dig-gain = <15>;

/* Manual Gain Control Setup */

//adi,mgc-rx1-ctrl-inp-enable; /* uncomment to use ctrl inputs */
//adi,mgc-rx2-ctrl-inp-enable; /* uncomment to use ctrl inputs */
adi,mgc-inc-gain-step = <2>;
adi,mgc-dec-gain-step = <2>;

/* adi,mgc-split-table-ctrl-inp-gain-mode:
* (relevant if adi,split-gain-table-mode-enable is set)
* 0 = AGC determine this
* 1 = only in LPF
* 2 = only in LMT
*/

adi,mgc-split-table-ctrl-inp-gain-mode = <0>;

/* Automatic Gain Control Setup */

adi,agc-attack-delay-extra-margin-us= <1>; /* us */
adi,agc-outer-thresh-high = <5>; /* -dBFS */
adi,agc-outer-thresh-high-dec-steps = <2>; /* 0..15 */
adi,agc-inner-thresh-high = <10>; /* -dBFS */
adi,agc-inner-thresh-high-dec-steps = <1>; /* 0..7 */
adi,agc-inner-thresh-low = <12>; /* -dBFS */
adi,agc-inner-thresh-low-inc-steps = <1>; /* 0..7 */
adi,agc-outer-thresh-low = <18>; /* -dBFS */
adi,agc-outer-thresh-low-inc-steps = <2>; /* 0..15 */

adi,agc-adc-small-overload-exceed-counter = <10>; /* 0..15 */
adi,agc-adc-large-overload-exceed-counter = <10>; /* 0..15 */
adi,agc-adc-large-overload-inc-steps = <2>; /* 0..15 */
//adi,agc-adc-lmt-small-overload-prevent-gain-inc-enable;
adi,agc-lmt-overload-large-exceed-counter = <10>; /* 0..15 */
adi,agc-lmt-overload-small-exceed-counter = <10>; /* 0..15 */
adi,agc-lmt-overload-large-inc-steps = <2>; /* 0..7 */
//adi,agc-dig-saturation-exceed-counter = <3>; /* 0..15 */
//adi,agc-dig-gain-step-size = <4>; /* 1..8 */

//adi,agc-sync-for-gain-counter-enable;
adi,agc-gain-update-interval-us = <1000>; /* 1ms */
//adi,agc-immed-gain-change-if-large-adc-overload-enable;
//adi,agc-immed-gain-change-if-large-lmt-overload-enable;

/* Fast AGC */

adi,fagc-dec-pow-measurement-duration = <64>; /* 64 Samples */
//adi,fagc-allow-agc-gain-increase-enable;
adi,fagc-lp-thresh-increment-steps = <1>;
adi,fagc-lp-thresh-increment-time = <5>;

adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt = <8>;
adi,fagc-final-overrange-count = <3>;
//adi,fagc-gain-increase-after-gain-lock-enable;
adi,fagc-gain-index-type-after-exit-rx-mode = <0>;
adi,fagc-lmt-final-settling-steps = <1>;
adi,fagc-lock-level = <10>;
adi,fagc-lock-level-gain-increase-upper-limit = <5>;
adi,fagc-lock-level-lmt-gain-increase-enable;

adi,fagc-lpf-final-settling-steps = <1>;
adi,fagc-optimized-gain-offset = <5>;
adi,fagc-power-measurement-duration-in-state5 = <64>;
adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable;
adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll = <10>;
adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable;
adi,fagc-rst-gla-if-en-agc-pulled-high-mode = <0>;
adi,fagc-rst-gla-large-adc-overload-enable;
adi,fagc-rst-gla-large-lmt-overload-enable;
adi,fagc-rst-gla-stronger-sig-thresh-above-ll = <10>;
adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable;
adi,fagc-state-wait-time-ns = <260>;
adi,fagc-use-last-lock-level-for-set-gain-enable;

/* RSSI */

/* adi,rssi-restart-mode:
* 0 = AGC_IN_FAST_ATTACK_MODE_LOCKS_THE_GAIN,
* 1 = EN_AGC_PIN_IS_PULLED_HIGH,
* 2 = ENTERS_RX_MODE,
* 3 = GAIN_CHANGE_OCCURS,
* 4 = SPI_WRITE_TO_REGISTER,
* 5 = GAIN_CHANGE_OCCURS_OR_EN_AGC_PIN_PULLED_HIGH,
*/
adi,rssi-restart-mode = <3>;
//adi,rssi-unit-is-rx-samples-enable;
adi,rssi-delay = <1>; /* 1us */
adi,rssi-wait = <1>; /* 1us */
adi,rssi-duration = <1000>; /* 1ms */

//test
adi,lvds-invert1-control = <0xFF>;
adi,lvds-invert2-control = <0x0F>;
adi,aux-adc-decimation = <256>;
adi,aux-adc-rate = <40000000>;
adi,dc-offset-count-high-range = <0x28>;
adi,dc-offset-count-low-range = <0x32>;

/* Control Outputs */
adi,ctrl-outs-index = <0>;
adi,ctrl-outs-enable-mask = <0xFF>;

/* AuxADC Temp Sense Control */

adi,temp-sense-measurement-interval-ms = <1000>;
adi,temp-sense-offset-signed = <0xCE>;
adi,temp-sense-periodic-measurement-enable;

/* AuxDAC Control */

adi,aux-dac-manual-mode-enable;

adi,aux-dac1-default-value-mV = <0>;
//adi,aux-dac1-active-in-rx-enable;
//adi,aux-dac1-active-in-tx-enable;
//adi,aux-dac1-active-in-alert-enable;
adi,aux-dac1-rx-delay-us = <0>;
adi,aux-dac1-tx-delay-us = <0>;

adi,aux-dac2-default-value-mV = <0>;
//adi,aux-dac2-active-in-rx-enable;
//adi,aux-dac2-active-in-tx-enable;
//adi,aux-dac2-active-in-alert-enable;
adi,aux-dac2-rx-delay-us = <0>;
adi,aux-dac2-tx-delay-us = <0>;

adi,delay-rx-data = <0>;
adi,rx-data-clock-delay = <0>;
adi,tx-data-delay = <0>;


// en_agc-gpios = <&gpio0 122 0>;
sync-gpios = <&gpio0 99 0>;
reset-gpios = <&gpio0 54 0>;
enable-gpios = <&gpio0 55 0>;
txnrx-gpios = <&gpio0 56 0>;
};
};
# 11 "zynq-antsdre200.dts" 2
# 24 "zynq-antsdre200.dts"

Edit Notes

Change q.
[edited by: Novas228 at 11:19 AM (GMT -4) on 24 May 2023]
Parents Reply Children
  • The HDL and drivers are verified together at release points, but not across releases. So its only luck if they work across different branches. My most likely guess of the issues you are having are related to the interface configuration. Especially if you are moving from a CMOS to an LVDS design on your own.

    -Travis

  • Thanks, I'll think about it, but do not forget that in no-os everything works as it should for me.

  • Yes but configuration is different between Linux and No-OS. So even if it works in No-OS doesn't mean you configured Linux correctly.

    -Travis

  • I did as you said but got the same results.

    Linux log:
    ...
    ad9361 spi0.0: ad9361_probe : AD936x Rev 0 successfully initialized
    cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x79024000 mapped to 0x(ptrval), probed DDS AD9361
    axi_sysid 45000000.axi-sysid-0: AXI System ID core version (1.01.a) found
    axi_sysid 45000000.axi-sysid-0: [fmcomms2] on [zc706] git branch <hdl_2021_r2> git <d0336c0f6ff88061d906621c11b616145f96358e> clean [2023-05-31 06:28:30] UTC
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    usbcore: registered new interface driver snd-usb-audio
    NET: Registered protocol family 10
    Segment Routing with IPv6
    sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    NET: Registered protocol family 17
    NET: Registered protocol family 36
    Key type dns_resolver registered
    Registering SWP/SWPB emulation handler
    of-fpga-region fpga-full: FPGA Region probed
    SAMPL CLK: 61440000 tuning: RX
    0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # # # # # # # # # # # # # # #
    1:# # # # # # # # # # # # # # # #
    ad9361 spi0.0: ad9361_dig_tune_delay: Tuning RX FAILED!
    cf_axi_adc: probe of 79020000.cf-ad9361-lpc failed with error -5
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    of_cfs_init
    of_cfs_init: OK
    ...

    No-os log:
    cf-ad9361-lpc: Successfully initialized (122875976 Hz)
    SAMPL CLK: 25000000 tuning: RX
    0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # o o o o o o o o o o o o o o
    1:# # # # # # # # # # # # # # # #
    SAMPL CLK: 40000000 tuning: RX
    0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # o o o o o o o o # # # # # #
    1:# # # # # # # # # # # # # # # #
    SAMPL CLK: 61440000 tuning: RX
    0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # o o o # # # # # # # # # # #
    1:# # # # # # # # # # # # # # # #
    SAMPL CLK: 61440000 tuning: RX
    0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # o O o # # # # # # # # # # #
    1:# # # # # # # # # # # # # # # #
    SAMPL CLK: 25000000 tuning: TX
    0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # # # # # # # # # # # # # # #
    1:# # o o o o o o o o o o o o o o
    SAMPL CLK: 40000000 tuning: TX
    0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # # # # # # # # # # # # # # #
    1:# # o o o o o o o # # # # # # #
    SAMPL CLK: 61440000 tuning: TX
    0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # # # # # # # # # # # # # # #
    1:# # o o o # # # # # # # # # # #
    SAMPL CLK: 61440000 tuning: TX
    0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:# # # # # # # # # # # # # # # #
    1:# # o O o # # # # # # # # # # #
    ad9361_init : AD936x Rev 2 successfully initialized
    cf-ad9361-dds-core-lpc: Successfully initialized (122875976 Hz)
    DMA_EXAMPLE: address=0x13c030 samples=65536 channels=4 bits=16
    Done.
    (I noticed one oddity when I start no-os, my board is flashed only on the second attempt.)

    Changes(hdl, origin/hdl_2021_r2, project fmcomms2/zc706):
    -delete hdmi, gpio_bd, spdif, i2c, tdd_sync, gpio_muxout_tx, gpio_muxout_rx, spi_udc;
    -ddr(i have 4096 mbit ddr);
    -uart1 to uart0;
    -constr(use my, they work).

    Linux(branch 'origin/2021_R2'):
    config: zynq_xcomm_adv7511_defconfig.


    device_tree: zynq-zc706-adv7511-ad9361-fmcomms2-3.dtbdevice_tree is missing modules that are removed in hdl.

    
    
    
    
    // SPDX-License-Identifier: GPL-2.0
    /*
     * Analog Devices AD-FMCOMMS2-EBZ/AD-FMCOMMS3-EBZ
     * https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz
     * https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms3-ebz
     *
     * hdl_project: <fmcomms2/zc706>
     * board_revision: <>
     *
     * Copyright (C) 2014-2019 Analog Devices Inc.
     */
    /dts-v1/;
    
    #include "zynq-zc706.dtsi"
    #include "zynq-zc706-adv7511.dtsi"
    
    // &i2c_mux {
    // 	fmc_i2c: i2c@6 {
    // 		#size-cells = <0>;
    // 		#address-cells = <1>;
    // 		reg = <6>;
    // 	};
    // };
    
    &fpga_axi  {
    	rx_dma: dma@7c400000 {
    		compatible = "adi,axi-dmac-1.00.a";
    		reg = <0x7c400000 0x1000>;
    		#dma-cells = <1>;
    		interrupts = <0 57 IRQ_TYPE_LEVEL_HIGH>;
    		clocks = <&clkc 16>;
    
    		adi,channels {
    			#size-cells = <0>;
    			#address-cells = <1>;
    
    			dma-channel@0 {
    				reg = <0>;
    				adi,source-bus-width = <64>;
    				adi,source-bus-type = <2>;
    				adi,destination-bus-width = <64>;
    				adi,destination-bus-type = <0>;
    			};
    		};
    	};
    
    	tx_dma: dma@7c420000 {
    		compatible = "adi,axi-dmac-1.00.a";
    		reg = <0x7c420000 0x1000>;
    		#dma-cells = <1>;
    		interrupts = <0 56 IRQ_TYPE_LEVEL_HIGH>;
    		clocks = <&clkc 16>;
    
    		adi,channels {
    			#size-cells = <0>;
    			#address-cells = <1>;
    
    			dma-channel@0 {
    				reg = <0>;
    				adi,source-bus-width = <64>;
    				adi,source-bus-type = <0>;
    				adi,destination-bus-width = <64>;
    				adi,destination-bus-type = <2>;
    			};
    		};
    	};
    
    	cf_ad9361_adc_core_0: cf-ad9361-lpc@79020000 {
    		compatible = "adi,axi-ad9361-6.00.a";
    		reg = <0x79020000 0x6000>;
    		dmas = <&rx_dma 0>;
    		dma-names = "rx";
    
    		spibus-connected = <&adc0_ad9361>;
    	};
    
    	cf_ad9361_dac_core_0: cf-ad9361-dds-core-lpc@79024000 {
    		compatible = "adi,axi-ad9361-dds-6.00.a";
    		reg = <0x79024000 0x1000>;
    		clocks = <&adc0_ad9361 13>;
    		clock-names = "sampl_clk";
    		dmas = <&tx_dma 0>;
    		dma-names = "tx";
    	};
    
    	mwipcore@43c00000 {
    		compatible = "mathworks,mwipcore-axi4lite-v1.00";
    		reg = <0x43C00000 0xffff>;
    	};
    };
    
    &spi0 {
    	status = "okay";
    };
    
    // &spi1 {
    // 	status = "okay";
    // };
    
    #define fmc_spi spi0
    // #define pmod_spi spi1
    
    #include "adi-fmcomms2.dtsi"
    #include "adi-fmcomms3-up-down-converter.dtsi"
    
    &adc0_ad9361 {
    	en_agc-gpios = <&gpio0 98 0>;
    	sync-gpios = <&gpio0 99 0>;
    	reset-gpios = <&gpio0 100 0>; /* Previously 83 */
    	enable-gpios = <&gpio0 101 0>;
    	txnrx-gpios = <&gpio0 102 0>;
    };
    
    // &lo_pll0_rx_adf4351 {
    // 	gpios = <&gpio0 103 0>;
    // };
    
    // &lo_pll0_tx_adf4351 {
    // 	gpios = <&gpio0 104 0>;
    // };
    
    
    
    
    / {
    	clocks {
    		ad9361_clkin: clock@0 {
    			compatible = "fixed-clock";
    
    			clock-frequency = <40000000>;
    			clock-output-names = "ad9361_ext_refclk";
    			#clock-cells = <0>;
    		};
    	};
    };
    
    &fmc_spi {
    	adc0_ad9361: ad9361-phy@0 {
    		compatible = "adi,ad9361";
    		reg = <0>;
    
    		/* SPI Setup */
    		spi-cpha;
    		// spi-max-frequency = <10000000>;
    
    		/* Clocks */
    		clocks = <&ad9361_clkin 0>;
    		clock-names = "ad9361_ext_refclk";
    		clock-output-names = "rx_sampl_clk", "tx_sampl_clk";
    		#clock-cells = <1>;
    
    		//adi,debug-mode-enable;
    		/* Digital Interface Control */
    
    		 /* adi,digital-interface-tune-skip-mode:
    		  * 0 = TUNE RX&TX
    		  * 1 = SKIP TX
    		  * 2 = SKIP ALL
    		  */
    		adi,digital-interface-tune-skip-mode = <0>;
    
    		adi,pp-tx-swap-enable;
    		adi,pp-rx-swap-enable;
    		adi,rx-frame-pulse-mode-enable;
    		adi,lvds-mode-enable;
    		adi,lvds-bias-mV = <150>;
    		adi,lvds-rx-onchip-termination-enable;
    		adi,rx-data-delay = <4>;
    		adi,tx-fb-clock-delay = <7>;
    
    		//adi,fdd-rx-rate-2tx-enable;
    
    		adi,dcxo-coarse-and-fine-tune = <8 5920>;
    		//adi,xo-disable-use-ext-refclk-enable;
    
    		/* Mode Setup */
    
    		adi,2rx-2tx-mode-enable;
    		//adi,split-gain-table-mode-enable;
    
    		/* ENSM Mode */
    		adi,frequency-division-duplex-mode-enable;
    		//adi,ensm-enable-pin-pulse-mode-enable;
    		//adi,ensm-enable-txnrx-control-enable;
    
    
    		/* adi,rx-rf-port-input-select:
    		 * 0 = (RX1A_N &  RX1A_P) and (RX2A_N & RX2A_P) enabled; balanced
    		 * 1 = (RX1B_N &  RX1B_P) and (RX2B_N & RX2B_P) enabled; balanced
    		 * 2 = (RX1C_N &  RX1C_P) and (RX2C_N & RX2C_P) enabled; balanced
    		 *
    		 * 3 = RX1A_N and RX2A_N enabled; unbalanced
    		 * 4 = RX1A_P and RX2A_P enabled; unbalanced
    		 * 5 = RX1B_N and RX2B_N enabled; unbalanced
    		 * 6 = RX1B_P and RX2B_P enabled; unbalanced
    		 * 7 = RX1C_N and RX2C_N enabled; unbalanced
    		 * 8 = RX1C_P and RX2C_P enabled; unbalanced
    		 */
    
    		adi,rx-rf-port-input-select = <0>; /* (RX1A_N &  RX1A_P) and (RX2A_N & RX2A_P) enabled; balanced */
    
    		/* adi,tx-rf-port-input-select:
    		 * 0	TX1A, TX2A
    		 * 1	TX1B, TX2B
    		 */
    
    		adi,tx-rf-port-input-select = <0>; /* TX1A, TX2A */
    		//adi,update-tx-gain-in-alert-enable;
    		adi,tx-attenuation-mdB = <10000>;
    		adi,tx-lo-powerdown-managed-enable;
    
    		adi,rf-rx-bandwidth-hz = <18000000>;
    		adi,rf-tx-bandwidth-hz = <18000000>;
    		adi,rx-synthesizer-frequency-hz = /bits/ 64 <2400000000>;
    		adi,tx-synthesizer-frequency-hz = /bits/ 64 <2450000000>;
    
    		/*				BBPLL     ADC        R2CLK     R1CLK    CLKRF    RSAMPL  */
    		adi,rx-path-clock-frequencies = <983040000 245760000 122880000 61440000 30720000 30720000>;
    		/*				BBPLL     DAC        T2CLK     T1CLK    CLKTF    TSAMPL  */
    		adi,tx-path-clock-frequencies = <983040000 122880000 122880000 61440000 30720000 30720000>;
    
    		/* Gain Control */
    
    		//adi,gaintable-name = "ad9361_std_gaintable";
    
    		/* adi,gc-rx[1|2]-mode:
    		 * 0 = RF_GAIN_MGC
    		 * 1 = RF_GAIN_FASTATTACK_AGC
    		 * 2 = RF_GAIN_SLOWATTACK_AGC
    		 * 3 = RF_GAIN_HYBRID_AGC
    		 */
    
    		adi,gc-rx1-mode = <2>;
    		adi,gc-rx2-mode = <2>;
    		adi,gc-adc-ovr-sample-size = <4>; /* sum 4 samples */
    		adi,gc-adc-small-overload-thresh = <47>; /* sum of squares */
    		adi,gc-adc-large-overload-thresh = <58>; /* sum of squares */
    		adi,gc-lmt-overload-high-thresh = <800>; /* mV */
    		adi,gc-lmt-overload-low-thresh = <704>; /* mV */
    		adi,gc-dec-pow-measurement-duration = <8192>; /* 0..524288 Samples */
    		adi,gc-low-power-thresh = <24>; /* 0..-64 dBFS vals are set pos */
    		//adi,gc-dig-gain-enable;
    		//adi,gc-max-dig-gain = <15>;
    
    		/* Manual Gain Control Setup */
    
    		//adi,mgc-rx1-ctrl-inp-enable; /* uncomment to use ctrl inputs */
    		//adi,mgc-rx2-ctrl-inp-enable; /* uncomment to use ctrl inputs */
    		adi,mgc-inc-gain-step = <2>;
    		adi,mgc-dec-gain-step = <2>;
    
    		/* adi,mgc-split-table-ctrl-inp-gain-mode:
    		 * (relevant if adi,split-gain-table-mode-enable is set)
    		 * 0 = AGC determine this
    		 * 1 = only in LPF
    		 * 2 = only in LMT
    		 */
    
    		adi,mgc-split-table-ctrl-inp-gain-mode = <0>;
    
    		/* Automatic Gain Control Setup */
    
    		adi,agc-attack-delay-extra-margin-us= <1>; /* us */
    		adi,agc-outer-thresh-high = <5>; /* -dBFS */
    		adi,agc-outer-thresh-high-dec-steps = <2>; /* 0..15 */
    		adi,agc-inner-thresh-high = <10>; /* -dBFS */
    		adi,agc-inner-thresh-high-dec-steps = <1>; /* 0..7 */
    		adi,agc-inner-thresh-low = <12>; /* -dBFS */
    		adi,agc-inner-thresh-low-inc-steps = <1>; /* 0..7 */
    		adi,agc-outer-thresh-low = <18>; /* -dBFS */
    		adi,agc-outer-thresh-low-inc-steps = <2>; /* 0..15 */
    
    		adi,agc-adc-small-overload-exceed-counter = <10>; /* 0..15 */
    		adi,agc-adc-large-overload-exceed-counter = <10>; /* 0..15 */
    		adi,agc-adc-large-overload-inc-steps = <2>; /* 0..15 */
    		//adi,agc-adc-lmt-small-overload-prevent-gain-inc-enable;
    		adi,agc-lmt-overload-large-exceed-counter = <10>; /* 0..15 */
    		adi,agc-lmt-overload-small-exceed-counter = <10>; /* 0..15 */
    		adi,agc-lmt-overload-large-inc-steps = <2>; /* 0..7 */
    		//adi,agc-dig-saturation-exceed-counter = <3>; /* 0..15 */
    		//adi,agc-dig-gain-step-size = <4>; /* 1..8 */
    
    		//adi,agc-sync-for-gain-counter-enable;
    		adi,agc-gain-update-interval-us = <1000>;  /* 1ms */
    		//adi,agc-immed-gain-change-if-large-adc-overload-enable;
    		//adi,agc-immed-gain-change-if-large-lmt-overload-enable;
    
    		/* Fast AGC */
    
    		adi,fagc-dec-pow-measurement-duration = <64>; /* 64 Samples */
                    //adi,fagc-allow-agc-gain-increase-enable;
                    adi,fagc-lp-thresh-increment-steps = <1>;
                    adi,fagc-lp-thresh-increment-time = <5>;
    
                    adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt = <8>;
                    adi,fagc-final-overrange-count = <3>;
                    //adi,fagc-gain-increase-after-gain-lock-enable;
                    adi,fagc-gain-index-type-after-exit-rx-mode = <0>;
                    adi,fagc-lmt-final-settling-steps = <1>;
                    adi,fagc-lock-level = <10>;
                    adi,fagc-lock-level-gain-increase-upper-limit = <5>;
                    adi,fagc-lock-level-lmt-gain-increase-enable;
    
                    adi,fagc-lpf-final-settling-steps = <1>;
                    adi,fagc-optimized-gain-offset = <5>;
                    adi,fagc-power-measurement-duration-in-state5 = <64>;
                    adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable;
                    adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll = <10>;
                    adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable;
                    adi,fagc-rst-gla-if-en-agc-pulled-high-mode = <0>;
                    adi,fagc-rst-gla-large-adc-overload-enable;
                    adi,fagc-rst-gla-large-lmt-overload-enable;
                    adi,fagc-rst-gla-stronger-sig-thresh-above-ll = <10>;
                    adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable;
                    adi,fagc-state-wait-time-ns = <260>;
                    adi,fagc-use-last-lock-level-for-set-gain-enable;
    
    		/* RSSI */
    
    		/* adi,rssi-restart-mode:
    		 * 0 = AGC_IN_FAST_ATTACK_MODE_LOCKS_THE_GAIN,
    		 * 1 = EN_AGC_PIN_IS_PULLED_HIGH,
    		 * 2 = ENTERS_RX_MODE,
    		 * 3 = GAIN_CHANGE_OCCURS,
    		 * 4 = SPI_WRITE_TO_REGISTER,
    		 * 5 = GAIN_CHANGE_OCCURS_OR_EN_AGC_PIN_PULLED_HIGH,
    		 */
    		adi,rssi-restart-mode = <3>;
    		//adi,rssi-unit-is-rx-samples-enable;
    		adi,rssi-delay = <1>; /* 1us */
    		adi,rssi-wait = <1>; /* 1us */
    		adi,rssi-duration = <1000>; /* 1ms */
    
    		/* Control Outputs */
    		adi,ctrl-outs-index = <0>;
    		adi,ctrl-outs-enable-mask = <0xFF>;
    
    		/* AuxADC Temp Sense Control */
    
    		adi,temp-sense-measurement-interval-ms = <1000>;
    		adi,temp-sense-offset-signed = <0xCE>;
    		adi,temp-sense-periodic-measurement-enable;
    
    		/* AuxDAC Control */
    
    		adi,aux-dac-manual-mode-enable;
    
    		adi,aux-dac1-default-value-mV = <0>;
    		//adi,aux-dac1-active-in-rx-enable;
    		//adi,aux-dac1-active-in-tx-enable;
    		//adi,aux-dac1-active-in-alert-enable;
    		adi,aux-dac1-rx-delay-us = <0>;
    		adi,aux-dac1-tx-delay-us = <0>;
    
    		adi,aux-dac2-default-value-mV = <0>;
    		//adi,aux-dac2-active-in-rx-enable;
    		//adi,aux-dac2-active-in-tx-enable;
    		//adi,aux-dac2-active-in-alert-enable;
    		adi,aux-dac2-rx-delay-us = <0>;
    		adi,aux-dac2-tx-delay-us = <0>;
    	};
    };
    
    // &fmc_i2c {
    // 	ad7291@2f {
    // 		compatible = "adi,ad7291";
    // 		reg = <0x2f>;
    // 	};
    
    // 	eeprom@50 {
    // 		compatible = "at24,24c02";
    // 		reg = <0x50>;
    // 	};
    // };
    
    
    
    
    
    
    
    #include "zynq-7000.dtsi"
    
    / {
    	interrupt-parent = <&intc>;
    
    	aliases: aliases {
    		ethernet0 = &gem0;
    		serial0 = &uart0;
    	};
    };
    
    &gem0 {
    	status = "okay";
    };
    
    &clkc {
    	ps-clk-frequency = <33333333>;
    };
    
    // &usb0 {
    // 	status = "okay";
    // 	dr_mode = "host"; /* This breaks OTG mode */
    // };
    
    &uart0 {
    	status = "okay";
    };
    
    &sdhci0 {
    	status = "okay";
    };
    
    
    
    
    
    
    
    
    
    #include "zynq.dtsi"
    
    #include <dt-bindings/interrupt-controller/irq.h>
    
    / {
    	model = "Xilinx Zynq ZC706";
    	memory {
    		device_type = "memory";
    		reg = <0x00000000 0x20000000>;
    	};
    
    	 chosen {
    	  bootargs = "earlycon";
    	  stdout-path = "serial0:115200n8";
    	 };
    
    	leds {
    		compatible = "gpio-leds";
    		ds8 {
    			label = "ds12:green";
    			gpios = <&gpio0 61 0>;
    		};
    
    		ds9 {
    			label = "ds15:green";
    			gpios = <&gpio0 62 0>;
    		};
    
    		ds10 {
    			label = "ds16:green";
    			gpios = <&gpio0 63 0>;
    		};
    
    		ds35 {
    			label = "ds17:green";
    			gpios = <&gpio0 64 0>;
    		};
    	};
    
    	gpio_keys {
    		compatible = "gpio-keys";
    		#address-cells = <1>;
    		#size-cells = <0>;
    		autorepeat;
    
    		sw7 {
    			label = "Left";
    			linux,code = <105>; // Left
    			gpios = <&gpio0 58 0>;
    		};
    
    		sw8 {
    			label = "Right";
    			linux,code = <106>; // Right
    			gpios = <&gpio0 60 0>;
    		};
    
    		sw9 {
    			label = "Select";
    			linux,code = <28>; // Enter
    			gpios = <&gpio0 59 0>;
    		};
    	};
    };
    
    &gem0 {
    	phy-handle = <&phy0>;
    	phy-mode = "rgmii-id";
    
    	phy0: phy@7 {
    		device_type = "ethernet-phy";
    		reg = <0x7>;
    	};
    };
    
    // &usb0 {
    // 	xlnx,phy-reset-gpio = <&gpio0 7 0>;
    // };
    
    &qspi {
    	status = "okay";
    	is-dual = <1>;
    	num-cs = <1>;
    	primary_flash: ps7-qspi@0 {
    		#address-cells = <1>;
    		#size-cells = <1>;
    		spi-tx-bus-width = <4>;
    		spi-rx-bus-width = <4>;
    		compatible = "n25q128a11";
    		reg = <0x0>;
    		// spi-max-frequency = <50000000>;
    		// partition@0 {
    		// 	label = "boot";
    		// 	reg = <0x00000000 0x00500000>;
    		// };
    		// partition@500000 {
    		// 	label = "bootenv";
    		// 	reg = <0x00500000 0x00020000>;
    		// };
    		// partition@520000 {
    		// 	label = "config";
    		// 	reg = <0x00520000 0x00020000>;
    		// };
    		// partition@540000 {
    		// 	label = "image";
    		// 	reg = <0x00540000 0x00a80000>;
    		// };
    		// partition@fc0000 {
    		// 	label = "spare";
    		// 	reg = <0x00fc0000 0x00000000>;
    		// };
    	};
    };
    
    
    
    #include <dt-bindings/interrupt-controller/irq.h>
    
    / {
    	fpga_axi: fpga-axi@0 {
    		compatible = "simple-bus";
    		#address-cells = <0x1>;
    		#size-cells = <0x1>;
    		ranges;
    
    		// i2c@41600000 {
    		// 	compatible = "xlnx,axi-iic-1.02.a", "xlnx,xps-iic-2.00.a";
    		// 	reg = <0x41600000 0x10000>;
    		// 	interrupt-parent = <&intc>;
    		// 	interrupts = <0 58 IRQ_TYPE_LEVEL_HIGH>;
    		// 	clocks = <&clkc 15>;
    		// 	clock-names = "pclk";
    
    		// 	#address-cells = <1>;
    		// 	#size-cells = <0>;
    
    		// 	i2c_mux: i2cswitch@74 {
    		// 		compatible = "nxp,pca9548";
    		// 		#address-cells = <1>;
    		// 		#size-cells = <0>;
    		// 		reg = <0x74>;
    
    		// 		i2c@0 {
    		// 			#address-cells = <1>;
    		// 			#size-cells = <0>;
    		// 			reg = <0>;
    		// 			osc@5d {
    		// 				compatible = "si570";
    		// 				temperature-stability = <50>;
    		// 				reg = <0x5d>;
    		// 				factory-fout = <156250000>;
    		// 				initial-fout = <148500000>;
    		// 			};
    		// 		};
    
    		// 		i2c@1 {
    		// 		    #address-cells = <1>;
    		// 		    #size-cells = <0>;
    		// 		    reg = <1>;
    
    		// 		    adv7511: adv7511@39 {
    		// 				compatible = "adi,adv7511";
    		// 				reg = <0x39>, <0x3f>;
    		// 				reg-names = "primary", "edid";
    
    		// 				adi,input-depth = <8>;
    		// 				adi,input-colorspace = "rgb";
    		// 				adi,input-clock = "1x";
    		// 				adi,clock-delay = <0>;
    
    		// 				#sound-dai-cells = <1>;
    
    		// 				ports {
    		// 					#address-cells = <1>;
    		// 					#size-cells = <0>;
    
    		// 					port@0 {
    		// 						reg = <0>;
    		// 						adv7511_in: endpoint {
    		// 							remote-endpoint = <&axi_hdmi_out>;
    		// 						};
    		// 					};
    
    		// 					port@1 {
    		// 						reg = <1>;
    		// 					};
    		// 				};
    		// 		    };
    		// 		};
    
    		// 		i2c@2 {
    		// 			#address-cells = <1>;
    		// 			#size-cells = <0>;
    		// 			reg = <2>;
    		// 			eeprom@54 {
    		// 				compatible = "at,24c08";
    		// 				reg = <0x54>;
    		// 			};
    		// 		};
    
    		// 		i2c@3 {
    		// 			#address-cells = <1>;
    		// 			#size-cells = <0>;
    		// 			reg = <3>;
    		// 			gpio@21 {
    		// 				compatible = "ti,tca6416";
    		// 				reg = <0x21>;
    		// 				gpio-controller;
    		// 				#gpio-cells = <2>;
    		// 			};
    		// 		};
    
    		// 		i2c@4 {
    		// 			#address-cells = <1>;
    		// 			#size-cells = <0>;
    		// 			reg = <4>;
    		// 			rtc@51 {
    		// 				compatible = "nxp,pcf8563";
    		// 				reg = <0x51>;
    		// 			};
    		// 		};
    		// 	};
    		// };
    
    		// hdmi_dma: dma@43000000 {
    		// 	compatible = "adi,axi-dmac-1.00.a";
    		// 	reg = <0x43000000 0x1000>;
    		// 	#dma-cells = <1>;
    		// 	interrupts = <0 59 IRQ_TYPE_LEVEL_HIGH>;
    		// 	clocks = <&clkc 16>;
    
    		// 	adi,channels {
    		// 		#size-cells = <0>;
    		// 		#address-cells = <1>;
    
    		// 		dma-channel@0 {
    		// 			reg = <0>;
    		// 			adi,source-bus-width = <64>;
    		// 			adi,source-bus-type = <0>;
    		// 			adi,destination-bus-width = <64>;
    		// 			adi,destination-bus-type = <1>;
    		// 		};
    		// 	};
    		// };
    
    		// hdmi_clock: axi-clkgen@79000000 {
    		// 	compatible = "adi,axi-clkgen-2.00.a";
    		// 	reg = <0x79000000 0x10000>;
    		// 	#clock-cells = <0>;
    		// 	clocks = <&clkc 15>, <&clkc 16>;
    		// 	clock-names = "s_axi_aclk", "clkin1";
    		// };
    
    		// axi_hdmi@70e00000 {
    		// 	compatible = "adi,axi-hdmi-tx-1.00.a";
    		// 	reg = <0x70e00000 0x10000>;
    		// 	dmas = <&hdmi_dma 0>;
    		// 	dma-names = "video";
    		// 	clocks = <&hdmi_clock>;
    		// 	adi,is-rgb;
    
    		// 	port {
    		// 		axi_hdmi_out: endpoint {
    		// 			remote-endpoint = <&adv7511_in>;
    		// 		};
    		// 	};
    		// };
    
    		// axi_spdif_tx_0: axi-spdif-tx@75c00000 {
    		// 	compatible = "adi,axi-spdif-tx-1.00.a";
    		// 	reg = <0x75c00000 0x1000>;
    		// 	dmas = <&dmac_s 0>;
    		// 	dma-names = "tx";
    		// 	clocks = <&clkc 15>, <&audio_clock>;
    		// 	clock-names = "axi", "ref";
    
    		// 	#sound-dai-cells = <0>;
    		// };
    
    		axi_sysid_0: axi-sysid-0@45000000 {
    			compatible = "adi,axi-sysid-1.00.a";
    			reg = <0x45000000 0x10000>;
    		};
    
    	};
    
    	// audio_clock: audio_clock {
    	// 	compatible = "fixed-clock";
    	// 	#clock-cells = <0>;
    	// 	clock-frequency = <12288000>;
    	// };
    
    	// adv7511_hdmi_snd {
    	// 	compatible = "simple-audio-card";
    	// 	simple-audio-card,name = "HDMI monitor";
    	// 	simple-audio-card,widgets =
    	// 		"Speaker", "Speaker";
    	// 	simple-audio-card,routing =
    	// 		"Speaker", "TX";
    
    	// 	simple-audio-card,dai-link@0 {
    	// 		format = "spdif";
    	// 		cpu {
    	// 			sound-dai = <&axi_spdif_tx_0>;
    	// 			frame-master;
    	// 			bitclock-master;
    	// 		};
    	// 		codec {
    	// 			sound-dai = <&adv7511 1>;
    	// 		};
    	// 	};
    	// };
    };
    
    
    
    /*
     * FMCOMMS3 optional Up/Down Converter PMOD
     */
    / {
    	clocks {
    		adf4351_clkin: clock@1 {
    			compatible = "fixed-clock";
    
    			clock-frequency = <25000000>;
    			clock-output-names = "refclk";
    			#clock-cells = <0>;
    		};
    	};
    };
    
    // &pmod_spi {
    // 		lo_pll0_tx_adf4351: adf4351-udc-tx-pmod@0 {
    // 			compatible = "adi,adf4351";
    // 			reg = <0>;
    
    // 			spi-max-frequency = <10000000>;
    
    // 			clocks = <&adf4351_clkin>;
    // 			clock-names = "clkin";
    
    // 			adi,channel-spacing = <1000000>;
    // 			adi,power-up-frequency = <370000000>;
    // 			adi,phase-detector-polarity-positive-enable;
    // 			adi,charge-pump-current = <2500>;
    // 			adi,output-power = <3>;
    // 			adi,mute-till-lock-enable;
    // 			adi,muxout-select = <6>;
    // 		};
    
    // 		lo_pll0_rx_adf4351: adf4351-udc-rx-pmod@1 {
    // 			compatible = "adi,adf4351";
    // 			reg = <1>;
    
    // 			spi-max-frequency = <10000000>;
    
    // 			clocks = <&adf4351_clkin>;
    // 			clock-names = "clkin";
    
    // 			adi,channel-spacing = <1000000>;
    // 			adi,power-up-frequency = <340000000>;
    // 			adi,phase-detector-polarity-positive-enable;
    // 			adi,charge-pump-current = <2500>;
    // 			adi,output-power = <3>;
    // 			adi,mute-till-lock-enable;
    // 			adi,muxout-select = <6>;
    // 		};
    // };
    
    



  • Can you set adi,digital-interface-tune-skip to 2 then manually run a tune post boot and post results here: Digital Interface Timing Verification [Analog Devices Wiki]

    At boot can you verify that RESETB is toggled as well.

    -Travis

  • Initially resetb didn't work for me, but I rebuilt the project on other gpios and it worked for me (for some reason, gpios > 40 don't work, although 64 are used in the project).
    As you can see in the log, I do not have device1, and nothing happens to device0.


    Log:

    Registering SWP/SWPB emulation handler
    of-fpga-region fpga-full: FPGA Region probed
    cf_axi_adc 79020000.cf-ad9361-lpc: ADI AIM (10.02.b) at 0x79020000 mapped to 0x(ptrval) probed ADC AD9361 as MASTER
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    of_cfs_init
    of_cfs_init: OK
    ALSA device list:
      No soundcards found.
    RAMDISK: gzip image found at block 0
    using deprecated initrd support, will be removed in 2021.
    EXT4-fs (ram0): mounting ext2 file system using the ext4 subsystem
    EXT4-fs (ram0): mounted filesystem without journal. Opts: (null)
    VFS: Mounted root (ext2 filesystem) on device 1:0.
    Starting rcS...
    ++ Mounting filesystem
    mount: mounting /dev/mmcblk0p1 on /mnt failed: Invalid argument
    mount: mounting /dev/mmcblk0 on /mnt failed: Invalid argument
    ++ Setting up mdev
    /etc/init.d/rcS: line 12: can't create /proc/sys/kernel/hotplug: nonexistent directory
    ++ Starting telnet daemon
    ++ Starting http daemon
    ++ Starting ftp daemon
    ++ Starting ssh daemon
    random: sshd: uninitialized urandom read (32 bytes read)
    rcS Complete
    zynq> mount -t debugfs none /sys/kernel/debug
    zynq> cd /sys/kernel/debug/
    zynq> ls
    adi_axi_data_offload  dmaengine             pinctrl
    asoc                  dri                   pmbus
    bdi                   f8003000.dmac         pwm
    block                 fault_around_bytes    regmap
    cec                   gpio                  regulator
    clear_warn_once       hid                   sleep_time
    clk                   iio                   suspend_stats
    device_component      memblock              usb
    devices_deferred      mmc0                  wakeup_sources
    dma_buf               mtd
    zynq> cd iio/
    zynq> cd iio\:device
    iio:device0/  iio:device2/  iio:device3/
    zynq> cd iio\:device0
    zynq> dmesg -n7
    zynq> echo 0 3 > digital_tune
    zynq> echo 1 3 > digital_tune
    zynq>

  • ad9361 spi0.0: ad9361_spi_write: reg 0x138 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x13A val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x139 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x13B val 0x3E
    ad9361 spi0.0: ad9361_spi_write: reg 0x13F val 0x6
    ad9361 spi0.0: ad9361_spi_write: reg 0x13C val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x13C val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x13F val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x13C val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x13C val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x13F val 0x0
    ad9361 spi0.0: ad9361_gc_setup
    ad9361 spi0.0: ad9361_spi_write: reg 0xFA val 0xEA
    ad9361 spi0.0: ad9361_spi_readm: reg 0xFB val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0xFB val 0x8
    ad9361 spi0.0: ad9361_spi_readm: reg 0xFB val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0xFB val 0x8
    ad9361 spi0.0: ad9361_spi_readm: reg 0xFB val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0xFB val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0xFC val 0x23
    ad9361 spi0.0: ad9361_spi_write: reg 0xFE val 0x20
    ad9361 spi0.0: ad9361_spi_write: reg 0x104 val 0x2F
    ad9361 spi0.0: ad9361_spi_write: reg 0x105 val 0x3A
    ad9361 spi0.0: ad9361_spi_write: reg 0x108 val 0x31
    ad9361 spi0.0: ad9361_spi_readm: reg 0x107 val 0x3F
    ad9361 spi0.0: ad9361_spi_write: reg 0x107 val 0x2B
    ad9361 spi0.0: ad9361_spi_write: reg 0x10B val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x10E val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x114 val 0x30
    ad9361 spi0.0: ad9361_spi_write: reg 0x81 val 0x0
    ad9361 spi0.0: ad9361_spi_readm: reg 0x15C val 0x19
    ad9361 spi0.0: ad9361_spi_write: reg 0x15C val 0x59
    ad9361 spi0.0: ad9361_spi_readm: reg 0x15C val 0x59
    ad9361 spi0.0: ad9361_spi_write: reg 0x15C val 0x79
    ad9361 spi0.0: ad9361_spi_readm: reg 0x15C val 0x79
    ad9361 spi0.0: ad9361_spi_write: reg 0x15C val 0x79
    ad9361 spi0.0: ad9361_spi_readm: reg 0x101 val 0xA
    ad9361 spi0.0: ad9361_spi_write: reg 0x101 val 0xA
    ad9361 spi0.0: ad9361_spi_write: reg 0x120 val 0xC
    ad9361 spi0.0: ad9361_spi_write: reg 0x129 val 0x56
    ad9361 spi0.0: ad9361_spi_write: reg 0x12A val 0x22
    ad9361 spi0.0: ad9361_spi_write: reg 0x123 val 0x11
    ad9361 spi0.0: ad9361_spi_write: reg 0x122 val 0xAA
    ad9361 spi0.0: ad9361_spi_write: reg 0x106 val 0x22
    ad9361 spi0.0: ad9361_spi_write: reg 0x121 val 0xAA
    ad9361 spi0.0: ad9361_spi_readm: reg 0x103 val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0x103 val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0x128 val 0x3
    ad9361 spi0.0: ad9361_spi_readm: reg 0x110 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x110 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x11B val 0x5
    ad9361 spi0.0: ad9361_spi_readm: reg 0x117 val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0x117 val 0x8
    ad9361 spi0.0: ad9361_spi_readm: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_write: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_readm: reg 0x118 val 0x3F
    ad9361 spi0.0: ad9361_spi_write: reg 0x118 val 0x5
    ad9361 spi0.0: ad9361_spi_readm: reg 0x112 val 0x4A
    ad9361 spi0.0: ad9361_spi_write: reg 0x112 val 0x4A
    ad9361 spi0.0: ad9361_spi_readm: reg 0x113 val 0x4A
    ad9361 spi0.0: ad9361_spi_write: reg 0x113 val 0x4A
    ad9361 spi0.0: ad9361_spi_readm: reg 0x116 val 0x65
    ad9361 spi0.0: ad9361_spi_write: reg 0x116 val 0x65
    ad9361 spi0.0: ad9361_spi_readm: reg 0x110 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x110 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x110 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x110 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x110 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x110 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_write: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_readm: reg 0x116 val 0x65
    ad9361 spi0.0: ad9361_spi_write: reg 0x116 val 0x65
    ad9361 spi0.0: ad9361_spi_readm: reg 0xFB val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0xFB val 0x8
    ad9361 spi0.0: ad9361_spi_readm: reg 0x115 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x115 val 0x0
    ad9361 spi0.0: ad9361_spi_readm: reg 0x113 val 0x4A
    ad9361 spi0.0: ad9361_spi_write: reg 0x113 val 0x4A
    ad9361 spi0.0: ad9361_spi_readm: reg 0x112 val 0x4A
    ad9361 spi0.0: ad9361_spi_write: reg 0x112 val 0x4A
    ad9361 spi0.0: ad9361_spi_readm: reg 0x110 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x110 val 0x42
    ad9361 spi0.0: ad9361_spi_readm: reg 0x110 val 0x42
    ad9361 spi0.0: ad9361_spi_write: reg 0x110 val 0x42
    ad9361 spi0.0: ad9361_spi_readm: reg 0x119 val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0x119 val 0x8
    ad9361 spi0.0: ad9361_spi_readm: reg 0x110 val 0x42
    ad9361 spi0.0: ad9361_spi_write: reg 0x110 val 0x40
    ad9361 spi0.0: ad9361_spi_readm: reg 0x114 val 0x30
    ad9361 spi0.0: ad9361_spi_write: reg 0x114 val 0x30
    ad9361 spi0.0: ad9361_spi_readm: reg 0x110 val 0x40
    ad9361 spi0.0: ad9361_spi_write: reg 0x110 val 0x40
    ad9361 spi0.0: ad9361_spi_readm: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_write: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_readm: reg 0x10A val 0x58
    ad9361 spi0.0: ad9361_spi_write: reg 0x10A val 0x58
    ad9361 spi0.0: ad9361_spi_readm: reg 0x109 val 0x4C
    ad9361 spi0.0: ad9361_spi_write: reg 0x109 val 0x4C
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x22 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x22 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0xFE val 0x20
    ad9361 spi0.0: ad9361_spi_write: reg 0xFE val 0x25
    ad9361 spi0.0: ad9361_spi_readm: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_write: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x15C val 0x79
    ad9361 spi0.0: ad9361_spi_write: reg 0x15C val 0x79
    ad9361 spi0.0: ad9361_spi_readm: reg 0x128 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0x128 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0x124 val 0xF4
    ad9361 spi0.0: ad9361_spi_write: reg 0x125 val 0x3B
    ad9361 spi0.0: ad9361_spi_readm: reg 0x117 val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0x117 val 0x8
    ad9361 spi0.0: ad9361_rx_bb_analog_filter_calib : rx_bb_bw 9000000 bbpll_freq 983040000
    ad9361 spi0.0: ad9361_spi_write: reg 0x1F8 val 0x9
    ad9361 spi0.0: ad9361_spi_readm: reg 0x1F9 val 0x1E
    ad9361 spi0.0: ad9361_spi_write: reg 0x1F9 val 0x1E
    ad9361 spi0.0: ad9361_spi_write: reg 0x1FB val 0x9
    ad9361 spi0.0: ad9361_spi_write: reg 0x1FC val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x1D5 val 0x3F
    ad9361 spi0.0: ad9361_spi_write: reg 0x1C0 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0x1E2 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x1E3 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x16 val 0x80
    ad9361 spi0.0: ad9361_run_calibration: CAL Mask 0x80
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x1E2 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0x1E3 val 0x3
    ad9361 spi0.0: ad9361_tx_bb_analog_filter_calib : tx_bb_bw 9000000 bbpll_freq 983040000
    ad9361 spi0.0: ad9361_spi_write: reg 0xD6 val 0x8
    ad9361 spi0.0: ad9361_spi_readm: reg 0xD7 val 0x1E
    ad9361 spi0.0: ad9361_spi_write: reg 0xD7 val 0x1E
    ad9361 spi0.0: ad9361_spi_write: reg 0xCA val 0x22
    ad9361 spi0.0: ad9361_spi_write: reg 0x16 val 0x40
    ad9361 spi0.0: ad9361_run_calibration: CAL Mask 0x40
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0xCA val 0x26
    ad9361 spi0.0: ad9361_spi_readm: reg 0x1EB val 0x0
    ad9361 spi0.0: ad9361_spi_readm: reg 0x1EC val 0x35
    ad9361 spi0.0: ad9361_spi_readm: reg 0x1E6 val 0x1
    ad9361 spi0.0: ad9361_rx_tia_calib : bb_bw_Hz 9000000
    ad9361 spi0.0: ad9361_spi_write: reg 0x1DB val 0x60
    ad9361 spi0.0: ad9361_spi_write: reg 0x1DC val 0x67
    ad9361 spi0.0: ad9361_spi_write: reg 0x1DD val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x1DE val 0x67
    ad9361 spi0.0: ad9361_spi_write: reg 0x1DF val 0x0
    ad9361 spi0.0: ad9361_tx_bb_second_filter_calib : tx_bb_bw 9000000
    ad9361 spi0.0: ad9361_spi_write: reg 0xD0 val 0x56
    ad9361 spi0.0: ad9361_spi_write: reg 0xD1 val 0xC
    ad9361 spi0.0: ad9361_spi_write: reg 0xD2 val 0x17
    ad9361 spi0.0: ad9361_spi_readm: reg 0xA val 0xA
    ad9361 spi0.0: ad9361_spi_readm: reg 0xA val 0xA
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x1EB val 0x0
    ad9361 spi0.0: ad9361_spi_readm: reg 0x1EC val 0x35
    ad9361 spi0.0: ad9361_spi_readm: reg 0x1E6 val 0x1
    ad9361 spi0.0: ad9361_rx_adc_setup : BBBW 8606895 : ADCfreq 245760000
    ad9361 spi0.0: c3_msb 0x0 : c3_lsb 0x35 : r2346 0x1 :
    ad9361 spi0.0: invrc_tconst_1e6 928281, sqrt_inv_rc_tconst_1e3 963
    ad9361 spi0.0: scaled_adc_clk_1e6 384000, inv_scaled_adc_clk_1e3 2604
    ad9361 spi0.0: tmp_1e3 1000, sqrt_term_1e3 619, min_sqrt_term_1e3 1000
    ad9361 spi0.0: ad9361_spi_write: reg 0x200 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x201 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x202 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x203 val 0x24
    ad9361 spi0.0: ad9361_spi_write: reg 0x204 val 0x24
    ad9361 spi0.0: ad9361_spi_write: reg 0x205 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x206 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x207 val 0x79
    ad9361 spi0.0: ad9361_spi_write: reg 0x208 val 0x55
    ad9361 spi0.0: ad9361_spi_write: reg 0x209 val 0x3A
    ad9361 spi0.0: ad9361_spi_write: reg 0x20A val 0x49
    ad9361 spi0.0: ad9361_spi_write: reg 0x20B val 0x35
    ad9361 spi0.0: ad9361_spi_write: reg 0x20C val 0x4C
    ad9361 spi0.0: ad9361_spi_write: reg 0x20D val 0x33
    ad9361 spi0.0: ad9361_spi_write: reg 0x20E val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x20F val 0x7C
    ad9361 spi0.0: ad9361_spi_write: reg 0x210 val 0x7C
    ad9361 spi0.0: ad9361_spi_write: reg 0x211 val 0x7C
    ad9361 spi0.0: ad9361_spi_write: reg 0x212 val 0x47
    ad9361 spi0.0: ad9361_spi_write: reg 0x213 val 0x47
    ad9361 spi0.0: ad9361_spi_write: reg 0x214 val 0x47
    ad9361 spi0.0: ad9361_spi_write: reg 0x215 val 0x4A
    ad9361 spi0.0: ad9361_spi_write: reg 0x216 val 0x4A
    ad9361 spi0.0: ad9361_spi_write: reg 0x217 val 0x4A
    ad9361 spi0.0: ad9361_spi_write: reg 0x218 val 0x2E
    ad9361 spi0.0: ad9361_spi_write: reg 0x219 val 0x98
    ad9361 spi0.0: ad9361_spi_write: reg 0x21A val 0x1B
    ad9361 spi0.0: ad9361_spi_write: reg 0x21B val 0x13
    ad9361 spi0.0: ad9361_spi_write: reg 0x21C val 0x98
    ad9361 spi0.0: ad9361_spi_write: reg 0x21D val 0x1B
    ad9361 spi0.0: ad9361_spi_write: reg 0x21E val 0x13
    ad9361 spi0.0: ad9361_spi_write: reg 0x21F val 0x98
    ad9361 spi0.0: ad9361_spi_write: reg 0x220 val 0x1B
    ad9361 spi0.0: ad9361_spi_write: reg 0x221 val 0x26
    ad9361 spi0.0: ad9361_spi_write: reg 0x222 val 0x27
    ad9361 spi0.0: ad9361_spi_write: reg 0x223 val 0x40
    ad9361 spi0.0: ad9361_spi_write: reg 0x224 val 0x40
    ad9361 spi0.0: ad9361_spi_write: reg 0x225 val 0x2C
    ad9361 spi0.0: ad9361_spi_write: reg 0x226 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x227 val 0x0
    ad9361 spi0.0: ad9361_bb_dc_offset_calib
    ad9361 spi0.0: ad9361_spi_write: reg 0x193 val 0x3F
    ad9361 spi0.0: ad9361_spi_write: reg 0x190 val 0xF
    ad9361 spi0.0: ad9361_spi_write: reg 0x194 val 0x1
    ad9361 spi0.0: ad9361_spi_write: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_run_calibration: CAL Mask 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x0
    ad9361 spi0.0: ad9361_rf_dc_offset_calib : rx_freq 2400000000
    ad9361 spi0.0: ad9361_spi_write: reg 0x185 val 0x20
    ad9361 spi0.0: ad9361_spi_write: reg 0x186 val 0x32
    ad9361 spi0.0: ad9361_spi_write: reg 0x187 val 0x24
    ad9361 spi0.0: ad9361_spi_write: reg 0x188 val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0x18B val 0x83
    ad9361 spi0.0: ad9361_spi_write: reg 0x189 val 0x30
    ad9361 spi0.0: ad9361_spi_write: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_run_calibration: CAL Mask 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x0
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_tx_quad_calib : bw_tx 9000000 clkrf 30720000 clktf 30720000
    ad9361 spi0.0: Tx NCO frequency: 1920000 (BW/4: 2250000) txnco_word 1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0xA3 val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0xA3 val 0x40
    ad9361 spi0.0: ad9361_spi_write: reg 0xA9 val 0xFF
    ad9361 spi0.0: ad9361_spi_write: reg 0xA2 val 0x7F
    ad9361 spi0.0: ad9361_spi_write: reg 0xA5 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0xA6 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0xAA val 0x25
    ad9361 spi0.0: ad9361_spi_write: reg 0xA4 val 0xF0
    ad9361 spi0.0: ad9361_spi_write: reg 0xAE val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0xA0 val 0x3A
    ad9361 spi0.0: ad9361_spi_write: reg 0xA1 val 0x7F
    ad9361 spi0.0: ad9361_spi_write: reg 0xA1 val 0x7B
    ad9361 spi0.0: ad9361_spi_write: reg 0x16 val 0x10
    ad9361 spi0.0: ad9361_run_calibration: CAL Mask 0x10
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x10
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x10
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x10
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x10
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16 val 0x0
    ad9361 spi0.0: ad9361_spi_readm: reg 0xA7 val 0x87
    ad9361 spi0.0: ad9361_spi_readm: reg 0xA8 val 0xD3
    ad9361 spi0.0: LO leakage: 1 Quadrature Calibration: 1 : rx_phase 26
    ad9361 spi0.0: ad9361_tracking_control : bbdc_track=1, rfdc_track=1, rxquad_track=1
    ad9361 spi0.0: ad9361_spi_write: reg 0x16A val 0x75
    ad9361 spi0.0: ad9361_spi_write: reg 0x16B val 0x95
    ad9361 spi0.0: ad9361_spi_write: reg 0x18B val 0xAD
    ad9361 spi0.0: ad9361_spi_readm: reg 0x16F val 0x18
    ad9361 spi0.0: ad9361_spi_write: reg 0x16F val 0x18
    ad9361 spi0.0: ad9361_spi_write: reg 0x169 val 0xCF
    ad9361 spi0.0: ad9361_pp_port_setup
    ad9361 spi0.0: ad9361_spi_write: reg 0x12 val 0x10
    ad9361 spi0.0: ad9361_spi_write: reg 0x13 val 0x1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x15 val 0x4
    ad9361 spi0.0: ad9361_spi_write: reg 0x15 val 0x4
    ad9361 spi0.0: ad9361_spi_readm: reg 0x77 val 0x40
    ad9361 spi0.0: ad9361_spi_write: reg 0x77 val 0x0
    ad9361 spi0.0: ad9361_set_tx_atten : attenuation 10000 mdB tx1=1 tx2=1
    ad9361 spi0.0: ad9361_spi_readm: reg 0x7C val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x7C val 0x0
    ad9361_spi_writem: reg 0x74 val 0x0
    ad9361_spi_writem: reg 0x73 val 0x28
    ad9361_spi_writem: reg 0x76 val 0x0
    ad9361_spi_writem: reg 0x75 val 0x28
    ad9361 spi0.0: ad9361_spi_readm: reg 0x7C val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x7C val 0x40
    ad9361 spi0.0: ad9361_rssi_setup
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_write: reg 0x150 val 0xDE
    ad9361 spi0.0: ad9361_spi_write: reg 0x151 val 0xBC
    ad9361 spi0.0: ad9361_spi_write: reg 0x152 val 0x88
    ad9361 spi0.0: ad9361_spi_write: reg 0x153 val 0x44
    ad9361 spi0.0: ad9361_spi_write: reg 0x154 val 0x22
    ad9361 spi0.0: ad9361_spi_write: reg 0x155 val 0x11
    ad9361 spi0.0: ad9361_spi_write: reg 0x156 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0x157 val 0x7
    ad9361 spi0.0: ad9361_spi_write: reg 0x158 val 0xC
    ad9361 spi0.0: ad9361_spi_readm: reg 0xA val 0xA
    ad9361 spi0.0: ad9361_spi_write: reg 0xA val 0xA
    ad9361 spi0.0: ad9361_txmon_setup
    ad9361 spi0.0: ad9361_spi_write: reg 0x6E val 0x9
    ad9361 spi0.0: ad9361_spi_write: reg 0x69 val 0xFF
    ad9361 spi0.0: ad9361_spi_readm: reg 0x6A val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x6A val 0x1
    ad9361 spi0.0: ad9361_spi_write: reg 0x70 val 0xC2
    ad9361 spi0.0: ad9361_spi_write: reg 0x71 val 0xC2
    ad9361 spi0.0: ad9361_spi_write: reg 0x78 val 0x94
    ad9361 spi0.0: ad9361_spi_write: reg 0x68 val 0x18
    ad9361 spi0.0: ad9361_spi_write: reg 0x67 val 0x0
    ad9361 spi0.0: ad9361_spi_readm: reg 0x17 val 0x15
    ad9361 spi0.0: Device is in 5 state, moving to a
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x29
    ad9361 spi0.0: ad9361_spi_readm: reg 0x37 val 0xA
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_probe : AD936x Rev 0 successfully initialized
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x79024000 mapped to 0x(ptrval), probed DDS AD9361
    axi_sysid 45000000.axi-sysid-0: AXI System ID core version (1.01.a) found
    axi_sysid 45000000.axi-sysid-0: [fmcomms2] on [zc706] git branch <hdl_2021_r2> git <d0336c0f6ff88061d906621c11b616145f96358e> clean [2023-05-31 06:28:30] UTC
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    usbcore: registered new interface driver snd-usb-audio
    NET: Registered protocol family 10
    Segment Routing with IPv6
    sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    NET: Registered protocol family 17
    NET: Registered protocol family 36
    Key type dns_resolver registered
    Registering SWP/SWPB emulation handler
    of-fpga-region fpga-full: FPGA Region probed
    ad9361 spi0.0: ad9361_spi_readm: reg 0x17 val 0x1A
    ad9361 spi0.0: ad9361_spi_readm: reg 0x17 val 0x1A
    ad9361 spi0.0: Device is in a state, forcing to 5
    ad9361 spi0.0: ad9361_spi_readm: reg 0x14 val 0x29
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0xD
    ad9361 spi0.0: ad9361_spi_write: reg 0x6 val 0x4
    ad9361 spi0.0: ad9361_spi_write: reg 0x7 val 0x70
    ad9361 spi0.0: ad9361_spi_readm: reg 0x14 val 0x9
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x29
    ad9361 spi0.0: ad9361_set_trx_clock_chain
    ad9361 spi0.0: ad9361_set_trx_clock_chain: 983040000 245760000 122880000 61440000 30720000 30720000
    ad9361 spi0.0: ad9361_set_trx_clock_chain: 983040000 122880000 122880000 61440000 30720000 30720000
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_write: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_write: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x22 val 0x2
    ad9361 spi0.0: ad9361_spi_write: reg 0x22 val 0x2
    ad9361 spi0.0: ad9361_spi_readm: reg 0xFE val 0x25
    ad9361 spi0.0: ad9361_spi_write: reg 0xFE val 0x25
    ad9361 spi0.0: ad9361_spi_readm: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_write: reg 0x111 val 0xCB
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x15C val 0x79
    ad9361 spi0.0: ad9361_spi_write: reg 0x15C val 0x79
    ad9361 spi0.0: ad9361_spi_readm: reg 0x128 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0x128 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0x124 val 0xF4
    ad9361 spi0.0: ad9361_spi_write: reg 0x125 val 0x3B
    ad9361 spi0.0: ad9361_spi_readm: reg 0x117 val 0x8
    ad9361 spi0.0: ad9361_spi_write: reg 0x117 val 0x8
    ad9361 spi0.0: ad9361_rssi_setup
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_write: reg 0x150 val 0xDE
    ad9361 spi0.0: ad9361_spi_write: reg 0x151 val 0xBC
    ad9361 spi0.0: ad9361_spi_write: reg 0x152 val 0x88
    ad9361 spi0.0: ad9361_spi_write: reg 0x153 val 0x44
    ad9361 spi0.0: ad9361_spi_write: reg 0x154 val 0x22
    ad9361 spi0.0: ad9361_spi_write: reg 0x155 val 0x11
    ad9361 spi0.0: ad9361_spi_write: reg 0x156 val 0x3
    ad9361 spi0.0: ad9361_spi_write: reg 0x157 val 0x7
    ad9361 spi0.0: ad9361_spi_write: reg 0x158 val 0xC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x44 val 0x18
    ad9361 spi0.0: ad9361_spi_readm: reg 0x43 val 0x29
    ad9361 spi0.0: ad9361_spi_readm: reg 0x42 val 0x5C
    ad9361 spi0.0: ad9361_spi_readm: reg 0x41 val 0x12
    ad9361 spi0.0: ad9361_spi_readm: reg 0xA val 0xA
    ad9361 spi0.0: ad9361_spi_readm: reg 0xA val 0xA
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x2 val 0xCC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_spi_readm: reg 0x3 val 0xDC
    ad9361 spi0.0: ad9361_auxadc_setup
    ad9361 spi0.0: ad9361_spi_write: reg 0xB val 0xCE
    ad9361 spi0.0: ad9361_spi_write: reg 0xC val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0xD val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0xF val 0x0
    ad9361 spi0.0: ad9361_spi_write: reg 0x1C val 0x18
    ad9361 spi0.0: ad9361_spi_write: reg 0x1D val 0x0
    ad9361 spi0.0: ad9361_spi_readm: reg 0x17 val 0x1A
    ad9361 spi0.0: Device is in a state, forcing to 5
    ad9361 spi0.0: ad9361_spi_readm: reg 0x14 val 0x29
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0xD
    ad9361 spi0.0: ad9361_spi_readm: reg 0x14 val 0x9
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x29
    cf_axi_adc 79020000.cf-ad9361-lpc: ADI AIM (10.02.b) at 0x79020000 mapped to 0x(ptrval) probed ADC AD9361 as MASTER
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    of_cfs_init
    of_cfs_init: OK
    ALSA device list:
    No soundcards found.
    RAMDISK: gzip image found at block 0
    using deprecated initrd support, will be removed in 2021.
    EXT4-fs (ram0): mounting ext2 file system using the ext4 subsystem
    EXT4-fs (ram0): mounted filesystem without journal. Opts: (null)
    VFS: Mounted root (ext2 filesystem) on device 1:0.
    random: sshd: uninitialized urandom read (32 bytes read)
    ad9361 spi0.0: ad9361_spi_readm: reg 0x17 val 0x1A
    ad9361 spi0.0: ad9361_spi_readm: reg 0x17 val 0x1A
    ad9361 spi0.0: Device is in a state, forcing to 5
    ad9361 spi0.0: ad9361_spi_readm: reg 0x14 val 0x29
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0xD
    ad9361 spi0.0: ad9361_spi_write: reg 0x6 val 0x4
    ad9361 spi0.0: ad9361_spi_write: reg 0x7 val 0x70
    ad9361 spi0.0: ad9361_spi_readm: reg 0x14 val 0x9
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x29
    ad9361 spi0.0: ad9361_spi_readm: reg 0x17 val 0x1A
    ad9361 spi0.0: ad9361_spi_readm: reg 0x17 val 0x1A
    ad9361 spi0.0: Device is in a state, forcing to 5
    ad9361 spi0.0: ad9361_spi_readm: reg 0x14 val 0x29
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0xD
    ad9361 spi0.0: ad9361_spi_write: reg 0x6 val 0x4
    ad9361 spi0.0: ad9361_spi_write: reg 0x7 val 0x70
    ad9361 spi0.0: ad9361_spi_readm: reg 0x14 val 0x9
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x5
    ad9361 spi0.0: ad9361_spi_write: reg 0x14 val 0x29
    zynq>

  • Can you run the bist_timing_analysis and provide output as well? Note that not all devices will appear in the sysfs debug as they all won't have debug attrs.

    -Travis

  • zynq> cd iio\:device0
    zynq> echo 1 > bist_random: crng init done
    zynq> echo 1 > bist_timing_analysis
    zynq>
    zynq> cat bist_t
    bist_timing_analysis bist_tone
    zynq> cat bist_timing_analysis
    ad9361_spi_writem: reg 0x74 val 0x1
    ad9361_spi_writem: reg 0x73 val 0x67
    ad9361_spi_writem: reg 0x76 val 0x1
    ad9361_spi_writem: reg 0x75 val 0x67
    ad9361_spi_writem: reg 0x74 val 0x0
    ad9361_spi_writem: reg 0x73 val 0x28
    ad9361_spi_writem: reg 0x76 val 0x0
    ad9361_spi_writem: reg 0x75 val 0x28
    CLK: 30720000 Hz 'o' = PASS
    DC0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
    0:. . . . . . . . . . . . . . . .
    1:. . . . . . . . . . . . . . . .
    2:. . . . . . . . . . . . . . . .
    3:. . . . . . . . . . . . . . . .
    4:. . . . . . . . . . . . . . . .
    5:. . . . . . . . . . . . . . . .
    6:. . . . . . . . . . . . . . . .
    7:. . . . . . . . . . . . . . . .
    8:. . . . . . . . . . . . . . . .
    9:. . . . . . . . . . . . . . . .
    a:. . . . . . . . . . . . . . . .
    b:. . . . . . . . . . . . . . . .
    c:. . . . . . . . . . . . . . . .
    d:. . . . . . . . . . . . . . . .
    e:. . . . . . . . . . . . . . . .
    f:. . . . . . . . . . . . . . . .

    zynq> cat bist_timing_analysis