Post Go back to editing

Trouble with cf_axi_dds module and modifying JESD204B link parameters

Category: Software
Product Number: AD9136_FMC_EBZ

Hi!

First of all, I would like to express my gratitude for your previous assistance(https://ez.analog.com/linux-software-drivers/f/q-a/569459/kernel-boot-failure-when-adding-a-new-custom-devicetree-with-petalinux), which helped me successfully start Linux and configure the AD9136. However, I am currently facing some issues with the cf_axi_dds module, as I am unable to control the DAC output to achieve the desired waveform.

I noticed that in the tutorial, the normal startup message for DDS should look like this: cf_axi_dds 79024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS master (8.00.b) at 0x79024000 mapped to 0xf0998000, probed DDS AD9361

But in my case, it appears as follows: cf_axi_dds 44a04000.jesd204-transport-layer: Analog Devices CF_AXI_DDS_DDS master (9.01.b) at 0x44A04000 mapped to 0x(ptrval), probed DDS (null)

Therefore, I believe this discrepancy might be the cause of the issue.What steps should I take to resolve this issue?

Additionally, I would like to know how to modify the parameters of the JESD204B link. For example, I would like to set the sampling rate of the AD9136 to 2 GSPS and change the external input reference clock to 250 MHz. Can this be easily configured without modifying the device tree file?

Thank you very much for your assistance.

root@analog:~# dmesg | grep jesd
[    0.280180] jesd204: created con: id=0, topo=0, link=0, /fpga-axi@0/jesd204-phy@44a60000 <-> /fpga-axi@0/jesd204-link-layer@44a90000
[    0.290816] jesd204: created con: id=1, topo=0, link=0, /fpga-axi@0/jesd204-link-layer@44a90000 <-> /fpga-axi@0/jesd204-transport-layer@44a04000
[    0.302494] jesd204: created con: id=2, topo=0, link=0, /fpga-axi@0/jesd204-transport-layer@44a04000 <-> /axi/spi@e0006000/dac@1
[    0.312785] jesd204: /axi/spi@e0006000/dac@1: JESD204[0:0] transition uninitialized -> initialized
[    0.320441] jesd204: found 4 devices and 1 topologies
[    1.256420] axi_adxcvr 44a60000.jesd204-phy: AXI-ADXCVR-TX (17.05.a) using QPLL on GTX2 at 0x44A60000. Number of lanes: 8.
[    1.267116] axi-jesd204-tx 44a90000.jesd204-link-layer: AXI-JESD204-TX (1.06.a) at 0x44A90000. Encoder 8b10b, width 4/4, lanes 8, jesd204-fsm.
[    1.393115] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition initialized -> probed
[    1.402261] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition probed -> idle
[    1.410825] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition idle -> device_init
[    1.419810] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition device_init -> link_init
[    1.429226] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition link_init -> link_supported
[    1.438916] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition link_supported -> link_pre_setup
[    1.449023] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition link_pre_setup -> clk_sync_stage1
[    1.459220] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition clk_sync_stage1 -> clk_sync_stage2
[    1.469498] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage3
[    1.521771] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition clk_sync_stage3 -> link_setup
[    1.531630] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition link_setup -> opt_setup_stage1
[    1.541567] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition opt_setup_stage1 -> opt_setup_stage2
[    1.552018] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition opt_setup_stage2 -> opt_setup_stage3
[    1.562468] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition opt_setup_stage3 -> opt_setup_stage4
[    1.572928] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition opt_setup_stage4 -> opt_setup_stage5
[    1.583380] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition opt_setup_stage5 -> clocks_enable
[    1.593648] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition clocks_enable -> link_enable
[    1.651875] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition link_enable -> link_running
[    1.661545] jesd204: /axi/spi@e0006000/dac@1,jesd204:0,parent=spi0.1: JESD204[0:0] transition link_running -> opt_post_running_stage
[    1.672175] cf_axi_dds 44a04000.jesd204-transport-layer: Analog Devices CF_AXI_DDS_DDS MASTER (9.01.b) at 0x44A04000 mapped to 0x(ptrval), probed DDS (null)
root@analog:~# dmesg | grep 9144
[    1.632875] ad9144 spi0.1: Link0 code grp sync: ff
[    1.636360] ad9144 spi0.1: Link0 frame sync stat: ff
[    1.640014] ad9144 spi0.1: Link0 good checksum stat: ff
[    1.643948] ad9144 spi0.1: Link0 init lane_sync stat: ff
[    1.647949] ad9144 spi0.1: Link0 8 lanes @ 3500000 kBps
root@analog:~# jesd204_status
-bash: jesd204_status: command not found
root@analog:~# jesd_status
┌──────────────────────────────────────────────────────────────────────────────┐
│┌(DEVICES) Found 1 JESD204 Link Layer peripherals────────────────────────────┐│
││                                                                            ││
││(0): axi-jesd204-tx/44a90000.jesd204-link-layer  [*]                        ││
│└────────────────────────────────────────────────────────────────────────────┘│
│┌(STATUS)────────────────────────────────────────────────────────────────────┐│
││Link is                      enabled                                        ││
││Link Status                  DATA                                           ││
││Measured Link Clock (MHz)    87.502                                         ││
││Reported Link Clock (MHz)    87.500                                         ││
││Measured Device Clock (MHz)  87.502                                         ││
││Reported Device Clock (MHz)  87.500                                         ││
││Desired Device Clock (MHz)   87.500                                         ││
││Lane rate (MHz)              3500.000                                       ││
││Lane rate / 40 (MHz)         87.500                                         ││
││LMFC rate (MHz)              10.937                                         ││
││SYSREF captured              Yes                                            ││
││SYSREF alignment error       No                                             ││
││SYNC~                        deasserted                                     ││
│└────────────────────────────────────────────────────────────────────────────┘│
│                                                                              │
│You can also use 'q' to quit and 'a' or 'd' to move between devices!          │
│F1axi-jesd204-tx/44a90000.jesd204-link-layerF9Quit                            │
└──────────────────────────────────────────────────────────────────────────────┘

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.