Post Go back to editing

ALSA Driver and ADAU1761 Sample Rate

Category: Software
Product Number: ADAU1761
Software Version: Kuiper Linux

Is it possible to set the sample rate in ADAU1761 via the ALSA driver supplied with Kuiper Linux?  I don't see a control for it when running amixer controls.  If it cannot be controlled via the driver, is it best to just set this via an I2C write?  I want to use 44.1kHz rather than the default 48kHz

Regards

Andy