Post Go back to editing

changing sample rates in AD9695_FMC example

Category: Software
Product Number: ad9695-625
Software Version: kupier master
  • setup
    • kupier Linux
      • ad9695 Boot.bin, devicetree, zynqmp common ...
      • zcu102 with ad9695-625
    • hardware setup, and software settings, per ad9695_fmc example wiki documentation

when I boot this I can talk to the SPI and see the iio interface but I don't get any data when using iio_scope, obviously because the device is overclocked.

to change the clocks I used/calculated the relationships to the lane rate and selected a mid range lane rate for the 625MSPS board. I verified the synchrona can output these frequencies:

  • SYSREF: 1.5625 MHZ (Lane Rate/256)
  • REFCLK: 100MHz (Lane Rate/40)
  • DEVICECLK: 100MHz (Lane Rate/40)
  • ADCCLK: 400MHz (Lane Rate/10)
  • JESD204B Lane Rate: 4Gbps

I searched the decompiled device tree and found entries matching the old clock numbers in these locations:

phandle originals  value decimal alias
X22 ADC_SYSREF 4D7C6D 5078125 clk 2 and spi
X40 DEV_CLK 135F1B40 325000000 clk 1
setting in spi interface ADCCLK 4D7C6D00 1300000000 spi sample rate

I changed these to the new clock frequencies accordingly

I went through the HDL documentation and scrips to change the JESD transceiver clocks to reflect these new values

when this didnt work I also changed the constraints files clock rates system clock period to 10ns and spi1.0 clock rate to 130ns (though I changed the spi clock after failure)

all of this leads to a failure to set up the spi interface. I have attached original vs new: tcl scripts, device trees, and system boot text. can anyone tell me what Im missing or what Im doing wrong?

7411.files.zip

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.