I've tried using the meta-adi repo/layers to add to our petalinux 2021.1 to no avail.
I then realize that the board we are using "zcu-106" is not supported.
What are the steps to add support for it?
Thanks
pat
AD9625
Recommended for New Designs
The AD9625 is a 12-bit monolithic sampling analog-to-digital converter (ADC) that operates at conversion rates of up to 2.6 giga samples per second (GSPS...
Datasheet
AD9625 on Analog.com
I've tried using the meta-adi repo/layers to add to our petalinux 2021.1 to no avail.
I then realize that the board we are using "zcu-106" is not supported.
What are the steps to add support for it?
Thanks
pat
Hi pat,
Please check this documentation for that. Come back with potential questions you have after reading it.
- Nuno Sá
Thanks for the response. However, I have had no luck getting my device-tree to build.
I've followed the instruction,
My device tree is auto-generated when I do the build and it is called system-top.dts from the imported xsa file I get from the FPGA member of my team.
I've created a file pl-delete-nodes-system-top.dtsi, under project-spec/meta-user/recipes-bsp/device-tree/files
Added it to the bbfile
SRC_URI_append = "file://config \
file://system-user.dtsi \
file://pl-delete-nodes-system-top.dtsi"
When I do petalinux-build -c device-tree I get lots of errors:
.....
cp: '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu1275-revA.dts' and '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu1275-revA.dts' are the same file
cp: '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu1275-revB.dts' and '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu1275-revB.dts' are the same file
cp: '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu1285-revA.dts' and '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu1285-revA.dts' are the same file
cp: '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu208-revA.dts' and '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu208-revA.dts' are the same file
cp: '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu216-revA.dts' and '/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/zynqmp-zcu216-revA.dts' are the same file
WARNING: /home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/temp/run.do_configure.633388:203 exit 1 from 'cp -rf "/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/"* "/home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/"'
WARNING: Backtrace (BB generated script):
#1: do_configure, /home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/temp/run.do_configure.633388, line 203
#2: main, /home/pat/tof-os-2021.1/build/tmp/work/zcu106-xilinx-linux/device-tree/xilinx-v2021.1+gitAUTOINC+252758eb1f-r0/temp/run.do_configure.633388, line 290
Backtrace (metadata-relative locations):
#1: do_configure, /home/pat/tof-os-2021.1/components/yocto/layers/meta-xilinx-tools/classes/xsctbase.bbclass, line 81
Hi Pat,
sorry for the late reply...
My device tree is auto-generated when I do the build and it is called system-top.dts from the imported xsa file I get from the FPGA member of my team.
No, that is not the dts you should be looking at. You should look at pl.dtsi and remove those nodes.
- Nuno Sá
Hi Pat,
sorry for the late reply...
My device tree is auto-generated when I do the build and it is called system-top.dts from the imported xsa file I get from the FPGA member of my team.
No, that is not the dts you should be looking at. You should look at pl.dtsi and remove those nodes.
- Nuno Sá