Post Go back to editing

Replicating IIO-Oscilloscope configurations on PetaLinux

Category: Software
Product Number: ADRV9371
Software Version: PetaLinux 2021.1

I have a setup with PetaLinux 2021.1 on top of a ADRV9371+ZCU102 platform, which I can configure remotely through Ethernet via IIO-Oscilloscope.

My question is:

  • How can I see exacly what the IIO-Oscilloscope configures when a setting change is performed remotely? Basicly what attribute/register write operations are performed and in which order are they? This is so the same can be replicated locally on the board without the need for the IIO-Oscilloscope plugin.

Thanks!

Parents Reply Children
No Data