Post Go back to editing

FMCOMMS5/ZCU706 on remote GNURadio

Hi,

After playing around using Kuiper linux on the board I want to setup a remote connection. I want to run gnuradio-companion on my windows PC through WSL2 and connect it to the ZCU706 via ethernet. The ethernet setup for local connections is working and already installed gnuradio-companion using $ sudo apt install gnuradio. After that  I add to the python path $ export PYTHONPATH=/usr/local/lib/python3.10/dist-packages:$PYTHONPATH  ran gnuradio-companion as follows $ sudo gnuradio-companion. There I just added an FMCOMMS5 sink an one source an connected them. After trying to run the following error appeared: AttributeError: module 'gnuradio.iio' has no attribute 'fmcomms5_source_f32c'. Did you mean: 'fmcomms2_source_fc32'? Did I do something wrong during the installation process? I am aware of https://wiki.analog.com/resources/tools-software/linux-software/gnuradio, but since installing gnuradio using the apt already has the FMCOMSS blocks and in the tutorial only gnuradio 3.7 and 3.8 are mentioned, I don't know what I have to do. 

Thanks in advance, best regards,

Diogo Baptista

Parents Reply
  • Sorry for the delay. Because the .grc file could not be uploaded here, I pasted a wetransfer link and got blocked from sending a reply in this post. This is a second account since the other is blocked.

    Regarding what you asked for, if you really want the .grc file tell me other way to sent it to you. In the mean time, I'm only using an FMCOMMS2/3/4 source block connected to a QT GUI Time Sink or an FMCOMMS5 connected to a QT GUI Time Sink

Children