Post Go back to editing

FMCOMMS5/ZCU706 on remote GNURadio

Hi,

After playing around using Kuiper linux on the board I want to setup a remote connection. I want to run gnuradio-companion on my windows PC through WSL2 and connect it to the ZCU706 via ethernet. The ethernet setup for local connections is working and already installed gnuradio-companion using $ sudo apt install gnuradio. After that  I add to the python path $ export PYTHONPATH=/usr/local/lib/python3.10/dist-packages:$PYTHONPATH  ran gnuradio-companion as follows $ sudo gnuradio-companion. There I just added an FMCOMMS5 sink an one source an connected them. After trying to run the following error appeared: AttributeError: module 'gnuradio.iio' has no attribute 'fmcomms5_source_f32c'. Did you mean: 'fmcomms2_source_fc32'? Did I do something wrong during the installation process? I am aware of https://wiki.analog.com/resources/tools-software/linux-software/gnuradio, but since installing gnuradio using the apt already has the FMCOMSS blocks and in the tutorial only gnuradio 3.7 and 3.8 are mentioned, I don't know what I have to do. 

Thanks in advance, best regards,

Diogo Baptista

Parents
  • Hi Diogo,

    The IIO blocks (including the ones for the FMCOMMS5) are already provided by GnuRadio 3.10, so there shouldn't be anything to install aside (as I understand you manually installed gr-iio in /usr/local/lib/python3.10/dist-packages). You only have to install the "libgnuradio-iio3.xxx" package and you should be good to go.

    Cheers,

    -Paul

Reply
  • Hi Diogo,

    The IIO blocks (including the ones for the FMCOMMS5) are already provided by GnuRadio 3.10, so there shouldn't be anything to install aside (as I understand you manually installed gr-iio in /usr/local/lib/python3.10/dist-packages). You only have to install the "libgnuradio-iio3.xxx" package and you should be good to go.

    Cheers,

    -Paul

Children