Post Go back to editing

meta-adi master branch fails to build on Petalinux 2021.2

Category: Software
Software Version: 2021r2

Hi,

due to an issue with the HDL Coder targeting workflow for ZCU102+ADRV9002 I am using the main branch for the TransceiverToolbox.

Using the TRx main branch together with old Petalinux (2019R1) caused driver compatibility issues that prevented loading any profiles onto the ADRV9002 chip. Moving to 2021R1 didn't really fix the issue: the drivers could not initialize the ADRV9002 AXI IP correctly, failing with error message:

cf_axi_adc: probe of 84a00000.axi-adrv9002-rx-lpc failed with error -5

I then tried to build off of the meta-adi main branch using Petalinux 2021.2. This fails with the following message:

ERROR: Required build target 'petalinux-image-minimal' has no buildable providers.
Missing or unbuildable dependency chain was: ['petalinux-image-minimal', 'libiio-python3']

Any ideas?

Thanks
--
Mariano Maté