ADIS16460
Not Recommended for New Designs
The ADIS16460 iSensor® device is a complete inertial system that includes a triaxial gyroscope and a triaxial accelerometer. Each sensor in the ADIS16460...
Datasheet
ADIS16460 on Analog.com
ADIS16475
Recommended for New Designs
The ADIS16475 is a precision, miniature MEMS inertial measurement unit (IMU) that includes a triaxial gyroscope and a triaxial accelerometer. Each inertial...
Datasheet
ADIS16475 on Analog.com
ADIS16480
Recommended for New Designs
The ADIS16480 iSensor® device is a complete inertial system that includes a triaxial gyroscope, a triaxial accelerometer, triaxial magnetometer, pressure...
Datasheet
ADIS16480 on Analog.com
Hello everyone,
I am trying connecting my ADIS16460 (EVAL-ADISIMU1) to a Raspberrypi 4 (using the ). I had been following the instruction on this guide:
https://wiki.analog.com/resources/tools-software/linux-software/embedded_arm_images?redirect=1
and this video:
Using ADI IMU's with Raspberry Pi and MATLAB - YouTube (2:05 min)
2. I configure my Raspberry pi with overlay in boot/config.txt (dtoverlay=adis16460)
However when I verify that the drivers loaded properly, I obtained an error:
analog@analog:~ $ iio_info
Library version: 0.24 (git tag: cc96e44)
Compiled with backends: local xml ip usb serial
IIO context created with local backend.
Backend version: 0.24 (git tag: cc96e44)
Backend description string: Linux analog 5.10.63-v7l+ #1 SMP Wed Aug 3 14:47:23 UTC 2022 armv7l
IIO context has 4 attributes:
hw_carrier: Raspberry Pi 4 Model B Rev 1.5
dtoverlay: adis16475
local,kernel: 5.10.63-v7l+
uri: local:
IIO context has 3 devices:
hwmon0: cpu_thermal
1 channels found:
temp1: (input)
1 channel-specific attributes found:
attr 0: input value: 49173
No trigger on this device
hwmon1: rpi_volt
1 channels found:
in0: (input)
1 channel-specific attributes found:
attr 0: lcrit_alarm value: 0
No trigger on this device
iio_sysfs_trigger:
0 channels found:
2 device-specific attributes found:
attr 0: add_trigger ERROR: Permission denied (13)
attr 1: remove_trigger ERROR: Permission denied (13)
No trigger on this device
Thank you for your help.
Best regards,
Ingrid M.
Hi Ingrid
2. I configure my Raspberry pi with overlay in boot/config.txt (dtoverlay=adis16460)
Did you created an overlay for adis16460? AFAICT, there's no overlay in the pi branch so I do not thing you'll have on in the sdcard image... That means that no overlay will be loaded during boot and your device won't show up in iio_info since it's not probed.
- Nuno Sá
Ok, thank you so much for your help!
Ok, tahnk you so much. Do you have the adis16460 overlay? (I don't understand very well
that codes)
Sorry for the late reply... Unfortunately, we do not have any overlay for adis16460. However, it should be pretty similar to what we have for the examples I pointed you.
Hello,
I had tried with two codes to see the answer for the IMU, but it continues without working.
I will show you the response of the IMU connected to the raspberry pi when I use the next two codes! The MISO have a offset level, but I don't receive anything!
1. case 1
import sys
import spidev
import RPi.GPIO as GPIO
import time
import array
from struct import *
spi=spidev.SpiDev()
spi.open(0, 0)
spi.max_speed_hz=400000
spi.mode=3
bcmRst=12
GPIO.setup(bcmRst,GPIO.OUT)
GPIO.output(bcmRst,GPIO.HIGH)
while True:
res=spi.wrytebytes([0x56,0x00])
data=spi.readbytes(2)
print(data)
finally:
spi.close()
GPIO.cleanup()


2. case 2
import sys
import spidev
import RPi.GPIO as GPIO
import time
import array
from struct import *
spi=spidev.SpiDev()
spi.open(0, 0)
spi.max_speed_hz=400000
spi.mode=3
bcmRst=12
GPIO.setup(bcmRst,GPIO.OUT)
GPIO.output(bcmRst,GPIO.HIGH)
while True:
res=spi.wrytebytes([0x56,0x00])
res=spi.wrytebytes([0x56,0x00])
finally:
spi.close()
GPIO.cleanup()


I will be very grateful if you can help me or see something strange on the code! I always obtain the same answer.
I will be very attentive. Best regards!
Hello,
I had tried with two codes to see the answer for the IMU, but it continues without working.
I will show you the response of the IMU connected to the raspberry pi when I use the next two codes! The MISO have a offset level, but I don't receive anything!
1. case 1
import sys
import spidev
import RPi.GPIO as GPIO
import time
import array
from struct import *
spi=spidev.SpiDev()
spi.open(0, 0)
spi.max_speed_hz=400000
spi.mode=3
bcmRst=12
GPIO.setup(bcmRst,GPIO.OUT)
GPIO.output(bcmRst,GPIO.HIGH)
while True:
res=spi.wrytebytes([0x56,0x00])
data=spi.readbytes(2)
print(data)
finally:
spi.close()
GPIO.cleanup()


2. case 2
import sys
import spidev
import RPi.GPIO as GPIO
import time
import array
from struct import *
spi=spidev.SpiDev()
spi.open(0, 0)
spi.max_speed_hz=400000
spi.mode=3
bcmRst=12
GPIO.setup(bcmRst,GPIO.OUT)
GPIO.output(bcmRst,GPIO.HIGH)
while True:
res=spi.wrytebytes([0x56,0x00])
res=spi.wrytebytes([0x56,0x00])
finally:
spi.close()
GPIO.cleanup()


I will be very grateful if you can help me or see something strange on the code! I always obtain the same answer.
I will be very attentive. Best regards!
Hi,
Using spidev is not the intended way to use devices and never did it myself. So, I'm not sure what's not working in here but I do know that these parts are typically very sensitive with spi timings and for example, the time delay between cs deassert and assert during a transfer. Another thing worth mentioning is the RST pin... Are you sure that's the correct one? And that the pin is active low?
You might also try to lower the max spi speed to see if it helps.
- Nuno Sá