Hi, We are using a custom board with Zynq SoC XCZU3cg and ADRV 9002. When loading the baremetal(no-os) code via Xilinx Vitis IDE version 2020.2 ,I am getting the following error:
adrv9002_setup,965:failed with "Error occured in Firmware System Code"<65535>.
Detailed error message is attached as text document. What could be the reason for the error?
Kindly provide some insights.
[ERROR]: Error number 3 (0x00000003), Recovery action -101.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_arm.c, in function adi_adrv9001_arm_CmdStatus_Wait, in line 619, variable name device.Error message ArmCmdStatusWait() failed due to thrown ARM error. Is device in correct state for calling command?. [ERROR]: Error number 65535 (0x0000ffff), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/private/src/adrv9001_arm.c, in function adrv9001_ArmCmdErrorHandler, in line 2654, variable name mailboxErrCode.Error message Error occurred in Firmware System code. [ERROR]: Error number 65535 (0x0000ffff), Recovery action -2.In file ../noos/drivers/rf-transceiver/navassa/devices/adrv9001/public/src/adi_adrv9001_cals.c, in function adi_adrv9001_cals_InitCals_Run, in line 103, variable name NULL.Error message Error occurred in Firmware System code. adrv9002_setup, 965: failed with "Error occurred in Firmware System code" (65535)
Thanks.