Post Go back to editing

AD738x Driver and SPI Engine

Category: Software

I am still trying to understand how IIO interacts with the axi-spi-engine platform driver and the ad738x SPI device driver after reading the SPI Engine overview on the Wiki.

The AD738x dual ADC driver at https://github.com/analogdevicesinc/linux/blob/master/drivers/iio/adc/ad738x.c configures the AD738x for 1-wire mode in ad738x_probe().  For my application I would like to configure the device to read conversions in 2-wire mode, and I'm trying to understand what changes are necessary to this driver, as well as the axi-spi-engine, offload, and spi execution HDL components.

If I instead run the AD7380 in 1-wire mode, is it correct that I need to configure the axi-spi-engine, offload, and spi execution components for 1 MISO line?  I currently have them configured with 2 MISO lines.

I read here that the AD7380 driver is not written for support of the offload engine.  What needs to be added to support this? I thought that the offload engine just queues up messages for the execution engine.  Or was that thread referring to DMA offload rather than the offload HDL component?

Note: I am currently running the 5.4 linux-xlnx kernel 2020.1, and  I have enabled support for the axi-spi-engine and dmac in the kernel.  The ad738x.c driver code is from the master branch.

Edit Notes

Clarified
[edited by: ddickerhoof at 12:26 PM (GMT -5) on 18 Jan 2023]
Parents Reply
  • A new question directly related to this is, do I need to set CONFIG_IIO_BUFFER_CB and/or CONFIG_IIO_BUFFER_HW_CONSUMER in the kernel configuration in order to support the SPI Engine/DMA for streaming?  I'm still tracking this down in the kernel code, so I don't fully understand it yet.  I'm not sure if the ADI AXI-DMAC is the hardware buffering that CONFIG_IIO_BUFFER_HW_CONSUMER references, or this is the in-kernel push mechanism that CONFIG_IIO_BUFFER_CB references.

Children