ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
Hi ADI community,
I want to use ZCU102 + ADRV9009 platform for my application. For that, I followed the ADI wiki instructions to download Image Linux on SD card and boot it from ZCU102.
This is my setup :
- 32 Go SD Card
- ADI Image Linux: 2019_R1 (22 June 2020)
- ZCU102 rev 1.1 + ADRV9009.
- IIO OSCILLOSCOPE v1.15
Linux is booted correctly. But when I want to use IIO OSCILLOSCOPE, I have something like this :

When I check iio_attr -d command, I found this :

iio_device3 to iio:device6 are missing (axi-adrv9009-rx-hpc, axi-adrv9009-tx-hpc, adrv9009-phy, axi-adrv9009-rx-obs-hpc).
I've used this version (2019_R1) image Linux in the past and never had this issue before.
Do you have any idea where this comes from? Could be a hardware problem?
I updated the Linux image to KUIPER Linux using the 28 July 2021 version. I booted successfully the Linux. When I check the IIO device, I find this

all IIO devices, but when I used IIO Oscilloscope, I have some errors

I appreciate any feedback from you
Best