Post Go back to editing

Building with Petalinux

Category: Software
Product Number: AD-FMCOMMS4-EBZ
Software Version: 2021.2

I am trying to build petalinux  by using meta-adi-xilinx.

target hardware : zed + FMCOMMS4

Tools : Petalinux tool 2021.2

I followed following instruction.(github.com/.../README.md)

source  <path-to-installed-PetaLinux>/settings.sh
petalinux-create -t project --template <PLATFORM> --name <PROJECT_NAME>, where <PLATFORM> is:
	* zynqMP (for UltraScale + MPSoC)
	* zynq (for Zynq)
	* microblaze (for MicroBlaze)
git clone https://github.com/analogdevicesinc/meta-adi.git
cd <path-to-project>
# Check the Building HDL link below
petalinux-config --get-hw-description=<path to hdf file>
# Select the devicetree that fits the project being built
echo "KERNEL_DTB=\"${dts_to_use}\"" >> project-spec/meta-user/conf/petalinuxbsp.conf
cd build
petalinux-build


But build error was happen.
From error log, some .dtsi file are not exist.
Following file are included from "components/plnx_workspace/device-tree/device-tree/system-top.dts"

  - zynq-zed.dtsi

  - zynq-zed-adv7511.dtsi

  - adi-fmcomms2.dtsi

  - adi-fmcomms3-up-down-converter.dtsi

Correctly include these files, Which file should I use ?  And, How to include  these files ?

Parents Reply Children