Category: Software
Product Number: AD-FMCOMMS4-EBZ
Software Version: 2021.2
I am trying to build petalinux by using meta-adi-xilinx.
target hardware : zed + FMCOMMS4
Tools : Petalinux tool 2021.2
I followed following instruction.(github.com/.../README.md)
source <path-to-installed-PetaLinux>/settings.sh petalinux-create -t project --template <PLATFORM> --name <PROJECT_NAME>, where <PLATFORM> is: * zynqMP (for UltraScale + MPSoC) * zynq (for Zynq) * microblaze (for MicroBlaze) git clone https://github.com/analogdevicesinc/meta-adi.git cd <path-to-project> # Check the Building HDL link below petalinux-config --get-hw-description=<path to hdf file> # Select the devicetree that fits the project being built echo "KERNEL_DTB=\"${dts_to_use}\"" >> project-spec/meta-user/conf/petalinuxbsp.conf cd build petalinux-build
But build error was happen.
From error log, some .dtsi file are not exist.
Following file are included from "components/plnx_workspace/device-tree/device-tree/system-top.dts"
- zynq-zed.dtsi
- zynq-zed-adv7511.dtsi
- adi-fmcomms2.dtsi
- adi-fmcomms3-up-down-converter.dtsi
Correctly include these files, Which file should I use ? And, How to include these files ?