Post Go back to editing

AD9361 TX attenuation set error

Category: Software
Product Number: AD9361

Hello All,

I can't set the attenuation level of the AD9361 TX path to less than 41 dB from the MATLAB interface and I am getting the following failed write error, however the user guide define a maximum of TX attenuation 89.75 dB with lookup table of 360 entries that has 0.25 dB resolution.



And help is highly appreciated!


Kind Regards

Arash



!
[edited by: Arashjafari at 10:02 PM (GMT -5) on 11 Nov 2022]
Parents Reply Children