I am using a ZCU102 board with a AD9371 card and the hdl_2019_R2 and meta-adi 2019_R2, Petalinix 2019.1.
I followed the instructions "github.com/.../README.md" to build the project.
When I build the project the following errors occur:
ERROR: linux-xlnx-4.19-adi_2019_R2+gitAUTOINC+cc28af1e4e-r0 do_fetch: Network access disabled through BB_NO_NETWORK (or set indirectly due to use of BB_FETCH_PREMIRRORONLY) but access requested with command /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -c -P /opt/xilinx/petalinux2019.1/downloads 'petalinux.xilinx.com/.../git2_github.com.analogdevicesinc.linux.git.tar.gz' (for url petalinux.xilinx.com/.../git2_github.com.analogdevicesinc.linux.git.tar.gz)
ERROR: linux-xlnx-4.19-adi_2019_R2+gitAUTOINC+cc28af1e4e-r0 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/cas/AD9371/AD9371_Petalinux/build/tmp/work/plnx_zynqmp-xilinx-linux/linux-xlnx/4.19-adi_2019_R2+gitAUTOINC+cc28af1e4e-r0/temp/log.do_fetch.29002
ERROR: Task (/opt/xilinx/petalinux2019.1/components/yocto/source/aarch64/layers/meta-xilinx/meta-xilinx-bsp/recipes-kernel/linux/linux-xlnx_2019.1.bb:do_fetch) failed with exit code '1'
Could you please help to check where the configration is wrong?
Thank you very much.
Abao
2022.10.18