Post Go back to editing

AD9361: Unhandled case in ad9361_tx_quad_calib

Category: Choose a category
Product Number: ADRV9364
Software Version: Git latest

Our application has a lower RX rate requirement than that for TX. We Monitor RX at a rate of 4 MSPS and when required to transmit, the rate is changed to accommodate TX requirement (4 MSPS to 60000 MSPS) as required. When required to cease transmission, the baseband rate is set to the minimum RX rate of 4 MSPS to save power. On a handful of occasions we have found that an ADRV9364 will not transmit IQ data until the system is rebooted. We have not attempted to cycle the AD9364 ensm_mode to any other states and then back to fdd to see if that resolves the issue largely because we are not able to duplicate it easily and we have no way of knowing when TX channel is non responsive. When TX channel is in this state, no matter what IQ data is sent to the TX channel, the output is a CW. We also see the following kernel messages:

[ 2652.175472] ad9361 spi3.0: Unhandled case in ad9361_tx_quad_calib line 2889 clkrf 3999999 clktf 15999999
[ 2652.213479] ad9361 spi3.0: Unhandled case in ad9361_tx_quad_calib line 2889 clkrf 3999999 clktf 15999999
[ 2652.937384] ad9361 spi3.0: Unhandled case in ad9361_tx_quad_calib line 2889 clkrf 3999999 clktf 15999999
[ 2712.005104] ad9361 spi3.0: Unhandled case in ad9361_tx_quad_calib line 2889 clkrf 3999999 clktf 15999999
[ 2712.042263] ad9361 spi3.0: Unhandled case in ad9361_tx_quad_calib line 2889 clkrf 3999999 clktf 15999999
[ 2712.813428] ad9361 spi3.0: Unhandled case in ad9361_tx_quad_calib line 2889 clkrf 3999999 clktf 15999999

We understand the message from looking at https://github.com/analogdevicesinc/linux/blob/master/drivers/iio/adc/ad9361.c#L2889 but have not idea how clkrf and clktf are selected such that the code ends up in a case that is not handled. And frankly, not sure that would necessarily cause the problem we are experiencing.

Next time the issues occurs, I'll try changing the rate and ensm mode. Any ideas to help us resolve this issue are welcome.



Fix language
[edited by: EdwardK at 5:30 PM (GMT -4) on 5 Oct 2022]

Top Replies

    •  Analog Employees 
    Oct 7, 2022 in reply to EdwardK +1 verified
    Looks like AD9361 Filter Design Wizard creates a filter with parameters that trigger the issue?

    Not directly - but let me explain.

    The RXSAMP and TXSAMP rate must always be equal. In case you…

Parents
  • Wondering do you have a FIR filter loaded with some interpolation or decimation?

    There is only one application controlling the IIO device? Right?

    Can you share more information about this use case?

    I don't think I ever come across something close. 

    -Michael

  • Hi Michael, 

    We have FIR filters but do not use interpolation or decimation. Out filters are asymmetric s in we do not use any in the RX chain and are applied to the TX size only when required to meet meet 3 dB specifications for specific waveforms. These filters were designed using AD9361 Filter Design Wizard 16.1.3-g924f0cd. The TX filters are used in 1 MHz output bandwidth steps from 1 MHz to 40 MHz. I can provide the filters if that helps to look at the setting therein. Note that the issue persists when FIR filters are disabled.

    There is one application controlling the IIO device but it multi threaded to allow logical separation of the RX and TX chains but have a shared lock prior to changing any rates. The RX chain only configures the Fs initially and the TX chain is responsible for rate changes thereafter.

    RX control signal is narrow band FSK or can be a tone. TX can be any modulation from CW to wideband waveforms. Our application is battery powered at as such we need to minimize Fs to reduce power consumption.

Reply
  • Hi Michael, 

    We have FIR filters but do not use interpolation or decimation. Out filters are asymmetric s in we do not use any in the RX chain and are applied to the TX size only when required to meet meet 3 dB specifications for specific waveforms. These filters were designed using AD9361 Filter Design Wizard 16.1.3-g924f0cd. The TX filters are used in 1 MHz output bandwidth steps from 1 MHz to 40 MHz. I can provide the filters if that helps to look at the setting therein. Note that the issue persists when FIR filters are disabled.

    There is one application controlling the IIO device but it multi threaded to allow logical separation of the RX and TX chains but have a shared lock prior to changing any rates. The RX chain only configures the Fs initially and the TX chain is responsible for rate changes thereafter.

    RX control signal is narrow band FSK or can be a tone. TX can be any modulation from CW to wideband waveforms. Our application is battery powered at as such we need to minimize Fs to reduce power consumption.

Children
  • Hi,

    I had a similar setup running today on our test bench.

    Changing baseband rate between 60MSPS and 4MSPS in a tight loop.

    No issues detected while running for 7 hours and exchanging millions of SPI messages.

    # pwd
    /sys/bus/platform/devices/e0006000.spi/spi_master/spi0/statistics

    # grep "" *
    bytes:206676953
    bytes_rx:35620637
    bytes_tx:171056319
    errors:0
    messages:68076769
    spi_async:0
    spi_sync:68076769
    spi_sync_immediate:68076769
    timedout:0
    transfer_bytes_histo_0-1:32951328
    transfer_bytes_histo_1024-2047:0
    transfer_bytes_histo_128-255:0
    transfer_bytes_histo_16-31:0
    transfer_bytes_histo_16384-32767:0
    transfer_bytes_histo_2-3:67854613
    transfer_bytes_histo_2048-4095:0
    transfer_bytes_histo_256-511:0
    transfer_bytes_histo_32-63:0
    transfer_bytes_histo_32768-65535:0
    transfer_bytes_histo_4-7:889450
    transfer_bytes_histo_4096-8191:0
    transfer_bytes_histo_512-1023:0
    transfer_bytes_histo_64-127:0
    transfer_bytes_histo_65536+:0
    transfer_bytes_histo_8-15:0
    transfer_bytes_histo_8192-16383:0
    transfers:101695391
    transfers_split_maxsize:0
    #

    I think the issue on your side could be caused by a SPI issue.

    Can you read all device attributes after the issue happened?

    # cd /sys/bus/iio/devices/iio\:device0
    
    # grep "" *
    
    calib_mode:auto
    
    calib_mode_available:auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
    
    dcxo_tune_coarse_available:[0 0 0]
    
    dcxo_tune_fine_available:[0 0 0]
    
    dev:252:0
    
    ensm_mode:fdd
    
    ensm_mode_available:sleep wait alert fdd pinctrl pinctrl_fdd_indep
    
    filter_fir_config:FIR Rx: 0,0 Tx: 0,0
    
    gain_table_config:<gaintable AD9361 type=FULL dest=3 start=1300000000 end=4000000000>
    
    gain_table_config:-3, 0x00, 0x00, 0x20
    
    gain_table_config:-3, 0x00, 0x00, 0x00
    
    gain_table_config:-3, 0x00, 0x00, 0x00
    
    gain_table_config:-2, 0x00, 0x01, 0x00
    
    gain_table_config:-1, 0x00, 0x02, 0x00
    
    gain_table_config:0, 0x00, 0x03, 0x00
    
    gain_table_config:1, 0x00, 0x04, 0x00
    
    gain_table_config:2, 0x00, 0x05, 0x00
    
    gain_table_config:3, 0x01, 0x03, 0x20
    
    gain_table_config:4, 0x01, 0x04, 0x00
    
    gain_table_config:5, 0x01, 0x05, 0x00
    
    gain_table_config:6, 0x01, 0x06, 0x00
    
    gain_table_config:7, 0x01, 0x07, 0x00
    
    gain_table_config:8, 0x01, 0x08, 0x00
    
    gain_table_config:9, 0x01, 0x09, 0x00
    
    gain_table_config:10, 0x01, 0x0A, 0x00
    
    gain_table_config:11, 0x01, 0x0B, 0x00
    
    gain_table_config:12, 0x01, 0x0C, 0x00
    
    gain_table_config:13, 0x01, 0x0D, 0x00
    
    gain_table_config:14, 0x01, 0x0E, 0x00
    
    gain_table_config:15, 0x02, 0x09, 0x20
    
    gain_table_config:16, 0x02, 0x0A, 0x00
    
    gain_table_config:17, 0x02, 0x0B, 0x00
    
    gain_table_config:18, 0x02, 0x0C, 0x00
    
    gain_table_config:19, 0x02, 0x0D, 0x00
    
    gain_table_config:20, 0x02, 0x0E, 0x00
    
    gain_table_config:21, 0x02, 0x0F, 0x00
    
    gain_table_config:22, 0x02, 0x10, 0x00
    
    gain_table_config:23, 0x02, 0x2B, 0x20
    
    gain_table_config:24, 0x02, 0x2C, 0x00
    
    gain_table_config:25, 0x04, 0x27, 0x20
    
    gain_table_config:26, 0x04, 0x28, 0x00
    
    gain_table_config:27, 0x04, 0x29, 0x00
    
    gain_table_config:28, 0x04, 0x2A, 0x00
    
    gain_table_config:29, 0x04, 0x2B, 0x00
    
    gain_table_config:30, 0x24, 0x21, 0x20
    
    gain_table_config:31, 0x24, 0x22, 0x00
    
    gain_table_config:32, 0x44, 0x20, 0x20
    
    gain_table_config:33, 0x44, 0x21, 0x00
    
    gain_table_config:34, 0x44, 0x22, 0x00
    
    gain_table_config:35, 0x44, 0x23, 0x00
    
    gain_table_config:36, 0x44, 0x24, 0x00
    
    gain_table_config:37, 0x44, 0x25, 0x00
    
    gain_table_config:38, 0x44, 0x26, 0x00
    
    gain_table_config:39, 0x44, 0x27, 0x00
    
    gain_table_config:40, 0x44, 0x28, 0x00
    
    gain_table_config:41, 0x44, 0x29, 0x00
    
    gain_table_config:42, 0x44, 0x2A, 0x00
    
    gain_table_config:43, 0x44, 0x2B, 0x00
    
    gain_table_config:44, 0x44, 0x2C, 0x00
    
    gain_table_config:45, 0x44, 0x2D, 0x00
    
    gain_table_config:46, 0x44, 0x2E, 0x00
    
    gain_table_config:47, 0x44, 0x2F, 0x00
    
    gain_table_config:48, 0x44, 0x30, 0x00
    
    gain_table_config:49, 0x44, 0x31, 0x00
    
    gain_table_config:50, 0x64, 0x2E, 0x20
    
    gain_table_config:51, 0x64, 0x2F, 0x00
    
    gain_table_config:52, 0x64, 0x30, 0x00
    
    gain_table_config:53, 0x64, 0x31, 0x00
    
    gain_table_config:54, 0x64, 0x32, 0x00
    
    gain_table_config:55, 0x64, 0x33, 0x00
    
    gain_table_config:56, 0x64, 0x34, 0x00
    
    gain_table_config:57, 0x64, 0x35, 0x00
    
    gain_table_config:58, 0x64, 0x36, 0x00
    
    gain_table_config:59, 0x64, 0x37, 0x00
    
    gain_table_config:60, 0x64, 0x38, 0x00
    
    gain_table_config:61, 0x65, 0x38, 0x20
    
    gain_table_config:62, 0x66, 0x38, 0x20
    
    gain_table_config:63, 0x67, 0x38, 0x20
    
    gain_table_config:64, 0x68, 0x38, 0x20
    
    gain_table_config:65, 0x69, 0x38, 0x20
    
    gain_table_config:66, 0x6A, 0x38, 0x20
    
    gain_table_config:67, 0x6B, 0x38, 0x20
    
    gain_table_config:68, 0x6C, 0x38, 0x20
    
    gain_table_config:69, 0x6D, 0x38, 0x20
    
    gain_table_config:70, 0x6E, 0x38, 0x20
    
    gain_table_config:71, 0x6F, 0x38, 0x20
    
    gain_table_config:</gaintable>
    
    in_out_voltage_filter_fir_en:0
    
    in_temp0_input:29825
    
    in_voltage0_gain_control_mode:slow_attack
    
    in_voltage0_hardwaregain:71.000000 dB
    
    in_voltage0_hardwaregain_available:[-3 1 71]
    
    in_voltage0_rf_port_select:A_BALANCED
    
    in_voltage0_rssi:122.25 dB
    
    in_voltage2_offset:57
    
    in_voltage2_raw:578
    
    in_voltage2_scale:0.305250
    
    in_voltage_bb_dc_offset_tracking_en:1
    
    in_voltage_filter_fir_en:0
    
    in_voltage_gain_control_mode_available:manual fast_attack slow_attack hybrid
    
    in_voltage_quadrature_tracking_en:1
    
    in_voltage_rf_bandwidth:18000000
    
    in_voltage_rf_bandwidth_available:[200000 1 56000000]
    
    in_voltage_rf_dc_offset_tracking_en:1
    
    in_voltage_rf_port_select_available:A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
    
    in_voltage_sampling_frequency:3999999
    
    in_voltage_sampling_frequency_available:[2083333 1 61440000]
    
    grep: multichip_sync: Permission denied
    
    name:ad9361-phy
    
    out_altvoltage0_RX_LO_external:0
    
    out_altvoltage0_RX_LO_fastlock_load:0
    
    out_altvoltage0_RX_LO_fastlock_save:0 103,103,103,103,103,103,103,103,103,103,103,103,103,103,103,103
    
    out_altvoltage0_RX_LO_fastlock_store:0
    
    out_altvoltage0_RX_LO_frequency:2400000000
    
    out_altvoltage0_RX_LO_frequency_available:[325000000 1 3800000000]
    
    out_altvoltage0_RX_LO_powerdown:0
    
    out_altvoltage1_TX_LO_external:0
    
    out_altvoltage1_TX_LO_fastlock_load:0
    
    out_altvoltage1_TX_LO_fastlock_save:0 94,94,94,94,94,94,94,94,94,94,94,94,94,94,94,94
    
    out_altvoltage1_TX_LO_fastlock_store:0
    
    out_altvoltage1_TX_LO_frequency:2449999998
    
    out_altvoltage1_TX_LO_frequency_available:[325000000 1 3800000000]
    
    out_altvoltage1_TX_LO_powerdown:0
    
    out_voltage0_hardwaregain:-10.000000 dB
    
    out_voltage0_hardwaregain_available:[-89.750000 0.250000 0.000000]
    
    out_voltage0_rf_port_select:A
    
    out_voltage0_rssi:0.00 dB
    
    out_voltage2_raw:306
    
    out_voltage2_scale:1.000000
    
    out_voltage3_raw:306
    
    out_voltage3_scale:1.000000
    
    out_voltage_filter_fir_en:0
    
    out_voltage_rf_bandwidth:18000000
    
    out_voltage_rf_bandwidth_available:[200000 1 40000000]
    
    out_voltage_rf_port_select_available:A B
    
    out_voltage_sampling_frequency:3999999
    
    out_voltage_sampling_frequency_available:[2083333 1 61440000]
    
    rssi_gain_step_error:lna_error: 0 0 0 0
    
    rssi_gain_step_error:mixer_error: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    
    rssi_gain_step_error:gain_step_calib_reg_val: 0 0 0 0 0
    
    rx_path_rates:BBPLL:1023999992 ADC:31999999 R2:15999999 R1:7999999 RF:3999999 RXSAMP:3999999
    
    trx_rate_governor:nominal
    
    trx_rate_governor_available:nominal highest_osr
    
    tx_path_rates:BBPLL:1023999992 DAC:31999999 T2:15999999 T1:7999999 TF:3999999 TXSAMP:3999999
    
    uevent:MAJOR=252
    
    uevent:MINOR=0
    
    uevent:DEVNAME=iio:device0
    
    uevent:DEVTYPE=iio_device
    
    uevent:OF_NAME=ad9361-phy
    
    uevent:OF_FULLNAME=/amba/spi@e0006000/ad9361-phy@0
    
    uevent:OF_COMPATIBLE_0=adi,ad9363a
    
    uevent:OF_COMPATIBLE_N=1
    
    xo_correction:39999990
    
    xo_correction_available:[39991991 1 40007989]
    
    # 
    
    CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.8 | VT102 | Offline | ttyUSB8                                                                                                                                    
    
    
    
    

    And then also a register?

    # iio_reg ad9361-phy 0x37
    0xa
    #

    -Michael
     

  • Thanks, will do as soon as I duplicate the issue

  • One more question do you see this issue only on one setup, or can you replicate this on different units as well?

    -Michael

  • We have seen the issue on multiple SoMs but by far a minority. So out of about 1500 SoMs I'd say that I have seen the issue personally about 20 times. It is likely triggered by a specific sequence in our test is documented and are following.

  • So it appears that we can replicate the "Unhandled case in ad9361_tx_quad_calib" issue on any unit when doing a 1 MHz 99% OBW waveform and likely other bandwidths when doing noise waveforms. Unfortunately, we have not duplicated the unresponsive issue and appears unrealated to the title of this question. Since we are here,

    I collected information you asked for

    SPI interface seems okay:

    adrv9364-m6am-2022Q2 /sys/bus/platform/devices/e0006000.spi/spi_master/spi3/statistics # grep "" *
    bytes:95191733
    bytes_rx:70886250
    bytes_tx:24305486
    errors:0
    messages:12121689
    spi_async:0
    spi_sync:12121689
    spi_sync_immediate:12121689
    timedout:0
    transfer_bytes_histo_0-1:296620
    transfer_bytes_histo_1024-2047:0
    transfer_bytes_histo_128-255:0
    transfer_bytes_histo_16-31:0
    transfer_bytes_histo_16384-32767:0
    transfer_bytes_histo_2048-4095:0
    transfer_bytes_histo_2-3:12120749
    transfer_bytes_histo_256-511:0
    transfer_bytes_histo_32-63:0
    transfer_bytes_histo_32768-65535:0
    transfer_bytes_histo_4096-8191:0
    transfer_bytes_histo_4-7:11766400
    transfer_bytes_histo_512-1023:0
    transfer_bytes_histo_64-127:0
    transfer_bytes_histo_65536+:0
    transfer_bytes_histo_8-15:0
    transfer_bytes_histo_8192-16383:0
    transfers:24183777
    transfers_split_maxsize:0
    

    AD9361 for various configurations:

    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # grep "" *
    calib_mode:auto
    calib_mode_available:auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
    grep: dcxo_tune_coarse: No such device
    dcxo_tune_coarse_available:[0 0 0]
    grep: dcxo_tune_fine: No such device
    dcxo_tune_fine_available:[0 0 0]
    dev:250:0
    ensm_mode:fdd
    ensm_mode_available:sleep wait alert fdd pinctrl pinctrl_fdd_indep
    filter_fir_config:FIR Rx: 0,0 Tx: 64,4
    gain_table_config:<gaintable AD9361 type=FULL dest=3 start=0 end=1300000000>
    gain_table_config:-1, 0x00, 0x00, 0x20
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:0, 0x00, 0x01, 0x00
    gain_table_config:1, 0x00, 0x02, 0x00
    gain_table_config:2, 0x00, 0x03, 0x00
    gain_table_config:3, 0x00, 0x04, 0x00
    gain_table_config:4, 0x00, 0x05, 0x00
    gain_table_config:5, 0x01, 0x03, 0x20
    gain_table_config:6, 0x01, 0x04, 0x00
    gain_table_config:7, 0x01, 0x05, 0x00
    gain_table_config:8, 0x01, 0x06, 0x00
    gain_table_config:9, 0x01, 0x07, 0x00
    gain_table_config:10, 0x01, 0x08, 0x00
    gain_table_config:11, 0x01, 0x09, 0x00
    gain_table_config:12, 0x01, 0x0A, 0x00
    gain_table_config:13, 0x01, 0x0B, 0x00
    gain_table_config:14, 0x01, 0x0C, 0x00
    gain_table_config:15, 0x01, 0x0D, 0x00
    gain_table_config:16, 0x01, 0x0E, 0x00
    gain_table_config:17, 0x02, 0x09, 0x20
    gain_table_config:18, 0x02, 0x0A, 0x00
    gain_table_config:19, 0x02, 0x0B, 0x00
    gain_table_config:20, 0x02, 0x0C, 0x00
    gain_table_config:21, 0x02, 0x0D, 0x00
    gain_table_config:22, 0x02, 0x0E, 0x00
    gain_table_config:23, 0x02, 0x0F, 0x00
    gain_table_config:24, 0x02, 0x10, 0x00
    gain_table_config:25, 0x02, 0x2B, 0x20
    gain_table_config:26, 0x02, 0x2C, 0x00
    gain_table_config:27, 0x04, 0x28, 0x20
    gain_table_config:28, 0x04, 0x29, 0x00
    gain_table_config:29, 0x04, 0x2A, 0x00
    gain_table_config:30, 0x04, 0x2B, 0x00
    gain_table_config:31, 0x24, 0x20, 0x20
    gain_table_config:32, 0x24, 0x21, 0x00
    gain_table_config:33, 0x44, 0x20, 0x20
    gain_table_config:34, 0x44, 0x21, 0x00
    gain_table_config:35, 0x44, 0x22, 0x00
    gain_table_config:36, 0x44, 0x23, 0x00
    gain_table_config:37, 0x44, 0x24, 0x00
    gain_table_config:38, 0x44, 0x25, 0x00
    gain_table_config:39, 0x44, 0x26, 0x00
    gain_table_config:40, 0x44, 0x27, 0x00
    gain_table_config:41, 0x44, 0x28, 0x00
    gain_table_config:42, 0x44, 0x29, 0x00
    gain_table_config:43, 0x44, 0x2A, 0x00
    gain_table_config:44, 0x44, 0x2B, 0x00
    gain_table_config:45, 0x44, 0x2C, 0x00
    gain_table_config:46, 0x44, 0x2D, 0x00
    gain_table_config:47, 0x44, 0x2E, 0x00
    gain_table_config:48, 0x44, 0x2F, 0x00
    gain_table_config:49, 0x44, 0x30, 0x00
    gain_table_config:50, 0x44, 0x31, 0x00
    gain_table_config:51, 0x44, 0x32, 0x00
    gain_table_config:52, 0x64, 0x2E, 0x20
    gain_table_config:53, 0x64, 0x2F, 0x00
    gain_table_config:54, 0x64, 0x30, 0x00
    gain_table_config:55, 0x64, 0x31, 0x00
    gain_table_config:56, 0x64, 0x32, 0x00
    gain_table_config:57, 0x64, 0x33, 0x00
    gain_table_config:58, 0x64, 0x34, 0x00
    gain_table_config:59, 0x64, 0x35, 0x00
    gain_table_config:60, 0x64, 0x36, 0x00
    gain_table_config:61, 0x64, 0x37, 0x00
    gain_table_config:62, 0x64, 0x38, 0x00
    gain_table_config:63, 0x65, 0x38, 0x20
    gain_table_config:64, 0x66, 0x38, 0x20
    gain_table_config:65, 0x67, 0x38, 0x20
    gain_table_config:66, 0x68, 0x38, 0x20
    gain_table_config:67, 0x69, 0x38, 0x20
    gain_table_config:68, 0x6A, 0x38, 0x20
    gain_table_config:69, 0x6B, 0x38, 0x20
    gain_table_config:70, 0x6C, 0x38, 0x20
    gain_table_config:71, 0x6D, 0x38, 0x20
    gain_table_config:72, 0x6E, 0x38, 0x20
    gain_table_config:73, 0x6F, 0x38, 0x20
    gain_table_config:</gaintable>
    in_out_voltage_filter_fir_en:0
    in_temp0_input:44737
    in_voltage0_gain_control_mode:slow_attack
    in_voltage0_hardwaregain:30.000000 dB
    in_voltage0_hardwaregain_available:[-1 1 73]
    in_voltage0_rf_port_select:A_BALANCED
    in_voltage0_rssi:54.25 dB
    in_voltage2_offset:57
    in_voltage2_raw:395
    in_voltage2_scale:0.305250
    in_voltage_bb_dc_offset_tracking_en:1
    in_voltage_filter_fir_en:0
    in_voltage_gain_control_mode_available:manual fast_attack slow_attack hybrid
    in_voltage_quadrature_tracking_en:1
    in_voltage_rf_bandwidth:400000
    in_voltage_rf_bandwidth_available:[200000 1 56000000]
    in_voltage_rf_dc_offset_tracking_en:1
    in_voltage_rf_port_select_available:A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
    in_voltage_sampling_frequency:3999999
    in_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: multichip_sync: Permission denied
    name:ad9361-phy
    grep: of_node: Is a directory
    out_altvoltage0_RX_LO_external:0
    out_altvoltage0_RX_LO_fastlock_load:0
    grep: out_altvoltage0_RX_LO_fastlock_recall: Invalid argument
    out_altvoltage0_RX_LO_fastlock_save:0 252,243,108,159,253,155,211,217,217,223,221,223,248,254,255,110
    out_altvoltage0_RX_LO_fastlock_store:0
    out_altvoltage0_RX_LO_frequency:128400000
    out_altvoltage0_RX_LO_frequency_available:[70000000 1 6000000000]
    out_altvoltage0_RX_LO_powerdown:0
    out_altvoltage1_TX_LO_external:0
    out_altvoltage1_TX_LO_fastlock_load:0
    grep: out_altvoltage1_TX_LO_fastlock_recall: Invalid argument
    out_altvoltage1_TX_LO_fastlock_save:0 100,102,246,255,38,118,230,238,125,254,230,106,102,110,215,182
    out_altvoltage1_TX_LO_fastlock_store:0
    out_altvoltage1_TX_LO_frequency:247999998
    out_altvoltage1_TX_LO_frequency_available:[46875001 1 6000000000]
    out_altvoltage1_TX_LO_powerdown:0
    out_voltage0_hardwaregain:-32.000000 dB
    out_voltage0_hardwaregain_available:[-89.750000 0.250000 0.000000]
    out_voltage0_rf_port_select:A
    out_voltage0_rssi:0.00 dB
    out_voltage2_raw:306
    out_voltage2_scale:1.000000
    out_voltage3_raw:306
    out_voltage3_scale:1.000000
    out_voltage_filter_fir_en:1
    out_voltage_rf_bandwidth:1260770
    out_voltage_rf_bandwidth_available:[200000 1 40000000]
    out_voltage_rf_port_select_available:A B
    out_voltage_sampling_frequency:3999999
    out_voltage_sampling_frequency_available:[520833 1 30720000]
    grep: power: Is a directory
    rssi_gain_step_error:lna_error: 0 0 0 0
    rssi_gain_step_error:mixer_error: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    rssi_gain_step_error:gain_step_calib_reg_val: 0 0 0 0 0
    rx_path_rates:BBPLL:1023999992 ADC:31999999 R2:15999999 R1:7999999 RF:3999999 RXSAMP:3999999
    grep: subsystem: Is a directory
    trx_rate_governor:nominal
    trx_rate_governor_available:nominal highest_osr
    tx_path_rates:BBPLL:1023999992 DAC:31999999 T2:15999999 T1:15999999 TF:15999999 TXSAMP:3999999
    uevent:MAJOR=250
    uevent:MINOR=0
    uevent:DEVNAME=iio:device0
    uevent:DEVTYPE=iio_device
    uevent:OF_NAME=ad9361-phy
    uevent:OF_FULLNAME=/axi/spi@e0006000/ad9361-phy@0
    uevent:OF_COMPATIBLE_0=adi,ad9364
    uevent:OF_COMPATIBLE_N=1
    xo_correction:39999530
    xo_correction_available:[39991531 1 40007529]
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # iio_reg ad9361-phy 0x37
    0xa
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # iio_reg ad9361-phy 0x37
    0xa
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # grep "" *              
    calib_mode:auto
    calib_mode_available:auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
    grep: dcxo_tune_coarse: No such device
    dcxo_tune_coarse_available:[0 0 0]
    grep: dcxo_tune_fine: No such device
    dcxo_tune_fine_available:[0 0 0]
    dev:250:0
    ensm_mode:fdd
    ensm_mode_available:sleep wait alert fdd pinctrl pinctrl_fdd_indep
    filter_fir_config:FIR Rx: 0,0 Tx: 64,4
    gain_table_config:<gaintable AD9361 type=FULL dest=3 start=0 end=1300000000>
    gain_table_config:-1, 0x00, 0x00, 0x20
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:0, 0x00, 0x01, 0x00
    gain_table_config:1, 0x00, 0x02, 0x00
    gain_table_config:2, 0x00, 0x03, 0x00
    gain_table_config:3, 0x00, 0x04, 0x00
    gain_table_config:4, 0x00, 0x05, 0x00
    gain_table_config:5, 0x01, 0x03, 0x20
    gain_table_config:6, 0x01, 0x04, 0x00
    gain_table_config:7, 0x01, 0x05, 0x00
    gain_table_config:8, 0x01, 0x06, 0x00
    gain_table_config:9, 0x01, 0x07, 0x00
    gain_table_config:10, 0x01, 0x08, 0x00
    gain_table_config:11, 0x01, 0x09, 0x00
    gain_table_config:12, 0x01, 0x0A, 0x00
    gain_table_config:13, 0x01, 0x0B, 0x00
    gain_table_config:14, 0x01, 0x0C, 0x00
    gain_table_config:15, 0x01, 0x0D, 0x00
    gain_table_config:16, 0x01, 0x0E, 0x00
    gain_table_config:17, 0x02, 0x09, 0x20
    gain_table_config:18, 0x02, 0x0A, 0x00
    gain_table_config:19, 0x02, 0x0B, 0x00
    gain_table_config:20, 0x02, 0x0C, 0x00
    gain_table_config:21, 0x02, 0x0D, 0x00
    gain_table_config:22, 0x02, 0x0E, 0x00
    gain_table_config:23, 0x02, 0x0F, 0x00
    gain_table_config:24, 0x02, 0x10, 0x00
    gain_table_config:25, 0x02, 0x2B, 0x20
    gain_table_config:26, 0x02, 0x2C, 0x00
    gain_table_config:27, 0x04, 0x28, 0x20
    gain_table_config:28, 0x04, 0x29, 0x00
    gain_table_config:29, 0x04, 0x2A, 0x00
    gain_table_config:30, 0x04, 0x2B, 0x00
    gain_table_config:31, 0x24, 0x20, 0x20
    gain_table_config:32, 0x24, 0x21, 0x00
    gain_table_config:33, 0x44, 0x20, 0x20
    gain_table_config:34, 0x44, 0x21, 0x00
    gain_table_config:35, 0x44, 0x22, 0x00
    gain_table_config:36, 0x44, 0x23, 0x00
    gain_table_config:37, 0x44, 0x24, 0x00
    gain_table_config:38, 0x44, 0x25, 0x00
    gain_table_config:39, 0x44, 0x26, 0x00
    gain_table_config:40, 0x44, 0x27, 0x00
    gain_table_config:41, 0x44, 0x28, 0x00
    gain_table_config:42, 0x44, 0x29, 0x00
    gain_table_config:43, 0x44, 0x2A, 0x00
    gain_table_config:44, 0x44, 0x2B, 0x00
    gain_table_config:45, 0x44, 0x2C, 0x00
    gain_table_config:46, 0x44, 0x2D, 0x00
    gain_table_config:47, 0x44, 0x2E, 0x00
    gain_table_config:48, 0x44, 0x2F, 0x00
    gain_table_config:49, 0x44, 0x30, 0x00
    gain_table_config:50, 0x44, 0x31, 0x00
    gain_table_config:51, 0x44, 0x32, 0x00
    gain_table_config:52, 0x64, 0x2E, 0x20
    gain_table_config:53, 0x64, 0x2F, 0x00
    gain_table_config:54, 0x64, 0x30, 0x00
    gain_table_config:55, 0x64, 0x31, 0x00
    gain_table_config:56, 0x64, 0x32, 0x00
    gain_table_config:57, 0x64, 0x33, 0x00
    gain_table_config:58, 0x64, 0x34, 0x00
    gain_table_config:59, 0x64, 0x35, 0x00
    gain_table_config:60, 0x64, 0x36, 0x00
    gain_table_config:61, 0x64, 0x37, 0x00
    gain_table_config:62, 0x64, 0x38, 0x00
    gain_table_config:63, 0x65, 0x38, 0x20
    gain_table_config:64, 0x66, 0x38, 0x20
    gain_table_config:65, 0x67, 0x38, 0x20
    gain_table_config:66, 0x68, 0x38, 0x20
    gain_table_config:67, 0x69, 0x38, 0x20
    gain_table_config:68, 0x6A, 0x38, 0x20
    gain_table_config:69, 0x6B, 0x38, 0x20
    gain_table_config:70, 0x6C, 0x38, 0x20
    gain_table_config:71, 0x6D, 0x38, 0x20
    gain_table_config:72, 0x6E, 0x38, 0x20
    gain_table_config:73, 0x6F, 0x38, 0x20
    gain_table_config:</gaintable>
    in_out_voltage_filter_fir_en:0
    in_temp0_input:45614
    in_voltage0_gain_control_mode:slow_attack
    in_voltage0_hardwaregain:20.000000 dB
    in_voltage0_hardwaregain_available:[-1 1 73]
    in_voltage0_rf_port_select:A_BALANCED
    in_voltage0_rssi:41.25 dB
    in_voltage2_offset:57
    in_voltage2_raw:366
    in_voltage2_scale:0.305250
    in_voltage_bb_dc_offset_tracking_en:1
    in_voltage_filter_fir_en:0
    in_voltage_gain_control_mode_available:manual fast_attack slow_attack hybrid
    in_voltage_quadrature_tracking_en:1
    in_voltage_rf_bandwidth:400000
    in_voltage_rf_bandwidth_available:[200000 1 56000000]
    in_voltage_rf_dc_offset_tracking_en:1
    in_voltage_rf_port_select_available:A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
    in_voltage_sampling_frequency:25599999
    in_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: multichip_sync: Permission denied
    name:ad9361-phy
    grep: of_node: Is a directory
    out_altvoltage0_RX_LO_external:0
    out_altvoltage0_RX_LO_fastlock_load:0
    grep: out_altvoltage0_RX_LO_fastlock_recall: Invalid argument
    out_altvoltage0_RX_LO_fastlock_save:0 252,243,108,159,253,155,211,217,217,223,221,223,248,254,255,110
    out_altvoltage0_RX_LO_fastlock_store:0
    out_altvoltage0_RX_LO_frequency:868824998
    out_altvoltage0_RX_LO_frequency_available:[70000000 1 6000000000]
    out_altvoltage0_RX_LO_powerdown:0
    out_altvoltage1_TX_LO_external:0
    out_altvoltage1_TX_LO_fastlock_load:0
    grep: out_altvoltage1_TX_LO_fastlock_recall: Invalid argument
    out_altvoltage1_TX_LO_fastlock_save:0 100,102,246,255,38,118,230,238,125,254,230,106,102,110,215,182
    out_altvoltage1_TX_LO_fastlock_store:0
    out_altvoltage1_TX_LO_frequency:1331000000
    out_altvoltage1_TX_LO_frequency_available:[46875001 1 6000000000]
    out_altvoltage1_TX_LO_powerdown:0
    out_voltage0_hardwaregain:-36.500000 dB
    out_voltage0_hardwaregain_available:[-89.750000 0.250000 0.000000]
    out_voltage0_rf_port_select:A
    out_voltage0_rssi:0.00 dB
    out_voltage2_raw:306
    out_voltage2_scale:1.000000
    out_voltage3_raw:306
    out_voltage3_scale:1.000000
    out_voltage_filter_fir_en:0
    out_voltage_rf_bandwidth:5000000
    out_voltage_rf_bandwidth_available:[200000 1 40000000]
    out_voltage_rf_port_select_available:A B
    out_voltage_sampling_frequency:25599999
    out_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: power: Is a directory
    rssi_gain_step_error:lna_error: 0 0 0 0
    rssi_gain_step_error:mixer_error: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    rssi_gain_step_error:gain_step_calib_reg_val: 0 0 0 0 0
    rx_path_rates:BBPLL:819199990 ADC:204799997 R2:102399998 R1:51199999 RF:25599999 RXSAMP:25599999
    grep: subsystem: Is a directory
    trx_rate_governor:nominal
    trx_rate_governor_available:nominal highest_osr
    tx_path_rates:BBPLL:819199990 DAC:204799997 T2:102399998 T1:51199999 TF:25599999 TXSAMP:25599999
    uevent:MAJOR=250
    uevent:MINOR=0
    uevent:DEVNAME=iio:device0
    uevent:DEVTYPE=iio_device
    uevent:OF_NAME=ad9361-phy
    uevent:OF_FULLNAME=/axi/spi@e0006000/ad9361-phy@0
    uevent:OF_COMPATIBLE_0=adi,ad9364
    uevent:OF_COMPATIBLE_N=1
    xo_correction:39999530
    xo_correction_available:[39991531 1 40007529]
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # grep "" *
    calib_mode:auto
    calib_mode_available:auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
    grep: dcxo_tune_coarse: No such device
    dcxo_tune_coarse_available:[0 0 0]
    grep: dcxo_tune_fine: No such device
    dcxo_tune_fine_available:[0 0 0]
    dev:250:0
    ensm_mode:fdd
    ensm_mode_available:sleep wait alert fdd pinctrl pinctrl_fdd_indep
    filter_fir_config:FIR Rx: 0,0 Tx: 64,4
    gain_table_config:<gaintable AD9361 type=FULL dest=3 start=0 end=1300000000>
    gain_table_config:-1, 0x00, 0x00, 0x20
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:0, 0x00, 0x01, 0x00
    gain_table_config:1, 0x00, 0x02, 0x00
    gain_table_config:2, 0x00, 0x03, 0x00
    gain_table_config:3, 0x00, 0x04, 0x00
    gain_table_config:4, 0x00, 0x05, 0x00
    gain_table_config:5, 0x01, 0x03, 0x20
    gain_table_config:6, 0x01, 0x04, 0x00
    gain_table_config:7, 0x01, 0x05, 0x00
    gain_table_config:8, 0x01, 0x06, 0x00
    gain_table_config:9, 0x01, 0x07, 0x00
    gain_table_config:10, 0x01, 0x08, 0x00
    gain_table_config:11, 0x01, 0x09, 0x00
    gain_table_config:12, 0x01, 0x0A, 0x00
    gain_table_config:13, 0x01, 0x0B, 0x00
    gain_table_config:14, 0x01, 0x0C, 0x00
    gain_table_config:15, 0x01, 0x0D, 0x00
    gain_table_config:16, 0x01, 0x0E, 0x00
    gain_table_config:17, 0x02, 0x09, 0x20
    gain_table_config:18, 0x02, 0x0A, 0x00
    gain_table_config:19, 0x02, 0x0B, 0x00
    gain_table_config:20, 0x02, 0x0C, 0x00
    gain_table_config:21, 0x02, 0x0D, 0x00
    gain_table_config:22, 0x02, 0x0E, 0x00
    gain_table_config:23, 0x02, 0x0F, 0x00
    gain_table_config:24, 0x02, 0x10, 0x00
    gain_table_config:25, 0x02, 0x2B, 0x20
    gain_table_config:26, 0x02, 0x2C, 0x00
    gain_table_config:27, 0x04, 0x28, 0x20
    gain_table_config:28, 0x04, 0x29, 0x00
    gain_table_config:29, 0x04, 0x2A, 0x00
    gain_table_config:30, 0x04, 0x2B, 0x00
    gain_table_config:31, 0x24, 0x20, 0x20
    gain_table_config:32, 0x24, 0x21, 0x00
    gain_table_config:33, 0x44, 0x20, 0x20
    gain_table_config:34, 0x44, 0x21, 0x00
    gain_table_config:35, 0x44, 0x22, 0x00
    gain_table_config:36, 0x44, 0x23, 0x00
    gain_table_config:37, 0x44, 0x24, 0x00
    gain_table_config:38, 0x44, 0x25, 0x00
    gain_table_config:39, 0x44, 0x26, 0x00
    gain_table_config:40, 0x44, 0x27, 0x00
    gain_table_config:41, 0x44, 0x28, 0x00
    gain_table_config:42, 0x44, 0x29, 0x00
    gain_table_config:43, 0x44, 0x2A, 0x00
    gain_table_config:44, 0x44, 0x2B, 0x00
    gain_table_config:45, 0x44, 0x2C, 0x00
    gain_table_config:46, 0x44, 0x2D, 0x00
    gain_table_config:47, 0x44, 0x2E, 0x00
    gain_table_config:48, 0x44, 0x2F, 0x00
    gain_table_config:49, 0x44, 0x30, 0x00
    gain_table_config:50, 0x44, 0x31, 0x00
    gain_table_config:51, 0x44, 0x32, 0x00
    gain_table_config:52, 0x64, 0x2E, 0x20
    gain_table_config:53, 0x64, 0x2F, 0x00
    gain_table_config:54, 0x64, 0x30, 0x00
    gain_table_config:55, 0x64, 0x31, 0x00
    gain_table_config:56, 0x64, 0x32, 0x00
    gain_table_config:57, 0x64, 0x33, 0x00
    gain_table_config:58, 0x64, 0x34, 0x00
    gain_table_config:59, 0x64, 0x35, 0x00
    gain_table_config:60, 0x64, 0x36, 0x00
    gain_table_config:61, 0x64, 0x37, 0x00
    gain_table_config:62, 0x64, 0x38, 0x00
    gain_table_config:63, 0x65, 0x38, 0x20
    gain_table_config:64, 0x66, 0x38, 0x20
    gain_table_config:65, 0x67, 0x38, 0x20
    gain_table_config:66, 0x68, 0x38, 0x20
    gain_table_config:67, 0x69, 0x38, 0x20
    gain_table_config:68, 0x6A, 0x38, 0x20
    gain_table_config:69, 0x6B, 0x38, 0x20
    gain_table_config:70, 0x6C, 0x38, 0x20
    gain_table_config:71, 0x6D, 0x38, 0x20
    gain_table_config:72, 0x6E, 0x38, 0x20
    gain_table_config:73, 0x6F, 0x38, 0x20
    gain_table_config:</gaintable>
    in_out_voltage_filter_fir_en:0
    in_temp0_input:45614
    in_voltage0_gain_control_mode:slow_attack
    in_voltage0_hardwaregain:20.000000 dB
    in_voltage0_hardwaregain_available:[-1 1 73]
    in_voltage0_rf_port_select:A_BALANCED
    in_voltage0_rssi:41.25 dB
    in_voltage2_offset:57
    in_voltage2_raw:370
    in_voltage2_scale:0.305250
    in_voltage_bb_dc_offset_tracking_en:1
    in_voltage_filter_fir_en:0
    in_voltage_gain_control_mode_available:manual fast_attack slow_attack hybrid
    in_voltage_quadrature_tracking_en:1
    in_voltage_rf_bandwidth:400000
    in_voltage_rf_bandwidth_available:[200000 1 56000000]
    in_voltage_rf_dc_offset_tracking_en:1
    in_voltage_rf_port_select_available:A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
    in_voltage_sampling_frequency:25599999
    in_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: multichip_sync: Permission denied
    name:ad9361-phy
    grep: of_node: Is a directory
    out_altvoltage0_RX_LO_external:0
    out_altvoltage0_RX_LO_fastlock_load:0
    grep: out_altvoltage0_RX_LO_fastlock_recall: Invalid argument
    out_altvoltage0_RX_LO_fastlock_save:0 252,243,108,159,253,155,211,217,217,223,221,223,248,254,255,110
    out_altvoltage0_RX_LO_fastlock_store:0
    out_altvoltage0_RX_LO_frequency:868824998
    out_altvoltage0_RX_LO_frequency_available:[70000000 1 6000000000]
    out_altvoltage0_RX_LO_powerdown:0
    out_altvoltage1_TX_LO_external:0
    out_altvoltage1_TX_LO_fastlock_load:0
    grep: out_altvoltage1_TX_LO_fastlock_recall: Invalid argument
    out_altvoltage1_TX_LO_fastlock_save:0 100,102,246,255,38,118,230,238,125,254,230,106,102,110,215,182
    out_altvoltage1_TX_LO_fastlock_store:0
    out_altvoltage1_TX_LO_frequency:1331000000
    out_altvoltage1_TX_LO_frequency_available:[46875001 1 6000000000]
    out_altvoltage1_TX_LO_powerdown:0
    out_voltage0_hardwaregain:-36.500000 dB
    out_voltage0_hardwaregain_available:[-89.750000 0.250000 0.000000]
    out_voltage0_rf_port_select:A
    out_voltage0_rssi:0.00 dB
    out_voltage2_raw:306
    out_voltage2_scale:1.000000
    out_voltage3_raw:306
    out_voltage3_scale:1.000000
    out_voltage_filter_fir_en:0
    out_voltage_rf_bandwidth:5000000
    out_voltage_rf_bandwidth_available:[200000 1 40000000]
    out_voltage_rf_port_select_available:A B
    out_voltage_sampling_frequency:25599999
    out_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: power: Is a directory
    rssi_gain_step_error:lna_error: 0 0 0 0
    rssi_gain_step_error:mixer_error: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    rssi_gain_step_error:gain_step_calib_reg_val: 0 0 0 0 0
    rx_path_rates:BBPLL:819199990 ADC:204799997 R2:102399998 R1:51199999 RF:25599999 RXSAMP:25599999
    grep: subsystem: Is a directory
    trx_rate_governor:nominal
    trx_rate_governor_available:nominal highest_osr
    tx_path_rates:BBPLL:819199990 DAC:204799997 T2:102399998 T1:51199999 TF:25599999 TXSAMP:25599999
    uevent:MAJOR=250
    uevent:MINOR=0
    uevent:DEVNAME=iio:device0
    uevent:DEVTYPE=iio_device
    uevent:OF_NAME=ad9361-phy
    uevent:OF_FULLNAME=/axi/spi@e0006000/ad9361-phy@0
    uevent:OF_COMPATIBLE_0=adi,ad9364
    uevent:OF_COMPATIBLE_N=1
    xo_correction:39999530
    xo_correction_available:[39991531 1 40007529]
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # grep "" *
    calib_mode:auto
    calib_mode_available:auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
    grep: dcxo_tune_coarse: No such device
    dcxo_tune_coarse_available:[0 0 0]
    grep: dcxo_tune_fine: No such device
    dcxo_tune_fine_available:[0 0 0]
    dev:250:0
    ensm_mode:fdd
    ensm_mode_available:sleep wait alert fdd pinctrl pinctrl_fdd_indep
    filter_fir_config:FIR Rx: 0,0 Tx: 64,4
    gain_table_config:<gaintable AD9361 type=FULL dest=3 start=0 end=1300000000>
    gain_table_config:-1, 0x00, 0x00, 0x20
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:0, 0x00, 0x01, 0x00
    gain_table_config:1, 0x00, 0x02, 0x00
    gain_table_config:2, 0x00, 0x03, 0x00
    gain_table_config:3, 0x00, 0x04, 0x00
    gain_table_config:4, 0x00, 0x05, 0x00
    gain_table_config:5, 0x01, 0x03, 0x20
    gain_table_config:6, 0x01, 0x04, 0x00
    gain_table_config:7, 0x01, 0x05, 0x00
    gain_table_config:8, 0x01, 0x06, 0x00
    gain_table_config:9, 0x01, 0x07, 0x00
    gain_table_config:10, 0x01, 0x08, 0x00
    gain_table_config:11, 0x01, 0x09, 0x00
    gain_table_config:12, 0x01, 0x0A, 0x00
    gain_table_config:13, 0x01, 0x0B, 0x00
    gain_table_config:14, 0x01, 0x0C, 0x00
    gain_table_config:15, 0x01, 0x0D, 0x00
    gain_table_config:16, 0x01, 0x0E, 0x00
    gain_table_config:17, 0x02, 0x09, 0x20
    gain_table_config:18, 0x02, 0x0A, 0x00
    gain_table_config:19, 0x02, 0x0B, 0x00
    gain_table_config:20, 0x02, 0x0C, 0x00
    gain_table_config:21, 0x02, 0x0D, 0x00
    gain_table_config:22, 0x02, 0x0E, 0x00
    gain_table_config:23, 0x02, 0x0F, 0x00
    gain_table_config:24, 0x02, 0x10, 0x00
    gain_table_config:25, 0x02, 0x2B, 0x20
    gain_table_config:26, 0x02, 0x2C, 0x00
    gain_table_config:27, 0x04, 0x28, 0x20
    gain_table_config:28, 0x04, 0x29, 0x00
    gain_table_config:29, 0x04, 0x2A, 0x00
    gain_table_config:30, 0x04, 0x2B, 0x00
    gain_table_config:31, 0x24, 0x20, 0x20
    gain_table_config:32, 0x24, 0x21, 0x00
    gain_table_config:33, 0x44, 0x20, 0x20
    gain_table_config:34, 0x44, 0x21, 0x00
    gain_table_config:35, 0x44, 0x22, 0x00
    gain_table_config:36, 0x44, 0x23, 0x00
    gain_table_config:37, 0x44, 0x24, 0x00
    gain_table_config:38, 0x44, 0x25, 0x00
    gain_table_config:39, 0x44, 0x26, 0x00
    gain_table_config:40, 0x44, 0x27, 0x00
    gain_table_config:41, 0x44, 0x28, 0x00
    gain_table_config:42, 0x44, 0x29, 0x00
    gain_table_config:43, 0x44, 0x2A, 0x00
    gain_table_config:44, 0x44, 0x2B, 0x00
    gain_table_config:45, 0x44, 0x2C, 0x00
    gain_table_config:46, 0x44, 0x2D, 0x00
    gain_table_config:47, 0x44, 0x2E, 0x00
    gain_table_config:48, 0x44, 0x2F, 0x00
    gain_table_config:49, 0x44, 0x30, 0x00
    gain_table_config:50, 0x44, 0x31, 0x00
    gain_table_config:51, 0x44, 0x32, 0x00
    gain_table_config:52, 0x64, 0x2E, 0x20
    gain_table_config:53, 0x64, 0x2F, 0x00
    gain_table_config:54, 0x64, 0x30, 0x00
    gain_table_config:55, 0x64, 0x31, 0x00
    gain_table_config:56, 0x64, 0x32, 0x00
    gain_table_config:57, 0x64, 0x33, 0x00
    gain_table_config:58, 0x64, 0x34, 0x00
    gain_table_config:59, 0x64, 0x35, 0x00
    gain_table_config:60, 0x64, 0x36, 0x00
    gain_table_config:61, 0x64, 0x37, 0x00
    gain_table_config:62, 0x64, 0x38, 0x00
    gain_table_config:63, 0x65, 0x38, 0x20
    gain_table_config:64, 0x66, 0x38, 0x20
    gain_table_config:65, 0x67, 0x38, 0x20
    gain_table_config:66, 0x68, 0x38, 0x20
    gain_table_config:67, 0x69, 0x38, 0x20
    gain_table_config:68, 0x6A, 0x38, 0x20
    gain_table_config:69, 0x6B, 0x38, 0x20
    gain_table_config:70, 0x6C, 0x38, 0x20
    gain_table_config:71, 0x6D, 0x38, 0x20
    gain_table_config:72, 0x6E, 0x38, 0x20
    gain_table_config:73, 0x6F, 0x38, 0x20
    gain_table_config:</gaintable>
    in_out_voltage_filter_fir_en:0
    in_temp0_input:46491
    in_voltage0_gain_control_mode:slow_attack
    in_voltage0_hardwaregain:20.000000 dB
    in_voltage0_hardwaregain_available:[-1 1 73]
    in_voltage0_rf_port_select:A_BALANCED
    in_voltage0_rssi:41.25 dB
    in_voltage2_offset:57
    in_voltage2_raw:371
    in_voltage2_scale:0.305250
    in_voltage_bb_dc_offset_tracking_en:1
    in_voltage_filter_fir_en:0
    in_voltage_gain_control_mode_available:manual fast_attack slow_attack hybrid
    in_voltage_quadrature_tracking_en:1
    in_voltage_rf_bandwidth:400000
    in_voltage_rf_bandwidth_available:[200000 1 56000000]
    in_voltage_rf_dc_offset_tracking_en:1
    in_voltage_rf_port_select_available:A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
    in_voltage_sampling_frequency:25599999
    in_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: multichip_sync: Permission denied
    name:ad9361-phy
    grep: of_node: Is a directory
    out_altvoltage0_RX_LO_external:0
    out_altvoltage0_RX_LO_fastlock_load:0
    grep: out_altvoltage0_RX_LO_fastlock_recall: Invalid argument
    out_altvoltage0_RX_LO_fastlock_save:0 252,243,108,159,253,155,211,217,217,223,221,223,248,254,255,110
    out_altvoltage0_RX_LO_fastlock_store:0
    out_altvoltage0_RX_LO_frequency:868824998
    out_altvoltage0_RX_LO_frequency_available:[70000000 1 6000000000]
    out_altvoltage0_RX_LO_powerdown:0
    out_altvoltage1_TX_LO_external:0
    out_altvoltage1_TX_LO_fastlock_load:0
    grep: out_altvoltage1_TX_LO_fastlock_recall: Invalid argument
    out_altvoltage1_TX_LO_fastlock_save:0 100,102,246,255,38,118,230,238,125,254,230,106,102,110,215,182
    out_altvoltage1_TX_LO_fastlock_store:0
    out_altvoltage1_TX_LO_frequency:1331000000
    out_altvoltage1_TX_LO_frequency_available:[46875001 1 6000000000]
    out_altvoltage1_TX_LO_powerdown:0
    out_voltage0_hardwaregain:-36.500000 dB
    out_voltage0_hardwaregain_available:[-89.750000 0.250000 0.000000]
    out_voltage0_rf_port_select:A
    out_voltage0_rssi:0.00 dB
    out_voltage2_raw:306
    out_voltage2_scale:1.000000
    out_voltage3_raw:306
    out_voltage3_scale:1.000000
    out_voltage_filter_fir_en:0
    out_voltage_rf_bandwidth:5000000
    out_voltage_rf_bandwidth_available:[200000 1 40000000]
    out_voltage_rf_port_select_available:A B
    out_voltage_sampling_frequency:25599999
    out_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: power: Is a directory
    rssi_gain_step_error:lna_error: 0 0 0 0
    rssi_gain_step_error:mixer_error: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    rssi_gain_step_error:gain_step_calib_reg_val: 0 0 0 0 0
    rx_path_rates:BBPLL:819199990 ADC:204799997 R2:102399998 R1:51199999 RF:25599999 RXSAMP:25599999
    grep: subsystem: Is a directory
    trx_rate_governor:nominal
    trx_rate_governor_available:nominal highest_osr
    tx_path_rates:BBPLL:819199990 DAC:204799997 T2:102399998 T1:51199999 TF:25599999 TXSAMP:25599999
    uevent:MAJOR=250
    uevent:MINOR=0
    uevent:DEVNAME=iio:device0
    uevent:DEVTYPE=iio_device
    uevent:OF_NAME=ad9361-phy
    uevent:OF_FULLNAME=/axi/spi@e0006000/ad9361-phy@0
    uevent:OF_COMPATIBLE_0=adi,ad9364
    uevent:OF_COMPATIBLE_N=1
    xo_correction:39999530
    xo_correction_available:[39991531 1 40007529]
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # grep "" *
    calib_mode:auto
    calib_mode_available:auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
    grep: dcxo_tune_coarse: No such device
    dcxo_tune_coarse_available:[0 0 0]
    grep: dcxo_tune_fine: No such device
    dcxo_tune_fine_available:[0 0 0]
    dev:250:0
    ensm_mode:fdd
    ensm_mode_available:sleep wait alert fdd pinctrl pinctrl_fdd_indep
    filter_fir_config:FIR Rx: 0,0 Tx: 64,4
    gain_table_config:<gaintable AD9361 type=FULL dest=3 start=0 end=1300000000>
    gain_table_config:-1, 0x00, 0x00, 0x20
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:0, 0x00, 0x01, 0x00
    gain_table_config:1, 0x00, 0x02, 0x00
    gain_table_config:2, 0x00, 0x03, 0x00
    gain_table_config:3, 0x00, 0x04, 0x00
    gain_table_config:4, 0x00, 0x05, 0x00
    gain_table_config:5, 0x01, 0x03, 0x20
    gain_table_config:6, 0x01, 0x04, 0x00
    gain_table_config:7, 0x01, 0x05, 0x00
    gain_table_config:8, 0x01, 0x06, 0x00
    gain_table_config:9, 0x01, 0x07, 0x00
    gain_table_config:10, 0x01, 0x08, 0x00
    gain_table_config:11, 0x01, 0x09, 0x00
    gain_table_config:12, 0x01, 0x0A, 0x00
    gain_table_config:13, 0x01, 0x0B, 0x00
    gain_table_config:14, 0x01, 0x0C, 0x00
    gain_table_config:15, 0x01, 0x0D, 0x00
    gain_table_config:16, 0x01, 0x0E, 0x00
    gain_table_config:17, 0x02, 0x09, 0x20
    gain_table_config:18, 0x02, 0x0A, 0x00
    gain_table_config:19, 0x02, 0x0B, 0x00
    gain_table_config:20, 0x02, 0x0C, 0x00
    gain_table_config:21, 0x02, 0x0D, 0x00
    gain_table_config:22, 0x02, 0x0E, 0x00
    gain_table_config:23, 0x02, 0x0F, 0x00
    gain_table_config:24, 0x02, 0x10, 0x00
    gain_table_config:25, 0x02, 0x2B, 0x20
    gain_table_config:26, 0x02, 0x2C, 0x00
    gain_table_config:27, 0x04, 0x28, 0x20
    gain_table_config:28, 0x04, 0x29, 0x00
    gain_table_config:29, 0x04, 0x2A, 0x00
    gain_table_config:30, 0x04, 0x2B, 0x00
    gain_table_config:31, 0x24, 0x20, 0x20
    gain_table_config:32, 0x24, 0x21, 0x00
    gain_table_config:33, 0x44, 0x20, 0x20
    gain_table_config:34, 0x44, 0x21, 0x00
    gain_table_config:35, 0x44, 0x22, 0x00
    gain_table_config:36, 0x44, 0x23, 0x00
    gain_table_config:37, 0x44, 0x24, 0x00
    gain_table_config:38, 0x44, 0x25, 0x00
    gain_table_config:39, 0x44, 0x26, 0x00
    gain_table_config:40, 0x44, 0x27, 0x00
    gain_table_config:41, 0x44, 0x28, 0x00
    gain_table_config:42, 0x44, 0x29, 0x00
    gain_table_config:43, 0x44, 0x2A, 0x00
    gain_table_config:44, 0x44, 0x2B, 0x00
    gain_table_config:45, 0x44, 0x2C, 0x00
    gain_table_config:46, 0x44, 0x2D, 0x00
    gain_table_config:47, 0x44, 0x2E, 0x00
    gain_table_config:48, 0x44, 0x2F, 0x00
    gain_table_config:49, 0x44, 0x30, 0x00
    gain_table_config:50, 0x44, 0x31, 0x00
    gain_table_config:51, 0x44, 0x32, 0x00
    gain_table_config:52, 0x64, 0x2E, 0x20
    gain_table_config:53, 0x64, 0x2F, 0x00
    gain_table_config:54, 0x64, 0x30, 0x00
    gain_table_config:55, 0x64, 0x31, 0x00
    gain_table_config:56, 0x64, 0x32, 0x00
    gain_table_config:57, 0x64, 0x33, 0x00
    gain_table_config:58, 0x64, 0x34, 0x00
    gain_table_config:59, 0x64, 0x35, 0x00
    gain_table_config:60, 0x64, 0x36, 0x00
    gain_table_config:61, 0x64, 0x37, 0x00
    gain_table_config:62, 0x64, 0x38, 0x00
    gain_table_config:63, 0x65, 0x38, 0x20
    gain_table_config:64, 0x66, 0x38, 0x20
    gain_table_config:65, 0x67, 0x38, 0x20
    gain_table_config:66, 0x68, 0x38, 0x20
    gain_table_config:67, 0x69, 0x38, 0x20
    gain_table_config:68, 0x6A, 0x38, 0x20
    gain_table_config:69, 0x6B, 0x38, 0x20
    gain_table_config:70, 0x6C, 0x38, 0x20
    gain_table_config:71, 0x6D, 0x38, 0x20
    gain_table_config:72, 0x6E, 0x38, 0x20
    gain_table_config:73, 0x6F, 0x38, 0x20
    gain_table_config:</gaintable>
    in_out_voltage_filter_fir_en:0
    in_temp0_input:46491
    in_voltage0_gain_control_mode:slow_attack
    in_voltage0_hardwaregain:20.000000 dB
    in_voltage0_hardwaregain_available:[-1 1 73]
    in_voltage0_rf_port_select:A_BALANCED
    in_voltage0_rssi:41.25 dB
    in_voltage2_offset:57
    in_voltage2_raw:369
    in_voltage2_scale:0.305250
    in_voltage_bb_dc_offset_tracking_en:1
    in_voltage_filter_fir_en:0
    in_voltage_gain_control_mode_available:manual fast_attack slow_attack hybrid
    in_voltage_quadrature_tracking_en:1
    in_voltage_rf_bandwidth:400000
    in_voltage_rf_bandwidth_available:[200000 1 56000000]
    in_voltage_rf_dc_offset_tracking_en:1
    in_voltage_rf_port_select_available:A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
    in_voltage_sampling_frequency:25599999
    in_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: multichip_sync: Permission denied
    name:ad9361-phy
    grep: of_node: Is a directory
    out_altvoltage0_RX_LO_external:0
    out_altvoltage0_RX_LO_fastlock_load:0
    grep: out_altvoltage0_RX_LO_fastlock_recall: Invalid argument
    out_altvoltage0_RX_LO_fastlock_save:0 252,243,108,159,253,155,211,217,217,223,221,223,248,254,255,110
    out_altvoltage0_RX_LO_fastlock_store:0
    out_altvoltage0_RX_LO_frequency:868824998
    out_altvoltage0_RX_LO_frequency_available:[70000000 1 6000000000]
    out_altvoltage0_RX_LO_powerdown:0
    out_altvoltage1_TX_LO_external:0
    out_altvoltage1_TX_LO_fastlock_load:0
    grep: out_altvoltage1_TX_LO_fastlock_recall: Invalid argument
    out_altvoltage1_TX_LO_fastlock_save:0 100,102,246,255,38,118,230,238,125,254,230,106,102,110,215,182
    out_altvoltage1_TX_LO_fastlock_store:0
    out_altvoltage1_TX_LO_frequency:1331000000
    out_altvoltage1_TX_LO_frequency_available:[46875001 1 6000000000]
    out_altvoltage1_TX_LO_powerdown:0
    out_voltage0_hardwaregain:-36.500000 dB
    out_voltage0_hardwaregain_available:[-89.750000 0.250000 0.000000]
    out_voltage0_rf_port_select:A
    out_voltage0_rssi:0.00 dB
    out_voltage2_raw:306
    out_voltage2_scale:1.000000
    out_voltage3_raw:306
    out_voltage3_scale:1.000000
    out_voltage_filter_fir_en:0
    out_voltage_rf_bandwidth:5000000
    out_voltage_rf_bandwidth_available:[200000 1 40000000]
    out_voltage_rf_port_select_available:A B
    out_voltage_sampling_frequency:25599999
    out_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: power: Is a directory
    rssi_gain_step_error:lna_error: 0 0 0 0
    rssi_gain_step_error:mixer_error: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    rssi_gain_step_error:gain_step_calib_reg_val: 0 0 0 0 0
    rx_path_rates:BBPLL:819199990 ADC:204799997 R2:102399998 R1:51199999 RF:25599999 RXSAMP:25599999
    grep: subsystem: Is a directory
    trx_rate_governor:nominal
    trx_rate_governor_available:nominal highest_osr
    tx_path_rates:BBPLL:819199990 DAC:204799997 T2:102399998 T1:51199999 TF:25599999 TXSAMP:25599999
    uevent:MAJOR=250
    uevent:MINOR=0
    uevent:DEVNAME=iio:device0
    uevent:DEVTYPE=iio_device
    uevent:OF_NAME=ad9361-phy
    uevent:OF_FULLNAME=/axi/spi@e0006000/ad9361-phy@0
    uevent:OF_COMPATIBLE_0=adi,ad9364
    uevent:OF_COMPATIBLE_N=1
    xo_correction:39999530
    xo_correction_available:[39991531 1 40007529]
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # iio_reg ad9361-phy 0x37
    0xa
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # grep "" *              
    calib_mode:auto
    calib_mode_available:auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
    grep: dcxo_tune_coarse: No such device
    dcxo_tune_coarse_available:[0 0 0]
    grep: dcxo_tune_fine: No such device
    dcxo_tune_fine_available:[0 0 0]
    dev:250:0
    ensm_mode:fdd
    ensm_mode_available:sleep wait alert fdd pinctrl pinctrl_fdd_indep
    filter_fir_config:FIR Rx: 0,0 Tx: 64,4
    gain_table_config:<gaintable AD9361 type=FULL dest=3 start=0 end=1300000000>
    gain_table_config:-1, 0x00, 0x00, 0x20
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:0, 0x00, 0x01, 0x00
    gain_table_config:1, 0x00, 0x02, 0x00
    gain_table_config:2, 0x00, 0x03, 0x00
    gain_table_config:3, 0x00, 0x04, 0x00
    gain_table_config:4, 0x00, 0x05, 0x00
    gain_table_config:5, 0x01, 0x03, 0x20
    gain_table_config:6, 0x01, 0x04, 0x00
    gain_table_config:7, 0x01, 0x05, 0x00
    gain_table_config:8, 0x01, 0x06, 0x00
    gain_table_config:9, 0x01, 0x07, 0x00
    gain_table_config:10, 0x01, 0x08, 0x00
    gain_table_config:11, 0x01, 0x09, 0x00
    gain_table_config:12, 0x01, 0x0A, 0x00
    gain_table_config:13, 0x01, 0x0B, 0x00
    gain_table_config:14, 0x01, 0x0C, 0x00
    gain_table_config:15, 0x01, 0x0D, 0x00
    gain_table_config:16, 0x01, 0x0E, 0x00
    gain_table_config:17, 0x02, 0x09, 0x20
    gain_table_config:18, 0x02, 0x0A, 0x00
    gain_table_config:19, 0x02, 0x0B, 0x00
    gain_table_config:20, 0x02, 0x0C, 0x00
    gain_table_config:21, 0x02, 0x0D, 0x00
    gain_table_config:22, 0x02, 0x0E, 0x00
    gain_table_config:23, 0x02, 0x0F, 0x00
    gain_table_config:24, 0x02, 0x10, 0x00
    gain_table_config:25, 0x02, 0x2B, 0x20
    gain_table_config:26, 0x02, 0x2C, 0x00
    gain_table_config:27, 0x04, 0x28, 0x20
    gain_table_config:28, 0x04, 0x29, 0x00
    gain_table_config:29, 0x04, 0x2A, 0x00
    gain_table_config:30, 0x04, 0x2B, 0x00
    gain_table_config:31, 0x24, 0x20, 0x20
    gain_table_config:32, 0x24, 0x21, 0x00
    gain_table_config:33, 0x44, 0x20, 0x20
    gain_table_config:34, 0x44, 0x21, 0x00
    gain_table_config:35, 0x44, 0x22, 0x00
    gain_table_config:36, 0x44, 0x23, 0x00
    gain_table_config:37, 0x44, 0x24, 0x00
    gain_table_config:38, 0x44, 0x25, 0x00
    gain_table_config:39, 0x44, 0x26, 0x00
    gain_table_config:40, 0x44, 0x27, 0x00
    gain_table_config:41, 0x44, 0x28, 0x00
    gain_table_config:42, 0x44, 0x29, 0x00
    gain_table_config:43, 0x44, 0x2A, 0x00
    gain_table_config:44, 0x44, 0x2B, 0x00
    gain_table_config:45, 0x44, 0x2C, 0x00
    gain_table_config:46, 0x44, 0x2D, 0x00
    gain_table_config:47, 0x44, 0x2E, 0x00
    gain_table_config:48, 0x44, 0x2F, 0x00
    gain_table_config:49, 0x44, 0x30, 0x00
    gain_table_config:50, 0x44, 0x31, 0x00
    gain_table_config:51, 0x44, 0x32, 0x00
    gain_table_config:52, 0x64, 0x2E, 0x20
    gain_table_config:53, 0x64, 0x2F, 0x00
    gain_table_config:54, 0x64, 0x30, 0x00
    gain_table_config:55, 0x64, 0x31, 0x00
    gain_table_config:56, 0x64, 0x32, 0x00
    gain_table_config:57, 0x64, 0x33, 0x00
    gain_table_config:58, 0x64, 0x34, 0x00
    gain_table_config:59, 0x64, 0x35, 0x00
    gain_table_config:60, 0x64, 0x36, 0x00
    gain_table_config:61, 0x64, 0x37, 0x00
    gain_table_config:62, 0x64, 0x38, 0x00
    gain_table_config:63, 0x65, 0x38, 0x20
    gain_table_config:64, 0x66, 0x38, 0x20
    gain_table_config:65, 0x67, 0x38, 0x20
    gain_table_config:66, 0x68, 0x38, 0x20
    gain_table_config:67, 0x69, 0x38, 0x20
    gain_table_config:68, 0x6A, 0x38, 0x20
    gain_table_config:69, 0x6B, 0x38, 0x20
    gain_table_config:70, 0x6C, 0x38, 0x20
    gain_table_config:71, 0x6D, 0x38, 0x20
    gain_table_config:72, 0x6E, 0x38, 0x20
    gain_table_config:73, 0x6F, 0x38, 0x20
    gain_table_config:</gaintable>
    in_out_voltage_filter_fir_en:0
    in_temp0_input:46491
    in_voltage0_gain_control_mode:slow_attack
    in_voltage0_hardwaregain:20.000000 dB
    in_voltage0_hardwaregain_available:[-1 1 73]
    in_voltage0_rf_port_select:A_BALANCED
    in_voltage0_rssi:41.25 dB
    in_voltage2_offset:57
    in_voltage2_raw:370
    in_voltage2_scale:0.305250
    in_voltage_bb_dc_offset_tracking_en:1
    in_voltage_filter_fir_en:0
    in_voltage_gain_control_mode_available:manual fast_attack slow_attack hybrid
    in_voltage_quadrature_tracking_en:1
    in_voltage_rf_bandwidth:400000
    in_voltage_rf_bandwidth_available:[200000 1 56000000]
    in_voltage_rf_dc_offset_tracking_en:1
    in_voltage_rf_port_select_available:A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
    in_voltage_sampling_frequency:25599999
    in_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: multichip_sync: Permission denied
    name:ad9361-phy
    grep: of_node: Is a directory
    out_altvoltage0_RX_LO_external:0
    out_altvoltage0_RX_LO_fastlock_load:0
    grep: out_altvoltage0_RX_LO_fastlock_recall: Invalid argument
    out_altvoltage0_RX_LO_fastlock_save:0 252,243,108,159,253,155,211,217,217,223,221,223,248,254,255,110
    out_altvoltage0_RX_LO_fastlock_store:0
    out_altvoltage0_RX_LO_frequency:868824998
    out_altvoltage0_RX_LO_frequency_available:[70000000 1 6000000000]
    out_altvoltage0_RX_LO_powerdown:0
    out_altvoltage1_TX_LO_external:0
    out_altvoltage1_TX_LO_fastlock_load:0
    grep: out_altvoltage1_TX_LO_fastlock_recall: Invalid argument
    out_altvoltage1_TX_LO_fastlock_save:0 100,102,246,255,38,118,230,238,125,254,230,106,102,110,215,182
    out_altvoltage1_TX_LO_fastlock_store:0
    out_altvoltage1_TX_LO_frequency:1331000000
    out_altvoltage1_TX_LO_frequency_available:[46875001 1 6000000000]
    out_altvoltage1_TX_LO_powerdown:0
    out_voltage0_hardwaregain:-36.500000 dB
    out_voltage0_hardwaregain_available:[-89.750000 0.250000 0.000000]
    out_voltage0_rf_port_select:A
    out_voltage0_rssi:0.00 dB
    out_voltage2_raw:306
    out_voltage2_scale:1.000000
    out_voltage3_raw:306
    out_voltage3_scale:1.000000
    out_voltage_filter_fir_en:0
    out_voltage_rf_bandwidth:5000000
    out_voltage_rf_bandwidth_available:[200000 1 40000000]
    out_voltage_rf_port_select_available:A B
    out_voltage_sampling_frequency:25599999
    out_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: power: Is a directory
    rssi_gain_step_error:lna_error: 0 0 0 0
    rssi_gain_step_error:mixer_error: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    rssi_gain_step_error:gain_step_calib_reg_val: 0 0 0 0 0
    rx_path_rates:BBPLL:819199990 ADC:204799997 R2:102399998 R1:51199999 RF:25599999 RXSAMP:25599999
    grep: subsystem: Is a directory
    trx_rate_governor:nominal
    trx_rate_governor_available:nominal highest_osr
    tx_path_rates:BBPLL:819199990 DAC:204799997 T2:102399998 T1:51199999 TF:25599999 TXSAMP:25599999
    uevent:MAJOR=250
    uevent:MINOR=0
    uevent:DEVNAME=iio:device0
    uevent:DEVTYPE=iio_device
    uevent:OF_NAME=ad9361-phy
    uevent:OF_FULLNAME=/axi/spi@e0006000/ad9361-phy@0
    uevent:OF_COMPATIBLE_0=adi,ad9364
    uevent:OF_COMPATIBLE_N=1
    xo_correction:39999530
    xo_correction_available:[39991531 1 40007529]
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # grep "" *
    calib_mode:auto
    calib_mode_available:auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
    grep: dcxo_tune_coarse: No such device
    dcxo_tune_coarse_available:[0 0 0]
    grep: dcxo_tune_fine: No such device
    dcxo_tune_fine_available:[0 0 0]
    dev:250:0
    ensm_mode:fdd
    ensm_mode_available:sleep wait alert fdd pinctrl pinctrl_fdd_indep
    filter_fir_config:FIR Rx: 0,0 Tx: 64,4
    gain_table_config:<gaintable AD9361 type=FULL dest=3 start=0 end=1300000000>
    gain_table_config:-1, 0x00, 0x00, 0x20
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:0, 0x00, 0x01, 0x00
    gain_table_config:1, 0x00, 0x02, 0x00
    gain_table_config:2, 0x00, 0x03, 0x00
    gain_table_config:3, 0x00, 0x04, 0x00
    gain_table_config:4, 0x00, 0x05, 0x00
    gain_table_config:5, 0x01, 0x03, 0x20
    gain_table_config:6, 0x01, 0x04, 0x00
    gain_table_config:7, 0x01, 0x05, 0x00
    gain_table_config:8, 0x01, 0x06, 0x00
    gain_table_config:9, 0x01, 0x07, 0x00
    gain_table_config:10, 0x01, 0x08, 0x00
    gain_table_config:11, 0x01, 0x09, 0x00
    gain_table_config:12, 0x01, 0x0A, 0x00
    gain_table_config:13, 0x01, 0x0B, 0x00
    gain_table_config:14, 0x01, 0x0C, 0x00
    gain_table_config:15, 0x01, 0x0D, 0x00
    gain_table_config:16, 0x01, 0x0E, 0x00
    gain_table_config:17, 0x02, 0x09, 0x20
    gain_table_config:18, 0x02, 0x0A, 0x00
    gain_table_config:19, 0x02, 0x0B, 0x00
    gain_table_config:20, 0x02, 0x0C, 0x00
    gain_table_config:21, 0x02, 0x0D, 0x00
    gain_table_config:22, 0x02, 0x0E, 0x00
    gain_table_config:23, 0x02, 0x0F, 0x00
    gain_table_config:24, 0x02, 0x10, 0x00
    gain_table_config:25, 0x02, 0x2B, 0x20
    gain_table_config:26, 0x02, 0x2C, 0x00
    gain_table_config:27, 0x04, 0x28, 0x20
    gain_table_config:28, 0x04, 0x29, 0x00
    gain_table_config:29, 0x04, 0x2A, 0x00
    gain_table_config:30, 0x04, 0x2B, 0x00
    gain_table_config:31, 0x24, 0x20, 0x20
    gain_table_config:32, 0x24, 0x21, 0x00
    gain_table_config:33, 0x44, 0x20, 0x20
    gain_table_config:34, 0x44, 0x21, 0x00
    gain_table_config:35, 0x44, 0x22, 0x00
    gain_table_config:36, 0x44, 0x23, 0x00
    gain_table_config:37, 0x44, 0x24, 0x00
    gain_table_config:38, 0x44, 0x25, 0x00
    gain_table_config:39, 0x44, 0x26, 0x00
    gain_table_config:40, 0x44, 0x27, 0x00
    gain_table_config:41, 0x44, 0x28, 0x00
    gain_table_config:42, 0x44, 0x29, 0x00
    gain_table_config:43, 0x44, 0x2A, 0x00
    gain_table_config:44, 0x44, 0x2B, 0x00
    gain_table_config:45, 0x44, 0x2C, 0x00
    gain_table_config:46, 0x44, 0x2D, 0x00
    gain_table_config:47, 0x44, 0x2E, 0x00
    gain_table_config:48, 0x44, 0x2F, 0x00
    gain_table_config:49, 0x44, 0x30, 0x00
    gain_table_config:50, 0x44, 0x31, 0x00
    gain_table_config:51, 0x44, 0x32, 0x00
    gain_table_config:52, 0x64, 0x2E, 0x20
    gain_table_config:53, 0x64, 0x2F, 0x00
    gain_table_config:54, 0x64, 0x30, 0x00
    gain_table_config:55, 0x64, 0x31, 0x00
    gain_table_config:56, 0x64, 0x32, 0x00
    gain_table_config:57, 0x64, 0x33, 0x00
    gain_table_config:58, 0x64, 0x34, 0x00
    gain_table_config:59, 0x64, 0x35, 0x00
    gain_table_config:60, 0x64, 0x36, 0x00
    gain_table_config:61, 0x64, 0x37, 0x00
    gain_table_config:62, 0x64, 0x38, 0x00
    gain_table_config:63, 0x65, 0x38, 0x20
    gain_table_config:64, 0x66, 0x38, 0x20
    gain_table_config:65, 0x67, 0x38, 0x20
    gain_table_config:66, 0x68, 0x38, 0x20
    gain_table_config:67, 0x69, 0x38, 0x20
    gain_table_config:68, 0x6A, 0x38, 0x20
    gain_table_config:69, 0x6B, 0x38, 0x20
    gain_table_config:70, 0x6C, 0x38, 0x20
    gain_table_config:71, 0x6D, 0x38, 0x20
    gain_table_config:72, 0x6E, 0x38, 0x20
    gain_table_config:73, 0x6F, 0x38, 0x20
    gain_table_config:</gaintable>
    in_out_voltage_filter_fir_en:0
    in_temp0_input:44737
    in_voltage0_gain_control_mode:slow_attack
    in_voltage0_hardwaregain:30.000000 dB
    in_voltage0_hardwaregain_available:[-1 1 73]
    in_voltage0_rf_port_select:A_BALANCED
    in_voltage0_rssi:54.25 dB
    in_voltage2_offset:57
    in_voltage2_raw:389
    in_voltage2_scale:0.305250
    in_voltage_bb_dc_offset_tracking_en:1
    in_voltage_filter_fir_en:0
    in_voltage_gain_control_mode_available:manual fast_attack slow_attack hybrid
    in_voltage_quadrature_tracking_en:1
    in_voltage_rf_bandwidth:400000
    in_voltage_rf_bandwidth_available:[200000 1 56000000]
    in_voltage_rf_dc_offset_tracking_en:1
    in_voltage_rf_port_select_available:A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
    in_voltage_sampling_frequency:3999999
    in_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: multichip_sync: Permission denied
    name:ad9361-phy
    grep: of_node: Is a directory
    out_altvoltage0_RX_LO_external:0
    out_altvoltage0_RX_LO_fastlock_load:0
    grep: out_altvoltage0_RX_LO_fastlock_recall: Invalid argument
    out_altvoltage0_RX_LO_fastlock_save:0 252,243,108,159,253,155,211,217,217,223,221,223,248,254,255,110
    out_altvoltage0_RX_LO_fastlock_store:0
    out_altvoltage0_RX_LO_frequency:128400000
    out_altvoltage0_RX_LO_frequency_available:[70000000 1 6000000000]
    out_altvoltage0_RX_LO_powerdown:0
    out_altvoltage1_TX_LO_external:0
    out_altvoltage1_TX_LO_fastlock_load:0
    grep: out_altvoltage1_TX_LO_fastlock_recall: Invalid argument
    out_altvoltage1_TX_LO_fastlock_save:0 100,102,246,255,38,118,230,238,125,254,230,106,102,110,215,182
    out_altvoltage1_TX_LO_fastlock_store:0
    out_altvoltage1_TX_LO_frequency:247999998
    out_altvoltage1_TX_LO_frequency_available:[46875001 1 6000000000]
    out_altvoltage1_TX_LO_powerdown:0
    out_voltage0_hardwaregain:-32.000000 dB
    out_voltage0_hardwaregain_available:[-89.750000 0.250000 0.000000]
    out_voltage0_rf_port_select:A
    out_voltage0_rssi:0.00 dB
    out_voltage2_raw:306
    out_voltage2_scale:1.000000
    out_voltage3_raw:306
    out_voltage3_scale:1.000000
    out_voltage_filter_fir_en:1
    out_voltage_rf_bandwidth:1260770
    out_voltage_rf_bandwidth_available:[200000 1 40000000]
    out_voltage_rf_port_select_available:A B
    out_voltage_sampling_frequency:3999999
    out_voltage_sampling_frequency_available:[520833 1 30720000]
    grep: power: Is a directory
    rssi_gain_step_error:lna_error: 0 0 0 0
    rssi_gain_step_error:mixer_error: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    rssi_gain_step_error:gain_step_calib_reg_val: 0 0 0 0 0
    rx_path_rates:BBPLL:1023999992 ADC:31999999 R2:15999999 R1:7999999 RF:3999999 RXSAMP:3999999
    grep: subsystem: Is a directory
    trx_rate_governor:nominal
    trx_rate_governor_available:nominal highest_osr
    tx_path_rates:BBPLL:1023999992 DAC:31999999 T2:15999999 T1:15999999 TF:15999999 TXSAMP:3999999
    uevent:MAJOR=250
    uevent:MINOR=0
    uevent:DEVNAME=iio:device0
    uevent:DEVTYPE=iio_device
    uevent:OF_NAME=ad9361-phy
    uevent:OF_FULLNAME=/axi/spi@e0006000/ad9361-phy@0
    uevent:OF_COMPATIBLE_0=adi,ad9364
    uevent:OF_COMPATIBLE_N=1
    xo_correction:39999530
    xo_correction_available:[39991531 1 40007529]
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # iio_reg ad9361-phy 0x37
    0xa
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # grep "" *              
    calib_mode:auto
    calib_mode_available:auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step
    grep: dcxo_tune_coarse: No such device
    dcxo_tune_coarse_available:[0 0 0]
    grep: dcxo_tune_fine: No such device
    dcxo_tune_fine_available:[0 0 0]
    dev:250:0
    ensm_mode:fdd
    ensm_mode_available:sleep wait alert fdd pinctrl pinctrl_fdd_indep
    filter_fir_config:FIR Rx: 0,0 Tx: 64,4
    gain_table_config:<gaintable AD9361 type=FULL dest=3 start=0 end=1300000000>
    gain_table_config:-1, 0x00, 0x00, 0x20
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:-1, 0x00, 0x00, 0x00
    gain_table_config:0, 0x00, 0x01, 0x00
    gain_table_config:1, 0x00, 0x02, 0x00
    gain_table_config:2, 0x00, 0x03, 0x00
    gain_table_config:3, 0x00, 0x04, 0x00
    gain_table_config:4, 0x00, 0x05, 0x00
    gain_table_config:5, 0x01, 0x03, 0x20
    gain_table_config:6, 0x01, 0x04, 0x00
    gain_table_config:7, 0x01, 0x05, 0x00
    gain_table_config:8, 0x01, 0x06, 0x00
    gain_table_config:9, 0x01, 0x07, 0x00
    gain_table_config:10, 0x01, 0x08, 0x00
    gain_table_config:11, 0x01, 0x09, 0x00
    gain_table_config:12, 0x01, 0x0A, 0x00
    gain_table_config:13, 0x01, 0x0B, 0x00
    gain_table_config:14, 0x01, 0x0C, 0x00
    gain_table_config:15, 0x01, 0x0D, 0x00
    gain_table_config:16, 0x01, 0x0E, 0x00
    gain_table_config:17, 0x02, 0x09, 0x20
    gain_table_config:18, 0x02, 0x0A, 0x00
    gain_table_config:19, 0x02, 0x0B, 0x00
    gain_table_config:20, 0x02, 0x0C, 0x00
    gain_table_config:21, 0x02, 0x0D, 0x00
    gain_table_config:22, 0x02, 0x0E, 0x00
    gain_table_config:23, 0x02, 0x0F, 0x00
    gain_table_config:24, 0x02, 0x10, 0x00
    gain_table_config:25, 0x02, 0x2B, 0x20
    gain_table_config:26, 0x02, 0x2C, 0x00
    gain_table_config:27, 0x04, 0x28, 0x20
    gain_table_config:28, 0x04, 0x29, 0x00
    gain_table_config:29, 0x04, 0x2A, 0x00
    gain_table_config:30, 0x04, 0x2B, 0x00
    gain_table_config:31, 0x24, 0x20, 0x20
    gain_table_config:32, 0x24, 0x21, 0x00
    gain_table_config:33, 0x44, 0x20, 0x20
    gain_table_config:34, 0x44, 0x21, 0x00
    gain_table_config:35, 0x44, 0x22, 0x00
    gain_table_config:36, 0x44, 0x23, 0x00
    gain_table_config:37, 0x44, 0x24, 0x00
    gain_table_config:38, 0x44, 0x25, 0x00
    gain_table_config:39, 0x44, 0x26, 0x00
    gain_table_config:40, 0x44, 0x27, 0x00
    gain_table_config:41, 0x44, 0x28, 0x00
    gain_table_config:42, 0x44, 0x29, 0x00
    gain_table_config:43, 0x44, 0x2A, 0x00
    gain_table_config:44, 0x44, 0x2B, 0x00
    gain_table_config:45, 0x44, 0x2C, 0x00
    gain_table_config:46, 0x44, 0x2D, 0x00
    gain_table_config:47, 0x44, 0x2E, 0x00
    gain_table_config:48, 0x44, 0x2F, 0x00
    gain_table_config:49, 0x44, 0x30, 0x00
    gain_table_config:50, 0x44, 0x31, 0x00
    gain_table_config:51, 0x44, 0x32, 0x00
    gain_table_config:52, 0x64, 0x2E, 0x20
    gain_table_config:53, 0x64, 0x2F, 0x00
    gain_table_config:54, 0x64, 0x30, 0x00
    gain_table_config:55, 0x64, 0x31, 0x00
    gain_table_config:56, 0x64, 0x32, 0x00
    gain_table_config:57, 0x64, 0x33, 0x00
    gain_table_config:58, 0x64, 0x34, 0x00
    gain_table_config:59, 0x64, 0x35, 0x00
    gain_table_config:60, 0x64, 0x36, 0x00
    gain_table_config:61, 0x64, 0x37, 0x00
    gain_table_config:62, 0x64, 0x38, 0x00
    gain_table_config:63, 0x65, 0x38, 0x20
    gain_table_config:64, 0x66, 0x38, 0x20
    gain_table_config:65, 0x67, 0x38, 0x20
    gain_table_config:66, 0x68, 0x38, 0x20
    gain_table_config:67, 0x69, 0x38, 0x20
    gain_table_config:68, 0x6A, 0x38, 0x20
    gain_table_config:69, 0x6B, 0x38, 0x20
    gain_table_config:70, 0x6C, 0x38, 0x20
    gain_table_config:71, 0x6D, 0x38, 0x20
    gain_table_config:72, 0x6E, 0x38, 0x20
    gain_table_config:73, 0x6F, 0x38, 0x20
    gain_table_config:</gaintable>
    in_out_voltage_filter_fir_en:0
    in_temp0_input:44737
    in_voltage0_gain_control_mode:slow_attack
    in_voltage0_hardwaregain:30.000000 dB
    in_voltage0_hardwaregain_available:[-1 1 73]
    in_voltage0_rf_port_select:A_BALANCED
    in_voltage0_rssi:54.25 dB
    in_voltage2_offset:57
    in_voltage2_raw:386
    in_voltage2_scale:0.305250
    in_voltage_bb_dc_offset_tracking_en:1
    in_voltage_filter_fir_en:0
    in_voltage_gain_control_mode_available:manual fast_attack slow_attack hybrid
    in_voltage_quadrature_tracking_en:1
    in_voltage_rf_bandwidth:400000
    in_voltage_rf_bandwidth_available:[200000 1 56000000]
    in_voltage_rf_dc_offset_tracking_en:1
    in_voltage_rf_port_select_available:A_BALANCED B_BALANCED C_BALANCED A_N A_P B_N B_P C_N C_P TX_MONITOR1 TX_MONITOR2 TX_MONITOR1_2
    in_voltage_sampling_frequency:3999999
    in_voltage_sampling_frequency_available:[2083333 1 61440000]
    grep: multichip_sync: Permission denied
    name:ad9361-phy
    grep: of_node: Is a directory
    out_altvoltage0_RX_LO_external:0
    out_altvoltage0_RX_LO_fastlock_load:0
    grep: out_altvoltage0_RX_LO_fastlock_recall: Invalid argument
    out_altvoltage0_RX_LO_fastlock_save:0 252,243,108,159,253,155,211,217,217,223,221,223,248,254,255,110
    out_altvoltage0_RX_LO_fastlock_store:0
    out_altvoltage0_RX_LO_frequency:128400000
    out_altvoltage0_RX_LO_frequency_available:[70000000 1 6000000000]
    out_altvoltage0_RX_LO_powerdown:0
    out_altvoltage1_TX_LO_external:0
    out_altvoltage1_TX_LO_fastlock_load:0
    grep: out_altvoltage1_TX_LO_fastlock_recall: Invalid argument
    out_altvoltage1_TX_LO_fastlock_save:0 100,102,246,255,38,118,230,238,125,254,230,106,102,110,215,182
    out_altvoltage1_TX_LO_fastlock_store:0
    out_altvoltage1_TX_LO_frequency:247999998
    out_altvoltage1_TX_LO_frequency_available:[46875001 1 6000000000]
    out_altvoltage1_TX_LO_powerdown:0
    out_voltage0_hardwaregain:-32.000000 dB
    out_voltage0_hardwaregain_available:[-89.750000 0.250000 0.000000]
    out_voltage0_rf_port_select:A
    out_voltage0_rssi:0.00 dB
    out_voltage2_raw:306
    out_voltage2_scale:1.000000
    out_voltage3_raw:306
    out_voltage3_scale:1.000000
    out_voltage_filter_fir_en:1
    out_voltage_rf_bandwidth:1260770
    out_voltage_rf_bandwidth_available:[200000 1 40000000]
    out_voltage_rf_port_select_available:A B
    out_voltage_sampling_frequency:3999999
    out_voltage_sampling_frequency_available:[520833 1 30720000]
    grep: power: Is a directory
    rssi_gain_step_error:lna_error: 0 0 0 0
    rssi_gain_step_error:mixer_error: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0
    rssi_gain_step_error:gain_step_calib_reg_val: 0 0 0 0 0
    rx_path_rates:BBPLL:1023999992 ADC:31999999 R2:15999999 R1:7999999 RF:3999999 RXSAMP:3999999
    grep: subsystem: Is a directory
    trx_rate_governor:nominal
    trx_rate_governor_available:nominal highest_osr
    tx_path_rates:BBPLL:1023999992 DAC:31999999 T2:15999999 T1:15999999 TF:15999999 TXSAMP:3999999
    uevent:MAJOR=250
    uevent:MINOR=0
    uevent:DEVNAME=iio:device0
    uevent:DEVTYPE=iio_device
    uevent:OF_NAME=ad9361-phy
    uevent:OF_FULLNAME=/axi/spi@e0006000/ad9361-phy@0
    uevent:OF_COMPATIBLE_0=adi,ad9364
    uevent:OF_COMPATIBLE_N=1
    xo_correction:39999530
    xo_correction_available:[39991531 1 40007529]
    adrv9364-m6am-2022Q2 /sys/bus/iio/devices/iio:device0 # iio_reg ad9361-phy 0x37
    0xa
    

    40 MHz wideband noise requiring filter below does not trigger issue.

    # Generated with AD9361 Filter Design Wizard 16.1.3-g924f0cd
    # MATLAB 9.8.0.1417392 (R2020a) Update 4, 09-Jul-2021 15:05:33
    # Inputs:
    # Data Sample Frequency = 60800000 Hz
    # Apass = 0.12 dB Astop = 60.00 dB
    # Fpass = 19000000 Hz Fstop = 22500000 Hz
    # Pass Frequency = 40000000 Hz
    TX 3 GAIN 0 INT 1
    RTX 972800000 243200000 121600000 60800000 60800000 60800000
    BWTX 19163714
    1235
    -712
    -1012
    2448
    -1636
    -1302
    3649
    -2277
    -2806
    7053
    -4562
    -5410
    13018
    -4762
    -14412
    28443
    28443
    -14412
    -4762
    13018
    -5410
    -4562
    7053
    -2806
    -2277
    3649
    -1302
    -1636
    2448
    -1012
    -712
    1235

    1 MHz MHz wideband noise requiring filter below does trigger reported issue.

    # Generated with AD9361 Filter Design Wizard 16.1.3-g924f0cd
    # MATLAB 9.8.0.1417392 (R2020a) Update 4, 09-Jul-2021 15:36:48
    # Inputs:
    # Data Sample Frequency = 4000000 Hz
    # Apass = 0.12 dB Astop = 60.00 dB
    # Fpass = 100000 Hz Fstop = 800000 Hz
    # Pass Frequency = 1000000 Hz
    TX 3 GAIN 0 INT 4
    RTX 768000000 192000000 64000000 32000000 16000000 4000000
    BWTX 1260770
    -6299
    14356
    -19852
    17263
    -15095
    10147
    -9167
    5208
    -5401
    2391
    -2968
    1044
    -1146
    731
    514
    1215
    2245
    2343
    4123
    3984
    6133
    5966
    8199
    8073
    10168
    10118
    11859
    11865
    13122
    13137
    13790
    13805
    13805
    13790
    13137
    13122
    11865
    11859
    10118
    10168
    8073
    8199
    5966
    6133
    3984
    4123
    2343
    2245
    1215
    514
    731
    -1146
    1044
    -2968
    2391
    -5401
    5208
    -9167
    10147
    -15095
    17263
    -19852
    14356
    -6299

    Finally, to duplicate the case,

    1. cat 1M.ftr > /sys/bus/iio/devices/iio\:device0/filter_fir_config
    2. echo 1000000000 > out_altvoltage1_TX_LO_frequency
    3. echo 247999998 > out_altvoltage1_TX_LO_frequency

    Looks like AD9361 Filter Design Wizard creates a filter with parameters that trigger the issue?

  • Looks like AD9361 Filter Design Wizard creates a filter with parameters that trigger the issue?

    Not directly - but let me explain.

    The RXSAMP and TXSAMP rate must always be equal. In case you have only some FIR interpolation on the TX or decimation on the RX side. The difference must be compensated in the other filter banks.

    However TX QUAD cal uses CLKRF and CLKTF and those can have only certain supported ratios. 

    To avoid the issue configure a FILTER that also defines the RX path decimation.

    Take a look here:

    https://github.com/analogdevicesinc/iio-oscilloscope/blob/master/filters/LTE20_MHz.ftr#L5

    In general reducing the sample rate just to save power might not be the only way.

    root@analog:/sys/bus/iio/devices/iio:device1# cat ensm_mode_available
    sleep wait alert fdd pinctrl pinctrl_fdd_indep

    Depending on your use case, you might just want to use ensm_mode sleep instead?

    BTW: I was not able to replicate the issue with your filter.

    Maybe you miss some step?

    I don't see where the filter is enabled?

    Step 1) just loads the filter 2) and 3) will trigger the TX QUAD cal in auto mode.

    Some hint's there - You might want to use manual_tx_quad mode 

    wiki.analog.com/.../ad9361

    root@analog:/sys/bus/iio/devices/iio:device1# cat calib_mode_available
    auto manual manual_tx_quad tx_quad rf_dc_offs rssi_gain_step

    You run tx_quad once in your prominent frequency and rate.

    So when you move to your power saving rate, the cal is not triggered anymore.

    This should save time, power and also avoid spurious transmissions.

    Please also disable the FIR filter before loading it again. 

    I think this might be related to way you run into this only occasional.

    The filter_fir_config attribute is currently not protected by a mutex, I'll add some fix here as well.

    -Michael

  • Thanks for your answer.

    Out scenario requires monitoring RSSI for 16 channels all the time in the lower power mode as well as when transmitting (RX and TX carrier frequencies do not overlap) and that is why we were avoiding symmetric filters to reduce code and calibration complexity but it is now clear what we need to do from your explanation above.

    It would be helpful for the kernel driver to reject a FIR configuration that does not meet the requirement you described above.

    I apologize for not providing a complete MWE, that happened because our application was running an no longer reconfiguring the AD9364 but as you worked out the filter was enabled.

  • We will adjust our algorithms as advised above and continue monitoring for the case where modulation fails and report separately if we hit the issue.